<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Embedded Software and Tools Clinic中的主题 Re: RT1064 ok instead of RT1060?</title>
    <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/RT1064-ok-instead-of-RT1060/m-p/929472#M10</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nick, this is under internal revision. Meanwhile, you can modify the project using the procedure described in &lt;A _jive_internal="true" class="" data-containerid="11778" data-containertype="14" data-content-finding="Community" data-objectid="344225" data-objecttype="102" href="https://community.nxp.com/docs/DOC-344225"&gt;eIQ on i.MX RT1064 EVK&lt;/A&gt; post.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Aug 2019 19:21:32 GMT</pubDate>
    <dc:creator>jc_pacheco</dc:creator>
    <dc:date>2019-08-22T19:21:32Z</dc:date>
    <item>
      <title>RT1064 ok instead of RT1060?</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/RT1064-ok-instead-of-RT1060/m-p/929469#M7</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I already have a few RT1064 EVKs.&amp;nbsp; Since the only significant difference that I am aware of is the 4MB of on-chip flash for the RT1064, can I use the RT1064 instead of buying the RT1060 EVK?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Update: I verified that eIQ is listed for the currently available RT1064 SDK, but it references a requirement for the RT1050 or RT1060 which apparently prevents it from being selected for inclusion with the SDK.&amp;nbsp; So a follow-up question:&amp;nbsp; Is it possible to use the RT1060 SDK with the RT1064 EVK?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Aug 2019 15:25:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/RT1064-ok-instead-of-RT1060/m-p/929469#M7</guid>
      <dc:creator>nbgatgi</dc:creator>
      <dc:date>2019-08-15T15:25:01Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 ok instead of RT1060?</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/RT1064-ok-instead-of-RT1060/m-p/929470#M8</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nick,&lt;/P&gt;&lt;P&gt;Yes, it is possible. You could modify all memory-related MCU settings in project's properties as well as during initialization to match the FLASH on your board.&lt;/P&gt;&lt;P&gt;See &lt;A href="https://community.nxp.com/docs/DOC-344225"&gt;eIQ on i.MX RT1064 EVK.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Keep in mind that support may be limited as this is not officially supported in the SDK.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Aug 2019 22:08:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/RT1064-ok-instead-of-RT1060/m-p/929470#M8</guid>
      <dc:creator>jc_pacheco</dc:creator>
      <dc:date>2019-08-19T22:08:28Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 ok instead of RT1060?</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/RT1064-ok-instead-of-RT1060/m-p/929471#M9</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Other than the internal flash of the RT1064, since there are no functional differences from the RT1060, why is it not supported?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Aug 2019 14:48:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/RT1064-ok-instead-of-RT1060/m-p/929471#M9</guid>
      <dc:creator>nbgatgi</dc:creator>
      <dc:date>2019-08-20T14:48:23Z</dc:date>
    </item>
    <item>
      <title>Re: RT1064 ok instead of RT1060?</title>
      <link>https://community.nxp.com/t5/Embedded-Software-and-Tools/RT1064-ok-instead-of-RT1060/m-p/929472#M10</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nick, this is under internal revision. Meanwhile, you can modify the project using the procedure described in &lt;A _jive_internal="true" class="" data-containerid="11778" data-containertype="14" data-content-finding="Community" data-objectid="344225" data-objecttype="102" href="https://community.nxp.com/docs/DOC-344225"&gt;eIQ on i.MX RT1064 EVK&lt;/A&gt; post.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2019 19:21:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Embedded-Software-and-Tools/RT1064-ok-instead-of-RT1060/m-p/929472#M10</guid>
      <dc:creator>jc_pacheco</dc:creator>
      <dc:date>2019-08-22T19:21:32Z</dc:date>
    </item>
  </channel>
</rss>