<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>University Programs中的主题 Re: TWRPI-MMA845XQ</title>
    <link>https://community.nxp.com/t5/University-Programs/TWRPI-MMA845XQ/m-p/221246#M97</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much! I agree with the lack of some documentation, but I am very well impressed with the improvements in many of the labs and tutorials documentation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cata.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 09 Jun 2012 20:34:18 GMT</pubDate>
    <dc:creator>CatalinaDelacu1</dc:creator>
    <dc:date>2012-06-09T20:34:18Z</dc:date>
    <item>
      <title>TWRPI-MMA845XQ</title>
      <link>https://community.nxp.com/t5/University-Programs/TWRPI-MMA845XQ/m-p/221244#M95</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, does anyone know where can I find the&amp;nbsp;TWRPI-MMA845XQ schematics? I have looked everywhere and havent been able to find it.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2012 12:23:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/TWRPI-MMA845XQ/m-p/221244#M95</guid>
      <dc:creator>CatalinaDelacu1</dc:creator>
      <dc:date>2012-06-07T12:23:22Z</dc:date>
    </item>
    <item>
      <title>Re: TWRPI-MMA845XQ</title>
      <link>https://community.nxp.com/t5/University-Programs/TWRPI-MMA845XQ/m-p/221245#M96</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As I understand it, the you need to match up the datasheet info for the part itself, and what pins are available on the sockets, which is quite annoying.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you look in&amp;nbsp;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/TWR-K40X256-UM.pdf?fpsp=1"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/TWR-K40X256-UM.pdf?fpsp=1&lt;/A&gt;, you'll find the socket pinout: &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;TWRPI AN0 (J8 Pin 8) ― ADC0_DP0/ADC1_DP3&lt;BR /&gt;TWRPI AN1 (J8 Pin 9) ― ADC0_DM0/ADC1_DM3&lt;BR /&gt;TWRPI AN2 (J8 Pin 12) ― ADC1_DP0/ADC0_DP3&lt;BR /&gt;TWRPI ID0 (J8 Pin 17) ― ADC0_DP1&lt;BR /&gt;TWRPI ID1 (J8 Pin 18) ― ADC0_DM1&lt;BR /&gt;TWRPI I2C SCL (J9 Pin 3) PTC10 I2C1_SCL&lt;BR /&gt;TWRPI I2C SDA (J9 Pin 4) PTC11 I2C1_SDA&lt;BR /&gt;TWRPI SPI MISO (J9 Pin 9) PTB23 SPI2_SIN&lt;BR /&gt;TWRPI SPI MOSI (J9 Pin 10) PTB22 SPI2_SOUT&lt;BR /&gt;TWRPI SPI SS (J9 Pin 11) PTB20 SPI2_PCS0&lt;BR /&gt;TWRPI SPI CLK (J9 Pin 12) PTB21 SPI2_SCK&lt;BR /&gt;TWRPI GPIO0 (J9 Pin 15) PTC12 PTC12&lt;BR /&gt;TWRPI GPIO1 (J9 Pin 16) PTB9 PTB9&lt;BR /&gt;TWRPI GPIO2 (J9 Pin 17) PTB10 PTB10&lt;BR /&gt;TWRPI GPIO3 (J9 Pin 18) PTC5 PTC5&lt;BR /&gt;TWRPI GPIO4 (J9 Pin 19) PTA5 PTA5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The accelerometer has I2C pins, and two interrupt pins. &amp;nbsp;So the only way it can work is if the I2C interface comes in on pins&amp;nbsp;I2C1_SCL and&amp;nbsp;I2C1_SDA. &amp;nbsp;No idea if the interrupts map to any of the GPIO pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The tower system seems really well thought out, but Freescale seems to be really lacking in providing this sort of documentation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jun 2012 21:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/TWRPI-MMA845XQ/m-p/221245#M96</guid>
      <dc:creator>JamesPotts</dc:creator>
      <dc:date>2012-06-08T21:13:32Z</dc:date>
    </item>
    <item>
      <title>Re: TWRPI-MMA845XQ</title>
      <link>https://community.nxp.com/t5/University-Programs/TWRPI-MMA845XQ/m-p/221246#M97</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much! I agree with the lack of some documentation, but I am very well impressed with the improvements in many of the labs and tutorials documentation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cata.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jun 2012 20:34:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/TWRPI-MMA845XQ/m-p/221246#M97</guid>
      <dc:creator>CatalinaDelacu1</dc:creator>
      <dc:date>2012-06-09T20:34:18Z</dc:date>
    </item>
  </channel>
</rss>