<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Which pins to use? in University Programs</title>
    <link>https://community.nxp.com/t5/University-Programs/Which-pins-to-use/m-p/178977#M8</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When&amp;nbsp; configuring the motor drive board version A which of the PORTB pins on the ribbon connector do you use to get the DC motors running if not using the MPC5604B board (back ordered)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 17 Nov 2012 00:41:22 GMT</pubDate>
    <dc:creator>jamaalhayes</dc:creator>
    <dc:date>2012-11-17T00:41:22Z</dc:date>
    <item>
      <title>Which pins to use?</title>
      <link>https://community.nxp.com/t5/University-Programs/Which-pins-to-use/m-p/178977#M8</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When&amp;nbsp; configuring the motor drive board version A which of the PORTB pins on the ribbon connector do you use to get the DC motors running if not using the MPC5604B board (back ordered)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Nov 2012 00:41:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/Which-pins-to-use/m-p/178977#M8</guid>
      <dc:creator>jamaalhayes</dc:creator>
      <dc:date>2012-11-17T00:41:22Z</dc:date>
    </item>
    <item>
      <title>Re: Which pins to use?</title>
      <link>https://community.nxp.com/t5/University-Programs/Which-pins-to-use/m-p/178978#M9</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Jamal,&lt;/P&gt;&lt;P&gt;I am pretty sure that the red line should face the potentiometer... I think that should answer your question...&lt;/P&gt;&lt;P&gt;I am a beginner too by the way....&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Nov 2012 02:36:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/Which-pins-to-use/m-p/178978#M9</guid>
      <dc:creator>cedricdestin</dc:creator>
      <dc:date>2012-11-24T02:36:11Z</dc:date>
    </item>
    <item>
      <title>Re: Which pins to use?</title>
      <link>https://community.nxp.com/t5/University-Programs/Which-pins-to-use/m-p/178979#M10</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PWMR and PWML.&amp;nbsp; So pins 15 and 16.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Nov 2012 22:50:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/Which-pins-to-use/m-p/178979#M10</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2012-11-26T22:50:36Z</dc:date>
    </item>
  </channel>
</rss>