<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LCD example project for Kwikstik won't run on device in University Programs</title>
    <link>https://community.nxp.com/t5/University-Programs/LCD-example-project-for-Kwikstik-won-t-run-on-device/m-p/212177#M40</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try running it out of FLASH instead of RAM.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(If you go into the properties of your project under C/C++ build there is a drop-down to change the configuration.)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Jan 2013 15:41:10 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2013-01-03T15:41:10Z</dc:date>
    <item>
      <title>LCD example project for Kwikstik won't run on device</title>
      <link>https://community.nxp.com/t5/University-Programs/LCD-example-project-for-Kwikstik-won-t-run-on-device/m-p/212176#M39</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried downloading the LCD_Example project from &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-1057"&gt;KWIKSTIK-K40&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The project compiles, but when I try to run it on the Kwikstik, I get the following error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Error launching LCD_Example_MK40X256VMD100_INTERNAL_RAM_Segger J-Link, Could not open memory configuration file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a Kwikstik (onboard MCU appears to be PK40X256VLQ100). The project uses the MK40X256VMD100.h header file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know where I would find the memory configuration file. Codewarrior's built in help tool and google searching have been useless so far. I'm a bit of a newbie to this, so help would be appreciated.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Dec 2012 19:26:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/LCD-example-project-for-Kwikstik-won-t-run-on-device/m-p/212176#M39</guid>
      <dc:creator>dividebyzero</dc:creator>
      <dc:date>2012-12-18T19:26:42Z</dc:date>
    </item>
    <item>
      <title>Re: LCD example project for Kwikstik won't run on device</title>
      <link>https://community.nxp.com/t5/University-Programs/LCD-example-project-for-Kwikstik-won-t-run-on-device/m-p/212177#M40</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try running it out of FLASH instead of RAM.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(If you go into the properties of your project under C/C++ build there is a drop-down to change the configuration.)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jan 2013 15:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/LCD-example-project-for-Kwikstik-won-t-run-on-device/m-p/212177#M40</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2013-01-03T15:41:10Z</dc:date>
    </item>
    <item>
      <title>Re: LCD example project for Kwikstik won't run on device</title>
      <link>https://community.nxp.com/t5/University-Programs/LCD-example-project-for-Kwikstik-won-t-run-on-device/m-p/212178#M41</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry, I figured it out a while ago. I forgot to update this question with my solution. For some reason when I imported the project, it was set up to use the P&amp;amp;E programmer. If I manually changed config to J-Link, it wouldn't setup correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just created a new project, selected J-link in the project setup wizard, and then copied all the code over. It then worked.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jan 2013 17:55:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/LCD-example-project-for-Kwikstik-won-t-run-on-device/m-p/212178#M41</guid>
      <dc:creator>dividebyzero</dc:creator>
      <dc:date>2013-01-03T17:55:03Z</dc:date>
    </item>
  </channel>
</rss>