<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>University Programs中的主题 Is it possible to design a system which measures SPO2 and provides necessary data to control a stepper motor using only these two Dev Kits MED-SPO2 and TWR-S08MM128</title>
    <link>https://community.nxp.com/t5/University-Programs/Is-it-possible-to-design-a-system-which-measures-SPO2-and/m-p/489915#M391</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp; this is Shivakumar a final year B Tech Student. I have planned to do a project on automatic oxygen regulator using pulse oximeter. I have decided to do this project using your Dev Kits i.e MED-SPO2: Pulse Oximeter Development Kit and TWR-S08MM128: MC9S08MM Medical Development Tower System Module.&amp;nbsp; So would you please&amp;nbsp; clarify the following query.&amp;nbsp; 1)Is it possible to design a system which measures SPO2 and provides necessary data to control a stepper motor using only these two Dev Kits MED-SPO2 and TWR-S08MM128&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Jan 2016 15:35:56 GMT</pubDate>
    <dc:creator>shivakumardindu</dc:creator>
    <dc:date>2016-01-15T15:35:56Z</dc:date>
    <item>
      <title>Is it possible to design a system which measures SPO2 and provides necessary data to control a stepper motor using only these two Dev Kits MED-SPO2 and TWR-S08MM128</title>
      <link>https://community.nxp.com/t5/University-Programs/Is-it-possible-to-design-a-system-which-measures-SPO2-and/m-p/489915#M391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp; this is Shivakumar a final year B Tech Student. I have planned to do a project on automatic oxygen regulator using pulse oximeter. I have decided to do this project using your Dev Kits i.e MED-SPO2: Pulse Oximeter Development Kit and TWR-S08MM128: MC9S08MM Medical Development Tower System Module.&amp;nbsp; So would you please&amp;nbsp; clarify the following query.&amp;nbsp; 1)Is it possible to design a system which measures SPO2 and provides necessary data to control a stepper motor using only these two Dev Kits MED-SPO2 and TWR-S08MM128&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2016 15:35:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/Is-it-possible-to-design-a-system-which-measures-SPO2-and/m-p/489915#M391</guid>
      <dc:creator>shivakumardindu</dc:creator>
      <dc:date>2016-01-15T15:35:56Z</dc:date>
    </item>
  </channel>
</rss>