<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I want to know how to use the IFB pin in the TFC-shield. in University Programs</title>
    <link>https://community.nxp.com/t5/University-Programs/I-want-to-know-how-to-use-the-IFB-pin-in-the-TFC-shield/m-p/420729#M367</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to control the DC motor through the TFC-shield. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the TFC-shield, there is a IFB pin (as I know, This pin represent the armature current&amp;nbsp; over 375 . am I right?) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is my questions,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Can I&amp;nbsp; PID control the DC motor with just known about armature current?&amp;nbsp; I have to measure the angular velocity of the tire as far as I know .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; because armature current and angular velocity are not simply related. so In my opinion It is hard to control the DC motor using armature current .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&amp;nbsp; If I can, then how to use this..?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 May 2015 16:36:22 GMT</pubDate>
    <dc:creator>jeonghwanchoi</dc:creator>
    <dc:date>2015-05-11T16:36:22Z</dc:date>
    <item>
      <title>I want to know how to use the IFB pin in the TFC-shield.</title>
      <link>https://community.nxp.com/t5/University-Programs/I-want-to-know-how-to-use-the-IFB-pin-in-the-TFC-shield/m-p/420729#M367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to control the DC motor through the TFC-shield. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the TFC-shield, there is a IFB pin (as I know, This pin represent the armature current&amp;nbsp; over 375 . am I right?) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is my questions,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Can I&amp;nbsp; PID control the DC motor with just known about armature current?&amp;nbsp; I have to measure the angular velocity of the tire as far as I know .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; because armature current and angular velocity are not simply related. so In my opinion It is hard to control the DC motor using armature current .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&amp;nbsp; If I can, then how to use this..?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 May 2015 16:36:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/I-want-to-know-how-to-use-the-IFB-pin-in-the-TFC-shield/m-p/420729#M367</guid>
      <dc:creator>jeonghwanchoi</dc:creator>
      <dc:date>2015-05-11T16:36:22Z</dc:date>
    </item>
    <item>
      <title>Re: I want to know how to use the IFB pin in the TFC-shield.</title>
      <link>https://community.nxp.com/t5/University-Programs/I-want-to-know-how-to-use-the-IFB-pin-in-the-TFC-shield/m-p/420730#M368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/GregoryCAMUZAT"&gt;GregoryCAMUZAT&lt;/A&gt;​ &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/johnmc(test)"&gt;johnmc(test)&lt;/A&gt; any idea about this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2015 11:40:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/I-want-to-know-how-to-use-the-IFB-pin-in-the-TFC-shield/m-p/420730#M368</guid>
      <dc:creator>FlavioStiffan</dc:creator>
      <dc:date>2015-07-21T11:40:20Z</dc:date>
    </item>
    <item>
      <title>Re: I want to know how to use the IFB pin in the TFC-shield.</title>
      <link>https://community.nxp.com/t5/University-Programs/I-want-to-know-how-to-use-the-IFB-pin-in-the-TFC-shield/m-p/420731#M369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I believe that is a current feedback pin. According to the datasheet: "The load current feedback output provides ground referenced 0.24% of the high side output current. (Tie to GND through a resistor if not used.)"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could measure the current through each motor with this pin, but I don't think that is very useful in controlling the motor--a speed sensor on the wheels is probably more useful. The schematics for the board are here: &lt;A _jive_internal="true" href="https://community.nxp.com/servlet/JiveServlet/download/93914-26-257650/FRDM-TFC-REVB-BUILD_PACKAGE.zip" title="https://community.freescale.com/servlet/JiveServlet/download/93914-26-257650/FRDM-TFC-REVB-BUILD_PACKAGE.zip"&gt;https://community.freescale.com/servlet/JiveServlet/download/93914-26-257650/FRDM-TFC-REVB-BUILD_PACKAGE.zip&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From that, you will see that you enable the H-bridge thru H-Bridge-Enable connected to PTE21 and control the speeds of each motor by applying PWM to H-Bridge-A-IN1/2 (PTC3 and PTC4) and H-Bridge-B-IN1/2 (PTC1 and PTC2).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Good Luck!&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2015 22:33:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/I-want-to-know-how-to-use-the-IFB-pin-in-the-TFC-shield/m-p/420731#M369</guid>
      <dc:creator>bobapplonie</dc:creator>
      <dc:date>2015-07-23T22:33:59Z</dc:date>
    </item>
  </channel>
</rss>