<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>University ProgramsのトピックRe: Servo to tie rod assembly question</title>
    <link>https://community.nxp.com/t5/University-Programs/Servo-to-tie-rod-assembly-question/m-p/280560#M209</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ok. Thx. I suppose I could instead use the "sink" screws that are shorter. And just not use the washer and nut.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Aug 2013 20:40:29 GMT</pubDate>
    <dc:creator>jefff</dc:creator>
    <dc:date>2013-08-28T20:40:29Z</dc:date>
    <item>
      <title>Servo to tie rod assembly question</title>
      <link>https://community.nxp.com/t5/University-Programs/Servo-to-tie-rod-assembly-question/m-p/280558#M207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The diagram that shows how the servo is connected to the tie rods is hard to see. See the attachment below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Image08282013151036.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40608iB25206AFEB017E1C/image-size/large?v=v2&amp;amp;px=999" role="button" title="Image08282013151036.jpg" alt="Image08282013151036.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The screws don't interfere with the turns, but it is sure close. Seems like it should use shorter screws. And I can't tell whether the washer goes near the nut, between the plastic and the tie rod, or under the head of the screw. Anyone know?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2013 20:29:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/Servo-to-tie-rod-assembly-question/m-p/280558#M207</guid>
      <dc:creator>jefff</dc:creator>
      <dc:date>2013-08-28T20:29:54Z</dc:date>
    </item>
    <item>
      <title>Re: Servo to tie rod assembly question</title>
      <link>https://community.nxp.com/t5/University-Programs/Servo-to-tie-rod-assembly-question/m-p/280559#M208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used short screws that fit tightly into the plastic of the horn; they were in the packet of hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I didn't use any washers at all between the ball and the horn - the tie rod end moved freely on the ball.&amp;nbsp; But now that I think about it, a washer on the screw side to keep the tie rod end over the ball is probably not a bad idea.&amp;nbsp; When I assembled it, it looked like one side of the rod end was slightly smaller than the other, so that is the side I put towards the horn. The larger opening faces the screw's head.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd thought about doing some photos during assembly since I have all the equipment for making nice product shots but I was too excited and impatient to get it built to stop and set all the lighting up to do it... *sigh*&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2013 20:35:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/Servo-to-tie-rod-assembly-question/m-p/280559#M208</guid>
      <dc:creator>david_dicarlo</dc:creator>
      <dc:date>2013-08-28T20:35:45Z</dc:date>
    </item>
    <item>
      <title>Re: Servo to tie rod assembly question</title>
      <link>https://community.nxp.com/t5/University-Programs/Servo-to-tie-rod-assembly-question/m-p/280560#M209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ok. Thx. I suppose I could instead use the "sink" screws that are shorter. And just not use the washer and nut.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2013 20:40:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/Servo-to-tie-rod-assembly-question/m-p/280560#M209</guid>
      <dc:creator>jefff</dc:creator>
      <dc:date>2013-08-28T20:40:29Z</dc:date>
    </item>
    <item>
      <title>Re: Servo to tie rod assembly question</title>
      <link>https://community.nxp.com/t5/University-Programs/Servo-to-tie-rod-assembly-question/m-p/280561#M210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To further elaborate on David's response.&amp;nbsp; Engineering is allowed. ;-) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My various pictures, videos are only to serve as examples. There are lots of extra parts in the kit plus whatever you have in the tool shed.&amp;nbsp; It is all fair game.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2013 20:40:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/Servo-to-tie-rod-assembly-question/m-p/280561#M210</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2013-08-28T20:40:47Z</dc:date>
    </item>
    <item>
      <title>Re: Servo to tie rod assembly question</title>
      <link>https://community.nxp.com/t5/University-Programs/Servo-to-tie-rod-assembly-question/m-p/280562#M211</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That said, there did seem to be a particular order that worked better for the assembly and adjustment of the steering linkages than the others I tried... It took many more iterations of spinning the tie rod ends on than I expected to get servo horn standing vertical with the wheels pointing straight ahead.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2013 20:51:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/Servo-to-tie-rod-assembly-question/m-p/280562#M211</guid>
      <dc:creator>david_dicarlo</dc:creator>
      <dc:date>2013-08-28T20:51:46Z</dc:date>
    </item>
  </channel>
</rss>