<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How can I connect line scan camera with TWR-K40X256? in University Programs</title>
    <link>https://community.nxp.com/t5/University-Programs/How-can-I-connect-line-scan-camera-with-TWR-K40X256/m-p/278819#M186</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you are using the Tower system you are going to have to do a little wiring.&amp;nbsp; There are two ideal spots you can tap into the Tower board.&amp;nbsp; First, on the side of the TWR-ELEV are some headers that are good spots.&amp;nbsp; The other option is to get a TWR-PROTO board and use that.&amp;nbsp; (Requires some soldering.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the where exactly to connect.&amp;nbsp; That is really arbitrary.&amp;nbsp; There are many pins on an MCU that do the same thing.&amp;nbsp; CLK and SI need to be connected to a timer pin (FTM).&amp;nbsp; AOUT needs to be connected to an Analog to Digital pin (A2D).&amp;nbsp; GND is ground and VDD is 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is not exactly the same board but contain some really useful videos great for a newbie that might help:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-93960"&gt;https://community.freescale.com/docs/DOC-93960&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-93903" style="font-size: 10pt; line-height: 1.5em;"&gt;https://community.freescale.com/docs/DOC-93903&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Jun 2013 14:52:46 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2013-06-06T14:52:46Z</dc:date>
    <item>
      <title>How can I connect line scan camera with TWR-K40X256?</title>
      <link>https://community.nxp.com/t5/University-Programs/How-can-I-connect-line-scan-camera-with-TWR-K40X256/m-p/278818#M185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;Hi,&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt; I am new to programming TWR-K40X256 and wanted to participate in freescale cup competition. I want to connect line scan camera with &lt;SPAN style="font-style: inherit; color: #3778c7; text-decoration: underline;"&gt;TWR-K40X256.&lt;/SPAN&gt;I have two elevator modules, one serial module and line scan camera. Do I need additional board to connect the camera with &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;TWR-K40X256 &lt;/SPAN&gt;board? Where exactly do I have to connect the connector(CLK, SI, AOUT, GND and VDD) from camera? &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;The details of the camera can be found here:&amp;nbsp; &lt;/SPAN&gt;&lt;A _jive_internal="true" data-containerid="2003" data-containertype="14" data-objectid="1058" data-objecttype="102" href="https://community.nxp.com/docs/DOC-1058" style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff; color: #3778c7; text-decoration: underline;"&gt;Line Scan Camera Board&lt;/A&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jun 2013 14:22:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/How-can-I-connect-line-scan-camera-with-TWR-K40X256/m-p/278818#M185</guid>
      <dc:creator>tolera</dc:creator>
      <dc:date>2013-06-06T14:22:54Z</dc:date>
    </item>
    <item>
      <title>Re: How can I connect line scan camera with TWR-K40X256?</title>
      <link>https://community.nxp.com/t5/University-Programs/How-can-I-connect-line-scan-camera-with-TWR-K40X256/m-p/278819#M186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you are using the Tower system you are going to have to do a little wiring.&amp;nbsp; There are two ideal spots you can tap into the Tower board.&amp;nbsp; First, on the side of the TWR-ELEV are some headers that are good spots.&amp;nbsp; The other option is to get a TWR-PROTO board and use that.&amp;nbsp; (Requires some soldering.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the where exactly to connect.&amp;nbsp; That is really arbitrary.&amp;nbsp; There are many pins on an MCU that do the same thing.&amp;nbsp; CLK and SI need to be connected to a timer pin (FTM).&amp;nbsp; AOUT needs to be connected to an Analog to Digital pin (A2D).&amp;nbsp; GND is ground and VDD is 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is not exactly the same board but contain some really useful videos great for a newbie that might help:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-93960"&gt;https://community.freescale.com/docs/DOC-93960&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-93903" style="font-size: 10pt; line-height: 1.5em;"&gt;https://community.freescale.com/docs/DOC-93903&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jun 2013 14:52:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/How-can-I-connect-line-scan-camera-with-TWR-K40X256/m-p/278819#M186</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2013-06-06T14:52:46Z</dc:date>
    </item>
    <item>
      <title>Re: How can I connect line scan camera with TWR-K40X256?</title>
      <link>https://community.nxp.com/t5/University-Programs/How-can-I-connect-line-scan-camera-with-TWR-K40X256/m-p/278820#M187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi John, I have discussed with my professor and he told me to use prototyping board. I have looked at the documents for TWR-PROTO and I think it needs soldering as you have said.&amp;nbsp; My question is now, is there any other board as can be seen on the attached picture to avoid soldering, as my professor is not happy about soldering?&lt;/P&gt;&lt;P&gt;Thanks&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/39556i52F4CEBFE3B4C416/image-size/large?v=v2&amp;amp;px=999" title="lfcar1.jpg" alt="lfcar1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2013 16:44:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/How-can-I-connect-line-scan-camera-with-TWR-K40X256/m-p/278820#M187</guid>
      <dc:creator>tolera</dc:creator>
      <dc:date>2013-06-11T16:44:44Z</dc:date>
    </item>
    <item>
      <title>Re: How can I connect line scan camera with TWR-K40X256?</title>
      <link>https://community.nxp.com/t5/University-Programs/How-can-I-connect-line-scan-camera-with-TWR-K40X256/m-p/278821#M188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No way around soldering if you are using the Tower kit.&amp;nbsp; If you look at your photo of the above the TWR-PROTO is that black board near the rear of the car.&amp;nbsp; That picture actually has a fair bit of custom work done.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want a solderless option I would suggest our newest kit, but it is based around the FRDM platform, not the Tower.&amp;nbsp; It eliminates a lot of the need for wiring.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You would only need two pieces to swap out of your existing kit.&amp;nbsp; Instead of the TWR-XXX you would use FRDM-KL25Z.&amp;nbsp; And instead of the blue rectangular motor control board you would plug the new &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-93914"&gt;FRDM motor control shield &lt;/A&gt;into it.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will put you in touch with your regional University Program contact to discuss further.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2013 15:10:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/How-can-I-connect-line-scan-camera-with-TWR-K40X256/m-p/278821#M188</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2013-06-12T15:10:53Z</dc:date>
    </item>
    <item>
      <title>Re: How can I connect line scan camera with TWR-K40X256?</title>
      <link>https://community.nxp.com/t5/University-Programs/How-can-I-connect-line-scan-camera-with-TWR-K40X256/m-p/278822#M189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks John again! Ok tell me contact address of the regional University Program.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2013 16:15:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/How-can-I-connect-line-scan-camera-with-TWR-K40X256/m-p/278822#M189</guid>
      <dc:creator>tolera</dc:creator>
      <dc:date>2013-06-12T16:15:57Z</dc:date>
    </item>
  </channel>
</rss>