<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>University ProgramsのトピックRe: MPC5604B interrupts</title>
    <link>https://community.nxp.com/t5/University-Programs/MPC5604B-interrupts/m-p/230927#M116</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The cookbook and the samples were the problem. The MPC5604B came in 2 revisions, and it seems that the hardware addresses on the bus have some differences.&lt;/P&gt;&lt;P&gt;The car shipped with a revision, but with code support for another, as in the used header with define constants for I/Os was for the other revision.&lt;/P&gt;&lt;P&gt;So for some I/Os worked perfectly since they were mapped the same, but other, like the interrupts registers, were mapped at a different addresses.&lt;/P&gt;&lt;P&gt;I accidentally found out when someone provided other example code for using other I/Os by using interrupts.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Jan 2015 12:19:52 GMT</pubDate>
    <dc:creator>catalinvasilef</dc:creator>
    <dc:date>2015-01-14T12:19:52Z</dc:date>
    <item>
      <title>MPC5604B interrupts</title>
      <link>https://community.nxp.com/t5/University-Programs/MPC5604B-interrupts/m-p/230923#M112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It's been some time since the 2 threads I've found here, related to MPC5604B interrupts, have been issued.&lt;/P&gt;&lt;P&gt;Has anyone successfully&amp;nbsp; used interrupts one this MCU ? If so, how? Can you provide some sample code?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2014 14:20:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/MPC5604B-interrupts/m-p/230923#M112</guid>
      <dc:creator>catalinvasile</dc:creator>
      <dc:date>2014-02-13T14:20:53Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604B interrupts</title>
      <link>https://community.nxp.com/t5/University-Programs/MPC5604B-interrupts/m-p/230924#M113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/michaelgoudey"&gt;michaelgoudey&lt;/A&gt; would you have any clue about this one?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 May 2014 12:55:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/MPC5604B-interrupts/m-p/230924#M113</guid>
      <dc:creator>FlavioStiffan</dc:creator>
      <dc:date>2014-05-20T12:55:35Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604B interrupts</title>
      <link>https://community.nxp.com/t5/University-Programs/MPC5604B-interrupts/m-p/230925#M114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/murraystewart-b04629"&gt;murraystewart-b04629&lt;/A&gt; maybe you have a clue about this. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 May 2014 13:19:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/MPC5604B-interrupts/m-p/230925#M114</guid>
      <dc:creator>FlavioStiffan</dc:creator>
      <dc:date>2014-05-20T13:19:59Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604B interrupts</title>
      <link>https://community.nxp.com/t5/University-Programs/MPC5604B-interrupts/m-p/230926#M115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Flavio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The original question is pretty old so I wonder if Catalin has already found sample code for interrupts on MPC5604B.&amp;nbsp; If the topic is still open, though, I'd probably first look at the Qorivva cookbook reference code.&amp;nbsp; There are both HW and SW vector mode examples included with the document, also known as AN2865.&amp;nbsp; Here are the links to the PDF and the ZIP file with examples.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://www.freescale.com/webapp/sps/download/license.jsp?colCode=AN2865SW&amp;amp;amp;location=null&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType"&gt;http://www.freescale.com/webapp/sps/download/license.jsp?colCode=AN2865SW&amp;amp;amp;location=null&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType&lt;/A&gt;=&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the format of this code is different than desired then there are examples included with CodeWarrior for MCU.&amp;nbsp; For example, CW MCU v10.5 includes examples for MPC5604P where the interrupt controller functions in the same fashion as MPC5604B.&amp;nbsp; Look under the following path within CodeWarrior:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;CodeWarrior&amp;gt;/MCU/CodeWarrior_Examples/Qorivva_Examples&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MPC5604P_INTC-HW-VLE&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MPC5604P_INTC-SW-VLE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are also examples included with the StarterTRAK development kit, such as TRK-MPC5606B, which may be suitable.&amp;nbsp; I haven't looked over those to confirm interrupts are used in each kit's example code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michael Goudey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 May 2014 21:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/MPC5604B-interrupts/m-p/230926#M115</guid>
      <dc:creator>michaelgoudey</dc:creator>
      <dc:date>2014-05-20T21:51:56Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5604B interrupts</title>
      <link>https://community.nxp.com/t5/University-Programs/MPC5604B-interrupts/m-p/230927#M116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The cookbook and the samples were the problem. The MPC5604B came in 2 revisions, and it seems that the hardware addresses on the bus have some differences.&lt;/P&gt;&lt;P&gt;The car shipped with a revision, but with code support for another, as in the used header with define constants for I/Os was for the other revision.&lt;/P&gt;&lt;P&gt;So for some I/Os worked perfectly since they were mapped the same, but other, like the interrupts registers, were mapped at a different addresses.&lt;/P&gt;&lt;P&gt;I accidentally found out when someone provided other example code for using other I/Os by using interrupts.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jan 2015 12:19:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/MPC5604B-interrupts/m-p/230927#M116</guid>
      <dc:creator>catalinvasilef</dc:creator>
      <dc:date>2015-01-14T12:19:52Z</dc:date>
    </item>
  </channel>
</rss>