<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>University Programsのトピックproblem with interface</title>
    <link>https://community.nxp.com/t5/University-Programs/problem-with-interface/m-p/221978#M101</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am using MPC5604B starter trak. I followed the installation instructions given in the corresponding pdf downloaded from the TFC 2012 website. i tried downloading the sample program given in the same website. when i choose Project---&amp;gt;Debug, as mentioned in the instuctions, i get 3 windows - code, status, cpu. but in addition to these, i'm getting a 4th window PEMICRO connection manager. in this window, if i give connect, i get a msg in the status window that "Device cannot be connected". &lt;/P&gt;&lt;P&gt;Also, in the hyperterminal, i chose COM1 and gave the values specified in the instructions. wat does this do with the kit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I could understand the sample program and i'm confident of doing the main program. but i couldn't understand the operation of the software with the kit while downloading.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I beg for some savior's help as i have not even downloaded a single program into the kit i received still. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Oct 2012 12:08:58 GMT</pubDate>
    <dc:creator>Vijayakrishna</dc:creator>
    <dc:date>2012-10-22T12:08:58Z</dc:date>
    <item>
      <title>problem with interface</title>
      <link>https://community.nxp.com/t5/University-Programs/problem-with-interface/m-p/221978#M101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am using MPC5604B starter trak. I followed the installation instructions given in the corresponding pdf downloaded from the TFC 2012 website. i tried downloading the sample program given in the same website. when i choose Project---&amp;gt;Debug, as mentioned in the instuctions, i get 3 windows - code, status, cpu. but in addition to these, i'm getting a 4th window PEMICRO connection manager. in this window, if i give connect, i get a msg in the status window that "Device cannot be connected". &lt;/P&gt;&lt;P&gt;Also, in the hyperterminal, i chose COM1 and gave the values specified in the instructions. wat does this do with the kit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I could understand the sample program and i'm confident of doing the main program. but i couldn't understand the operation of the software with the kit while downloading.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I beg for some savior's help as i have not even downloaded a single program into the kit i received still. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Oct 2012 12:08:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/problem-with-interface/m-p/221978#M101</guid>
      <dc:creator>Vijayakrishna</dc:creator>
      <dc:date>2012-10-22T12:08:58Z</dc:date>
    </item>
    <item>
      <title>Re: problem with interface</title>
      <link>https://community.nxp.com/t5/University-Programs/problem-with-interface/m-p/221979#M102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The hyperterminal bit is only available if you have populated the RS232 transceiver on the TRAK board.&amp;nbsp; You must modify the board before that bit of the software will work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the failure to launch the debugger, that is a pretty straightforward process.&amp;nbsp; I would suggest trying a different USB port so that it redetects all the drivers and let Windows configure.&amp;nbsp; When it's plugged into the USB you should be getting power to the board.&amp;nbsp; That's the first easy thing to check.&amp;nbsp; If you are not, go through the jumper configurations part of the directions again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Oct 2012 16:32:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/University-Programs/problem-with-interface/m-p/221979#M102</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2012-10-29T16:32:31Z</dc:date>
    </item>
  </channel>
</rss>