<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Connecting nor flash with t2080 processor in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/Connecting-nor-flash-with-t2080-processor/m-p/380995#M79</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, PowerPC and Power ISA architectures have a specific feature, Most Significant Bit (MSB) has index 0. So IFC_AD[0] is the MSB on the bus and it should be connected to MSB of the NOR flash, that is DQ[15]. This expalins "reversal" in connectivity on the IFC bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Feb 2015 06:24:24 GMT</pubDate>
    <dc:creator>Bulat</dc:creator>
    <dc:date>2015-02-18T06:24:24Z</dc:date>
    <item>
      <title>Connecting nor flash with t2080 processor</title>
      <link>https://community.nxp.com/t5/T-Series/Connecting-nor-flash-with-t2080-processor/m-p/380994#M78</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hai&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am using t2080 QorIQ Series processor in my design ,I found in the reference schematic that the flash chip connected to t2080 (data line0 is connected to data pin 15 of flash chip )&lt;/P&gt;&lt;P&gt;why is this reversal&amp;nbsp; in connectivity.Is there any specific reason ?&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;AGXIN.J&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Feb 2015 14:54:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Connecting-nor-flash-with-t2080-processor/m-p/380994#M78</guid>
      <dc:creator>agxinj</dc:creator>
      <dc:date>2015-02-17T14:54:34Z</dc:date>
    </item>
    <item>
      <title>Re: Connecting nor flash with t2080 processor</title>
      <link>https://community.nxp.com/t5/T-Series/Connecting-nor-flash-with-t2080-processor/m-p/380995#M79</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, PowerPC and Power ISA architectures have a specific feature, Most Significant Bit (MSB) has index 0. So IFC_AD[0] is the MSB on the bus and it should be connected to MSB of the NOR flash, that is DQ[15]. This expalins "reversal" in connectivity on the IFC bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Feb 2015 06:24:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Connecting-nor-flash-with-t2080-processor/m-p/380995#M79</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2015-02-18T06:24:24Z</dc:date>
    </item>
  </channel>
</rss>