<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic T4240rdb network performance issue in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T4240rdb-network-performance-issue/m-p/493374#M773</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;I got inconsistent ipsec null performance results while&amp;nbsp; using t4240rdb board with dpaa ports fman1 and fman2. I have two t4240rdb boards using kernel, dtb, filesystem taken from sdk 1.6. &lt;/P&gt;&lt;P&gt;I use ixia&amp;nbsp; to&amp;nbsp; generate packets. While I am sending packets at a rate of % 100 only in one direction the performance is 400mbps.But while I inject packets at a rate of % 100 in both direction i got 300mbps as an aggregate performance. Why the aggregate performance is not around 2×400 mbps on such a high performance board. I couldnt even reach 400mbps.&lt;/P&gt;&lt;P&gt;After conducting some tests I reached&amp;nbsp; an&amp;nbsp; interesting result. If I decrease the traffic rate near % 60 I got an aggregate 2×420 mbps performance. And&amp;nbsp;&amp;nbsp; I&amp;nbsp; observed the performance is starting to decrease if the packet drops started. I couldn't explain why the performance is dramatically decreasing if I exceed a traffic rate % 60. As if there is a rate control mechanism which limits the total packet throughput. Any help will be appreciated. &lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Jan 2016 19:05:16 GMT</pubDate>
    <dc:creator>sedat_altun</dc:creator>
    <dc:date>2016-01-15T19:05:16Z</dc:date>
    <item>
      <title>T4240rdb network performance issue</title>
      <link>https://community.nxp.com/t5/T-Series/T4240rdb-network-performance-issue/m-p/493374#M773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;I got inconsistent ipsec null performance results while&amp;nbsp; using t4240rdb board with dpaa ports fman1 and fman2. I have two t4240rdb boards using kernel, dtb, filesystem taken from sdk 1.6. &lt;/P&gt;&lt;P&gt;I use ixia&amp;nbsp; to&amp;nbsp; generate packets. While I am sending packets at a rate of % 100 only in one direction the performance is 400mbps.But while I inject packets at a rate of % 100 in both direction i got 300mbps as an aggregate performance. Why the aggregate performance is not around 2×400 mbps on such a high performance board. I couldnt even reach 400mbps.&lt;/P&gt;&lt;P&gt;After conducting some tests I reached&amp;nbsp; an&amp;nbsp; interesting result. If I decrease the traffic rate near % 60 I got an aggregate 2×420 mbps performance. And&amp;nbsp;&amp;nbsp; I&amp;nbsp; observed the performance is starting to decrease if the packet drops started. I couldn't explain why the performance is dramatically decreasing if I exceed a traffic rate % 60. As if there is a rate control mechanism which limits the total packet throughput. Any help will be appreciated. &lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2016 19:05:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240rdb-network-performance-issue/m-p/493374#M773</guid>
      <dc:creator>sedat_altun</dc:creator>
      <dc:date>2016-01-15T19:05:16Z</dc:date>
    </item>
    <item>
      <title>Re: T4240rdb network performance issue</title>
      <link>https://community.nxp.com/t5/T-Series/T4240rdb-network-performance-issue/m-p/493375#M774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There must be something not configured properly. Suggestions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Use the most recent SDK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Follow the recommendations at the link below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK_1.9/GUID-15BE1669-CD22-45D9-B703-6E12E5D466A7" title="https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK_1.9/GUID-15BE1669-CD22-45D9-B703-6E12E5D466A7"&gt;https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK_1.9/GUID-15BE1669-CD22-45D9-B703-6E12E5D466A7&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 12:50:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240rdb-network-performance-issue/m-p/493375#M774</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2016-01-18T12:50:53Z</dc:date>
    </item>
    <item>
      <title>Re: T4240rdb network performance issue</title>
      <link>https://community.nxp.com/t5/T-Series/T4240rdb-network-performance-issue/m-p/493376#M775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your response,&lt;/P&gt;&lt;P&gt;I also tried most recent SDK but nothing changed. &lt;/P&gt;&lt;P&gt;It maybe due to traffic shaping or policing configuration of the t4240.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 20:44:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240rdb-network-performance-issue/m-p/493376#M775</guid>
      <dc:creator>sedat_altun</dc:creator>
      <dc:date>2016-01-20T20:44:11Z</dc:date>
    </item>
  </channel>
</rss>