<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic QorIQ T1040 weak pull-up value in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/QorIQ-T1040-weak-pull-up-value/m-p/480715#M635</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;T1040 Data Sheet says that some pins have a weak (~20 kΩ) internal pull-up P-FET.&lt;/P&gt;&lt;P&gt;What is the minimum and maximum values of resistance (and/or current) of these pull-ups through the full PVT range?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Denis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Apr 2016 11:32:13 GMT</pubDate>
    <dc:creator>fdm</dc:creator>
    <dc:date>2016-04-05T11:32:13Z</dc:date>
    <item>
      <title>QorIQ T1040 weak pull-up value</title>
      <link>https://community.nxp.com/t5/T-Series/QorIQ-T1040-weak-pull-up-value/m-p/480715#M635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;T1040 Data Sheet says that some pins have a weak (~20 kΩ) internal pull-up P-FET.&lt;/P&gt;&lt;P&gt;What is the minimum and maximum values of resistance (and/or current) of these pull-ups through the full PVT range?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Denis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 11:32:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/QorIQ-T1040-weak-pull-up-value/m-p/480715#M635</guid>
      <dc:creator>fdm</dc:creator>
      <dc:date>2016-04-05T11:32:13Z</dc:date>
    </item>
    <item>
      <title>Re: QorIQ T1040 weak pull-up value</title>
      <link>https://community.nxp.com/t5/T-Series/QorIQ-T1040-weak-pull-up-value/m-p/480716#M636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;T1040 Data Sheet also says “This pull-up is designed such that it can be overpowered by an external 4.7 k resistor. However, if the signal is intended to be high after reset, and if there is any device on the net that might pull down the value of the net at reset, a pull-up or active driver is needed”&lt;/P&gt;&lt;P&gt;I.e. if the cfg pin will not open the datasheet Require for an external pull-up or active driver. So actual characteristic of the internal pull-up is 4.7k value for external pull-down. They guaranteed that 4.7k pull-down sets the cfg pin to '0', while open cfg pin will have the high level '1'.&lt;/P&gt;&lt;P&gt;I think your question is a question for design group. At least I've never seen such data. Here just some speculations:&lt;/P&gt;&lt;P&gt;* For low level threshold ViL= 0.54V at 1.8V, neglecting by input current we get that weak pull-up has to be greater than 11 k&amp;nbsp;&amp;nbsp; { 1.8*4.7/(4.7+11)=0.539 }.&lt;/P&gt;&lt;P&gt;* If we consider input as&amp;nbsp; 2 resistors of 36k connected to the gnd and 1.8V for the max input current -\+ 50uA (specified in the data sheet) then we get that the weak pull-up has to be less than 36k in order to reach Vih=1.2V at 1.8V {1.8*36/(36/2+36)=1.2&amp;nbsp; }.&amp;nbsp; If we take 50uA as input current at 1.2V than we get that pull-up has to be less than 12k&amp;nbsp;&amp;nbsp; {(1.8-1.2)/0.05=12} which I consider as unrealistic.&lt;/P&gt;&lt;P&gt;So ~20k is good value for the internal pull-up which should be inside 15k - 35 k&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Apr 2016 10:12:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/QorIQ-T1040-weak-pull-up-value/m-p/480716#M636</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2016-04-06T10:12:46Z</dc:date>
    </item>
  </channel>
</rss>