<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NXP T2080 Build for Little endian in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/NXP-T2080-Build-for-Little-endian/m-p/2371636#M5427</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I am using the T2080 board with a BSP built in big-endian mode, but I need to build it for little-endian mode. Is there any ready-made BSP available for little-endian mode, or any documentation available for building little-endian Linux on the T2080 board?&lt;/P&gt;</description>
    <pubDate>Wed, 27 May 2026 04:25:58 GMT</pubDate>
    <dc:creator>Ganesh3955</dc:creator>
    <dc:date>2026-05-27T04:25:58Z</dc:date>
    <item>
      <title>NXP T2080 Build for Little endian</title>
      <link>https://community.nxp.com/t5/T-Series/NXP-T2080-Build-for-Little-endian/m-p/2371636#M5427</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I am using the T2080 board with a BSP built in big-endian mode, but I need to build it for little-endian mode. Is there any ready-made BSP available for little-endian mode, or any documentation available for building little-endian Linux on the T2080 board?&lt;/P&gt;</description>
      <pubDate>Wed, 27 May 2026 04:25:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/NXP-T2080-Build-for-Little-endian/m-p/2371636#M5427</guid>
      <dc:creator>Ganesh3955</dc:creator>
      <dc:date>2026-05-27T04:25:58Z</dc:date>
    </item>
    <item>
      <title>Re: NXP T2080 Build for Little endian</title>
      <link>https://community.nxp.com/t5/T-Series/NXP-T2080-Build-for-Little-endian/m-p/2372288#M5430</link>
      <description>&lt;P&gt;T2080 NXP BSPs support only big-endian mode.&lt;/P&gt;
&lt;P&gt;Little-endian kernel building and its further operation was not tested.&lt;/P&gt;</description>
      <pubDate>Thu, 28 May 2026 07:46:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/NXP-T2080-Build-for-Little-endian/m-p/2372288#M5430</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2026-05-28T07:46:34Z</dc:date>
    </item>
  </channel>
</rss>