<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Seriesのトピックfailed to send message 100 ret is 0 while loading AMDGPU</title>
    <link>https://community.nxp.com/t5/T-Series/failed-to-send-message-100-ret-is-0-while-loading-AMDGPU/m-p/2364970#M5406</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;While loading AMDGPU driver in T1040 board , i&amp;nbsp; getting following error, what could be the issue here&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;root@t1042d4rdb:~# insmod /amdgpu.ko&lt;BR /&gt;[drm] amdgpu kernel modesetting enabled.&lt;BR /&gt;amdgpu 0001:01:00.0: enabling device (0006 -&amp;gt; 0007)&lt;BR /&gt;[drm] initializing kernel modesetting (POLARIS12 0x1002:0x6987 0x1787:0x2389 0x80).&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: Trusted Memory Zone (TMZ) feature not supported&lt;BR /&gt;[drm] register mmio base: 0xA0000000&lt;BR /&gt;[drm] register mmio size: 262144&lt;BR /&gt;[drm] PCIE atomic ops is not supported&lt;BR /&gt;[drm] add ip block number 0 &amp;lt;vi_common&amp;gt;&lt;BR /&gt;[drm] add ip block number 1 &amp;lt;gmc_v8_0&amp;gt;&lt;BR /&gt;[drm] add ip block number 2 &amp;lt;tonga_ih&amp;gt;&lt;BR /&gt;[drm] add ip block number 3 &amp;lt;gfx_v8_0&amp;gt;&lt;BR /&gt;[drm] add ip block number 4 &amp;lt;sdma_v3_0&amp;gt;&lt;BR /&gt;[drm] add ip block number 5 &amp;lt;powerplay&amp;gt;&lt;BR /&gt;[drm] add ip block number 6 &amp;lt;dm&amp;gt;&lt;BR /&gt;[drm] add ip block number 7 &amp;lt;uvd_v6_0&amp;gt;&lt;BR /&gt;[drm] add ip block number 8 &amp;lt;vce_v3_0&amp;gt;&lt;BR /&gt;[drm:.check_atom_bios [amdgpu]] ATOMBIOS detected&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: Fetched VBIOS from ROM BAR&lt;BR /&gt;amdgpu: ATOM BIOS: 113-ER16BFE-001&lt;BR /&gt;[drm:.amdgpu_atombios_init [amdgpu]] atom firmware requested 00000000 0kb&lt;BR /&gt;[drm] UVD is enabled in VM mode&lt;BR /&gt;[drm] UVD ENC is enabled in VM mode&lt;BR /&gt;[drm] VCE enabled in VM mode&lt;BR /&gt;[drm] GPU posting now...&lt;BR /&gt;[drm] vm size is 64 GB, 2 levels, block size is 10-bit, fragment size is 9-bit&lt;BR /&gt;[drm:.gmc_v8_0_sw_init [amdgpu]]&lt;BR /&gt;amdgpu 0001:01:00.0: BAR 2: releasing [mem 0xd10000000-0xd101fffff 64bit pref]&lt;BR /&gt;amdgpu 0001:01:00.0: BAR 0: releasing [mem 0xd00000000-0xd0fffffff 64bit pref]&lt;BR /&gt;pcieport 0001:00:00.0: BAR 9: releasing [mem 0xd00000000-0xeffffffff 64bit pref]&lt;BR /&gt;pcieport 0001:00:00.0: BAR 9: assigned [mem 0xd00000000-0xe7fffffff 64bit pref]&lt;BR /&gt;amdgpu 0001:01:00.0: BAR 0: assigned [mem 0xd00000000-0xdffffffff 64bit pref]&lt;BR /&gt;amdgpu 0001:01:00.0: BAR 2: assigned [mem 0xe00000000-0xe001fffff 64bit pref]&lt;BR /&gt;pcieport 0001:00:00.0: PCI bridge to [bus 01]&lt;BR /&gt;pcieport 0001:00:00.0: bridge window [io 0x8000080000010000-0x800008000001ffff]&lt;BR /&gt;pcieport 0001:00:00.0: bridge window [mem 0xa0000000-0xafffffff]&lt;BR /&gt;pcieport 0001:00:00.0: bridge window [mem 0xd00000000-0xe7fffffff 64bit pref]&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: VRAM: 4096M 0x000000F400000000 - 0x000000F4FFFFFFFF (4096M used)&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: GART: 256M 0x000000FF00000000 - 0x000000FF0FFFFFFF&lt;BR /&gt;[drm] Detected VRAM RAM=4096M, BAR=4096M&lt;BR /&gt;[drm] RAM width 128bits GDDR5&lt;BR /&gt;[drm] amdgpu: 4096M of VRAM memory ready&lt;BR /&gt;[drm] amdgpu: 1457M of GTT memory ready.&lt;BR /&gt;[drm] GART: num cpu pages 65536, num gpu pages 65536&lt;BR /&gt;[drm:.amdgpu_ucode_print_mc_hdr [amdgpu]] MC&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] size_bytes: 32608&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] header_size_bytes: 40&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] header_version_major: 1&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] header_version_minor: 0&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ip_version_major: 8&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ip_version_minor: 1&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ucode_version: 0x00b4dc50&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ucode_size_bytes: 32160&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ucode_array_offset_bytes: 448&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] crc32: 0x9b1e395c&lt;BR /&gt;[drm:.amdgpu_ucode_print_mc_hdr [amdgpu]] io_debug_size_bytes: 192&lt;BR /&gt;[drm:.amdgpu_ucode_print_mc_hdr [amdgpu]] io_debug_array_offset_bytes: 256&lt;BR /&gt;[drm] PCIE GART of 256M enabled (table at 0x000000F400000000).&lt;BR /&gt;[drm:.amdgpu_irq_init [amdgpu]] amdgpu: irq initialized.&lt;BR /&gt;[drm:.gfx_v8_0_sw_init [amdgpu]]&lt;BR /&gt;[drm] Chained IB support enabled!&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring gfx use gpu addr 0x000000ff00400040&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.0.0 use gpu addr 0x000000ff004000e0&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.1.0 use gpu addr 0x000000ff00400180&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.2.0 use gpu addr 0x000000ff00400220&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.3.0 use gpu addr 0x000000ff004002c0&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.0.1 use gpu addr 0x000000ff00400360&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.1.1 use gpu addr 0x000000ff00400400&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.2.1 use gpu addr 0x000000ff004004a0&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.3.1 use gpu addr 0x000000ff00400540&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring kiq_2.1.0 use gpu addr 0x000000ff004005e0&lt;BR /&gt;[drm:.sdma_v3_0_sw_init [amdgpu]]&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring sdma0 use gpu addr 0x000000ff00400680&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring sdma1 use gpu addr 0x000000ff00400720&lt;BR /&gt;amdgpu: hwmgr_sw_init smu backed is polaris10_smu&lt;BR /&gt;[drm] Found UVD firmware Version: 1.130 Family ID: 16&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring uvd use gpu addr 0x000000f4001afa80&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring uvd_enc0 use gpu addr 0x000000ff00400860&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring uvd_enc1 use gpu addr 0x000000ff00400900&lt;BR /&gt;[drm] Found VCE firmware Version: 53.26 Binary ID: 3&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring vce0 use gpu addr 0x000000ff004009a0&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring vce1 use gpu addr 0x000000ff00400a40&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring vce2 use gpu addr 0x000000ff00400ae0&lt;BR /&gt;[drm:.amdgpu_ucode_print_smc_hdr [amdgpu]] SMC&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] size_bytes: 130388&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] header_size_bytes: 36&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] header_version_major: 1&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] header_version_minor: 0&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ip_version_major: 7&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ip_version_minor: 2&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ucode_version: 0x00221700&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ucode_size_bytes: 130132&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ucode_array_offset_bytes: 256&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] crc32: 0xae2b3b78&lt;BR /&gt;[drm:.amdgpu_ucode_print_smc_hdr [amdgpu]] ucode_start_addr: 131072&lt;BR /&gt;amdgpu:&lt;BR /&gt;failed to send message 100 ret is 0&lt;BR /&gt;amdgpu: SMU Firmware start failed!&lt;BR /&gt;amdgpu: Failed to load SMU ucode.&lt;BR /&gt;amdgpu: fw load failed&lt;BR /&gt;amdgpu: smu firmware loading failed&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: amdgpu_device_ip_init failed&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: Fatal error during GPU init&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: amdgpu: finishing device.&lt;BR /&gt;[drm:.gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2&lt;BR /&gt;[drm:.gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2&lt;BR /&gt;[drm:.gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2&lt;BR /&gt;[drm:.gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2&lt;BR /&gt;amdgpu: probe of 0001:01:00.0 failed with error -22&lt;BR /&gt;BUG: Unable to handle kernel data access on read at 0x8000080080954000&lt;BR /&gt;Faulting instruction address: 0xc000000000011870&lt;BR /&gt;Oops: Kernel access of bad area, sig: 11 [#1]&lt;BR /&gt;BE PAGE_SIZE=4K SMP NR_CPUS=24 CoreNet Generic&lt;BR /&gt;Modules linked in: amdgpu(+) backlight drm_ttm_helper ttm gpu_sched ucc_uart fsl_jr_uio&lt;BR /&gt;CPU: 2 PID: 816 Comm: insmod Not tainted 5.15.71+g95448dd0dc9b #1&lt;BR /&gt;**bleep**: c000000000011870 LR: 8000000000e0d120 CTR: 0000000000058400&lt;BR /&gt;REGS: c00000000a956d80 TRAP: 0300 Not tainted (5.15.71+g95448dd0dc9b)&lt;BR /&gt;MSR: 0000000080029002 &amp;lt;CE,EE,ME&amp;gt; CR: 22002228 XER: 00000000&lt;BR /&gt;DEAR: 8000080080954000 ESR: 0000000000000000 IRQMASK: 0&lt;BR /&gt;GPR00: 8000000000e0d100 c00000000a957020 c0000000013faa00 c00000000c000000&lt;BR /&gt;GPR04: 8000080080954000 00000000002c2000 00000000000b0800 000000007ecc9000&lt;BR /&gt;GPR08: 0000000000058400 8000080080954000 c00000000bfffffc 80000000010b76d8&lt;BR /&gt;GPR12: c0000000000117f4 c00000003ffff140 000000010b5456f0 000000010b4fa188&lt;BR /&gt;GPR16: 0000000000000000 000000010b545810 000000010b5202b0 0000000000000000&lt;BR /&gt;GPR20: 0000000000000000 0000000000000000 c00000000ae16a48 8000080080954000&lt;BR /&gt;GPR24: 00000000002c2000 0000000000000000 c00000000ae00010 0000000000000001&lt;BR /&gt;GPR28: c00000000ae00000 c00000000ae10000 0000000000000000 c00000000ae10000&lt;BR /&gt;**bleep** [c000000000011870] ._memcpy_fromio+0x7c/0x100&lt;BR /&gt;LR [8000000000e0d120] .amdgpu_uvd_suspend+0x1d4/0x268 [amdgpu]&lt;BR /&gt;Call Trace:&lt;BR /&gt;[c00000000a957020] [8000000000e0d100] .amdgpu_uvd_suspend+0x1b4/0x268 [amdgpu] (unreliable)&lt;BR /&gt;[c00000000a9570f0] [8000000000e1110c] .uvd_v6_0_sw_fini+0x1c/0xcc [amdgpu]&lt;BR /&gt;[c00000000a957180] [8000000000cf24b0] .amdgpu_device_fini_sw+0x124/0x378 [amdgpu]&lt;BR /&gt;[c00000000a957240] [8000000000cf9e0c] .amdgpu_driver_release_kms+0x1c/0x40 [amdgpu]&lt;BR /&gt;[c00000000a9572c0] [c000000000704380] .devm_drm_dev_init_release+0x78/0xcc&lt;BR /&gt;[c00000000a957340] [c000000000755248] .devm_action_release+0x28/0x3c&lt;BR /&gt;[c00000000a9573b0] [c00000000075576c] .release_nodes+0x78/0x108&lt;BR /&gt;[c00000000a957450] [c000000000757174] .devres_release_all+0xa8/0x11c&lt;BR /&gt;[c00000000a957510] [c00000000074f788] .really_probe.part.0+0x1b8/0x440&lt;BR /&gt;[c00000000a9575b0] [c00000000074fad8] .__driver_probe_device+0xc8/0x198&lt;BR /&gt;[c00000000a957640] [c00000000074fbf8] .driver_probe_device+0x50/0x16c&lt;BR /&gt;[c00000000a9576e0] [c00000000075055c] .__driver_attach+0xb4/0x200&lt;BR /&gt;[c00000000a957770] [c00000000074c518] .bus_for_each_dev+0x9c/0x110&lt;BR /&gt;[c00000000a957820] [c00000000074eca4] .driver_attach+0x24/0x38&lt;BR /&gt;[c00000000a957890] [c00000000074e4ec] .bus_add_driver+0x1d4/0x2a8&lt;BR /&gt;[c00000000a957940] [c00000000075107c] .driver_register+0xa4/0x194&lt;BR /&gt;[c00000000a9579c0] [c0000000006217ec] .__pci_register_driver+0x58/0x6c&lt;BR /&gt;[c00000000a957a30] [80000000010a9608] .amdgpu_init+0x74/0x94 [amdgpu]&lt;BR /&gt;[c00000000a957ab0] [c0000000000021cc] .do_one_initcall+0x6c/0x284&lt;BR /&gt;[c00000000a957b90] [c0000000001174a4] .do_init_module+0x5c/0x2bc&lt;BR /&gt;[c00000000a957c30] [c00000000011a980] .__do_sys_finit_module+0xc4/0x10c&lt;BR /&gt;[c00000000a957d60] [c000000000012454] .system_call_exception+0x11c/0x1c4&lt;BR /&gt;[c00000000a957e10] [c0000000000001f8] system_call_common+0xf0/0x210&lt;BR /&gt;--- interrupt: c00 at 0x3fffbe532ee4&lt;BR /&gt;**bleep**: 00003fffbe532ee4 LR: 00000001366cdbfc CTR: 0000000000000000&lt;BR /&gt;REGS: c00000000a957e80 TRAP: 0c00 Not tainted (5.15.71+g95448dd0dc9b)&lt;BR /&gt;MSR: 000000008002d002 &amp;lt;CE,EE,PR,ME&amp;gt; CR: 28002882 XER: 00000000&lt;BR /&gt;IRQMASK: 0&lt;BR /&gt;GPR00: 0000000000000161 00003fffd14f61a0 00003fffbe637200 0000000000000003&lt;BR /&gt;GPR04: 00000001366d9148 0000000000000000 0000000000000000 0000000000000000&lt;BR /&gt;GPR08: 0000000000000000 0000000000000000 0000000000000000 0000000000000000&lt;BR /&gt;GPR12: 0000000000000000 00003fffbe6cf810 000000010b5456f0 000000010b4fa188&lt;BR /&gt;GPR16: 0000000000000000 000000010b545810 000000010b5202b0 0000000000000000&lt;BR /&gt;GPR20: 0000000000000000 0000000000000000 0000000000000002 00003fffd14f6ee5&lt;BR /&gt;GPR24: 00003fffd14f6860 00000001366fd9e8 0000000000000000 00000001366fcbd0&lt;BR /&gt;GPR28: 00000001366d9148 0000000000000000 0000000000000000 0000000136701760&lt;BR /&gt;**bleep** [00003fffbe532ee4] 0x3fffbe532ee4&lt;BR /&gt;LR [00000001366cdbfc] 0x1366cdbfc&lt;BR /&gt;--- interrupt: c00&lt;BR /&gt;Instruction dump:&lt;BR /&gt;4e800020 28250003 40810068 3905fffc 7908f082 38c80001 70c90001 3943fffc&lt;BR /&gt;7c892378 40820070 78c8f842 7d0903a6 &amp;lt;80e90000&amp;gt; 390a0004 90ea0004 7c0006ac&lt;BR /&gt;---[ end trace e1f14bc598aaf8c6 ]---&lt;/P&gt;&lt;P&gt;Segmentation fault&lt;/P&gt;</description>
    <pubDate>Wed, 13 May 2026 15:03:43 GMT</pubDate>
    <dc:creator>Ganesh3955</dc:creator>
    <dc:date>2026-05-13T15:03:43Z</dc:date>
    <item>
      <title>failed to send message 100 ret is 0 while loading AMDGPU</title>
      <link>https://community.nxp.com/t5/T-Series/failed-to-send-message-100-ret-is-0-while-loading-AMDGPU/m-p/2364970#M5406</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;While loading AMDGPU driver in T1040 board , i&amp;nbsp; getting following error, what could be the issue here&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;root@t1042d4rdb:~# insmod /amdgpu.ko&lt;BR /&gt;[drm] amdgpu kernel modesetting enabled.&lt;BR /&gt;amdgpu 0001:01:00.0: enabling device (0006 -&amp;gt; 0007)&lt;BR /&gt;[drm] initializing kernel modesetting (POLARIS12 0x1002:0x6987 0x1787:0x2389 0x80).&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: Trusted Memory Zone (TMZ) feature not supported&lt;BR /&gt;[drm] register mmio base: 0xA0000000&lt;BR /&gt;[drm] register mmio size: 262144&lt;BR /&gt;[drm] PCIE atomic ops is not supported&lt;BR /&gt;[drm] add ip block number 0 &amp;lt;vi_common&amp;gt;&lt;BR /&gt;[drm] add ip block number 1 &amp;lt;gmc_v8_0&amp;gt;&lt;BR /&gt;[drm] add ip block number 2 &amp;lt;tonga_ih&amp;gt;&lt;BR /&gt;[drm] add ip block number 3 &amp;lt;gfx_v8_0&amp;gt;&lt;BR /&gt;[drm] add ip block number 4 &amp;lt;sdma_v3_0&amp;gt;&lt;BR /&gt;[drm] add ip block number 5 &amp;lt;powerplay&amp;gt;&lt;BR /&gt;[drm] add ip block number 6 &amp;lt;dm&amp;gt;&lt;BR /&gt;[drm] add ip block number 7 &amp;lt;uvd_v6_0&amp;gt;&lt;BR /&gt;[drm] add ip block number 8 &amp;lt;vce_v3_0&amp;gt;&lt;BR /&gt;[drm:.check_atom_bios [amdgpu]] ATOMBIOS detected&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: Fetched VBIOS from ROM BAR&lt;BR /&gt;amdgpu: ATOM BIOS: 113-ER16BFE-001&lt;BR /&gt;[drm:.amdgpu_atombios_init [amdgpu]] atom firmware requested 00000000 0kb&lt;BR /&gt;[drm] UVD is enabled in VM mode&lt;BR /&gt;[drm] UVD ENC is enabled in VM mode&lt;BR /&gt;[drm] VCE enabled in VM mode&lt;BR /&gt;[drm] GPU posting now...&lt;BR /&gt;[drm] vm size is 64 GB, 2 levels, block size is 10-bit, fragment size is 9-bit&lt;BR /&gt;[drm:.gmc_v8_0_sw_init [amdgpu]]&lt;BR /&gt;amdgpu 0001:01:00.0: BAR 2: releasing [mem 0xd10000000-0xd101fffff 64bit pref]&lt;BR /&gt;amdgpu 0001:01:00.0: BAR 0: releasing [mem 0xd00000000-0xd0fffffff 64bit pref]&lt;BR /&gt;pcieport 0001:00:00.0: BAR 9: releasing [mem 0xd00000000-0xeffffffff 64bit pref]&lt;BR /&gt;pcieport 0001:00:00.0: BAR 9: assigned [mem 0xd00000000-0xe7fffffff 64bit pref]&lt;BR /&gt;amdgpu 0001:01:00.0: BAR 0: assigned [mem 0xd00000000-0xdffffffff 64bit pref]&lt;BR /&gt;amdgpu 0001:01:00.0: BAR 2: assigned [mem 0xe00000000-0xe001fffff 64bit pref]&lt;BR /&gt;pcieport 0001:00:00.0: PCI bridge to [bus 01]&lt;BR /&gt;pcieport 0001:00:00.0: bridge window [io 0x8000080000010000-0x800008000001ffff]&lt;BR /&gt;pcieport 0001:00:00.0: bridge window [mem 0xa0000000-0xafffffff]&lt;BR /&gt;pcieport 0001:00:00.0: bridge window [mem 0xd00000000-0xe7fffffff 64bit pref]&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: VRAM: 4096M 0x000000F400000000 - 0x000000F4FFFFFFFF (4096M used)&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: GART: 256M 0x000000FF00000000 - 0x000000FF0FFFFFFF&lt;BR /&gt;[drm] Detected VRAM RAM=4096M, BAR=4096M&lt;BR /&gt;[drm] RAM width 128bits GDDR5&lt;BR /&gt;[drm] amdgpu: 4096M of VRAM memory ready&lt;BR /&gt;[drm] amdgpu: 1457M of GTT memory ready.&lt;BR /&gt;[drm] GART: num cpu pages 65536, num gpu pages 65536&lt;BR /&gt;[drm:.amdgpu_ucode_print_mc_hdr [amdgpu]] MC&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] size_bytes: 32608&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] header_size_bytes: 40&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] header_version_major: 1&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] header_version_minor: 0&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ip_version_major: 8&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ip_version_minor: 1&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ucode_version: 0x00b4dc50&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ucode_size_bytes: 32160&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ucode_array_offset_bytes: 448&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] crc32: 0x9b1e395c&lt;BR /&gt;[drm:.amdgpu_ucode_print_mc_hdr [amdgpu]] io_debug_size_bytes: 192&lt;BR /&gt;[drm:.amdgpu_ucode_print_mc_hdr [amdgpu]] io_debug_array_offset_bytes: 256&lt;BR /&gt;[drm] PCIE GART of 256M enabled (table at 0x000000F400000000).&lt;BR /&gt;[drm:.amdgpu_irq_init [amdgpu]] amdgpu: irq initialized.&lt;BR /&gt;[drm:.gfx_v8_0_sw_init [amdgpu]]&lt;BR /&gt;[drm] Chained IB support enabled!&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring gfx use gpu addr 0x000000ff00400040&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.0.0 use gpu addr 0x000000ff004000e0&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.1.0 use gpu addr 0x000000ff00400180&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.2.0 use gpu addr 0x000000ff00400220&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.3.0 use gpu addr 0x000000ff004002c0&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.0.1 use gpu addr 0x000000ff00400360&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.1.1 use gpu addr 0x000000ff00400400&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.2.1 use gpu addr 0x000000ff004004a0&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.3.1 use gpu addr 0x000000ff00400540&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring kiq_2.1.0 use gpu addr 0x000000ff004005e0&lt;BR /&gt;[drm:.sdma_v3_0_sw_init [amdgpu]]&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring sdma0 use gpu addr 0x000000ff00400680&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring sdma1 use gpu addr 0x000000ff00400720&lt;BR /&gt;amdgpu: hwmgr_sw_init smu backed is polaris10_smu&lt;BR /&gt;[drm] Found UVD firmware Version: 1.130 Family ID: 16&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring uvd use gpu addr 0x000000f4001afa80&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring uvd_enc0 use gpu addr 0x000000ff00400860&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring uvd_enc1 use gpu addr 0x000000ff00400900&lt;BR /&gt;[drm] Found VCE firmware Version: 53.26 Binary ID: 3&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring vce0 use gpu addr 0x000000ff004009a0&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring vce1 use gpu addr 0x000000ff00400a40&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring vce2 use gpu addr 0x000000ff00400ae0&lt;BR /&gt;[drm:.amdgpu_ucode_print_smc_hdr [amdgpu]] SMC&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] size_bytes: 130388&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] header_size_bytes: 36&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] header_version_major: 1&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] header_version_minor: 0&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ip_version_major: 7&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ip_version_minor: 2&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ucode_version: 0x00221700&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ucode_size_bytes: 130132&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ucode_array_offset_bytes: 256&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] crc32: 0xae2b3b78&lt;BR /&gt;[drm:.amdgpu_ucode_print_smc_hdr [amdgpu]] ucode_start_addr: 131072&lt;BR /&gt;amdgpu:&lt;BR /&gt;failed to send message 100 ret is 0&lt;BR /&gt;amdgpu: SMU Firmware start failed!&lt;BR /&gt;amdgpu: Failed to load SMU ucode.&lt;BR /&gt;amdgpu: fw load failed&lt;BR /&gt;amdgpu: smu firmware loading failed&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: amdgpu_device_ip_init failed&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: Fatal error during GPU init&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: amdgpu: finishing device.&lt;BR /&gt;[drm:.gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2&lt;BR /&gt;[drm:.gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2&lt;BR /&gt;[drm:.gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2&lt;BR /&gt;[drm:.gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2&lt;BR /&gt;amdgpu: probe of 0001:01:00.0 failed with error -22&lt;BR /&gt;BUG: Unable to handle kernel data access on read at 0x8000080080954000&lt;BR /&gt;Faulting instruction address: 0xc000000000011870&lt;BR /&gt;Oops: Kernel access of bad area, sig: 11 [#1]&lt;BR /&gt;BE PAGE_SIZE=4K SMP NR_CPUS=24 CoreNet Generic&lt;BR /&gt;Modules linked in: amdgpu(+) backlight drm_ttm_helper ttm gpu_sched ucc_uart fsl_jr_uio&lt;BR /&gt;CPU: 2 PID: 816 Comm: insmod Not tainted 5.15.71+g95448dd0dc9b #1&lt;BR /&gt;**bleep**: c000000000011870 LR: 8000000000e0d120 CTR: 0000000000058400&lt;BR /&gt;REGS: c00000000a956d80 TRAP: 0300 Not tainted (5.15.71+g95448dd0dc9b)&lt;BR /&gt;MSR: 0000000080029002 &amp;lt;CE,EE,ME&amp;gt; CR: 22002228 XER: 00000000&lt;BR /&gt;DEAR: 8000080080954000 ESR: 0000000000000000 IRQMASK: 0&lt;BR /&gt;GPR00: 8000000000e0d100 c00000000a957020 c0000000013faa00 c00000000c000000&lt;BR /&gt;GPR04: 8000080080954000 00000000002c2000 00000000000b0800 000000007ecc9000&lt;BR /&gt;GPR08: 0000000000058400 8000080080954000 c00000000bfffffc 80000000010b76d8&lt;BR /&gt;GPR12: c0000000000117f4 c00000003ffff140 000000010b5456f0 000000010b4fa188&lt;BR /&gt;GPR16: 0000000000000000 000000010b545810 000000010b5202b0 0000000000000000&lt;BR /&gt;GPR20: 0000000000000000 0000000000000000 c00000000ae16a48 8000080080954000&lt;BR /&gt;GPR24: 00000000002c2000 0000000000000000 c00000000ae00010 0000000000000001&lt;BR /&gt;GPR28: c00000000ae00000 c00000000ae10000 0000000000000000 c00000000ae10000&lt;BR /&gt;**bleep** [c000000000011870] ._memcpy_fromio+0x7c/0x100&lt;BR /&gt;LR [8000000000e0d120] .amdgpu_uvd_suspend+0x1d4/0x268 [amdgpu]&lt;BR /&gt;Call Trace:&lt;BR /&gt;[c00000000a957020] [8000000000e0d100] .amdgpu_uvd_suspend+0x1b4/0x268 [amdgpu] (unreliable)&lt;BR /&gt;[c00000000a9570f0] [8000000000e1110c] .uvd_v6_0_sw_fini+0x1c/0xcc [amdgpu]&lt;BR /&gt;[c00000000a957180] [8000000000cf24b0] .amdgpu_device_fini_sw+0x124/0x378 [amdgpu]&lt;BR /&gt;[c00000000a957240] [8000000000cf9e0c] .amdgpu_driver_release_kms+0x1c/0x40 [amdgpu]&lt;BR /&gt;[c00000000a9572c0] [c000000000704380] .devm_drm_dev_init_release+0x78/0xcc&lt;BR /&gt;[c00000000a957340] [c000000000755248] .devm_action_release+0x28/0x3c&lt;BR /&gt;[c00000000a9573b0] [c00000000075576c] .release_nodes+0x78/0x108&lt;BR /&gt;[c00000000a957450] [c000000000757174] .devres_release_all+0xa8/0x11c&lt;BR /&gt;[c00000000a957510] [c00000000074f788] .really_probe.part.0+0x1b8/0x440&lt;BR /&gt;[c00000000a9575b0] [c00000000074fad8] .__driver_probe_device+0xc8/0x198&lt;BR /&gt;[c00000000a957640] [c00000000074fbf8] .driver_probe_device+0x50/0x16c&lt;BR /&gt;[c00000000a9576e0] [c00000000075055c] .__driver_attach+0xb4/0x200&lt;BR /&gt;[c00000000a957770] [c00000000074c518] .bus_for_each_dev+0x9c/0x110&lt;BR /&gt;[c00000000a957820] [c00000000074eca4] .driver_attach+0x24/0x38&lt;BR /&gt;[c00000000a957890] [c00000000074e4ec] .bus_add_driver+0x1d4/0x2a8&lt;BR /&gt;[c00000000a957940] [c00000000075107c] .driver_register+0xa4/0x194&lt;BR /&gt;[c00000000a9579c0] [c0000000006217ec] .__pci_register_driver+0x58/0x6c&lt;BR /&gt;[c00000000a957a30] [80000000010a9608] .amdgpu_init+0x74/0x94 [amdgpu]&lt;BR /&gt;[c00000000a957ab0] [c0000000000021cc] .do_one_initcall+0x6c/0x284&lt;BR /&gt;[c00000000a957b90] [c0000000001174a4] .do_init_module+0x5c/0x2bc&lt;BR /&gt;[c00000000a957c30] [c00000000011a980] .__do_sys_finit_module+0xc4/0x10c&lt;BR /&gt;[c00000000a957d60] [c000000000012454] .system_call_exception+0x11c/0x1c4&lt;BR /&gt;[c00000000a957e10] [c0000000000001f8] system_call_common+0xf0/0x210&lt;BR /&gt;--- interrupt: c00 at 0x3fffbe532ee4&lt;BR /&gt;**bleep**: 00003fffbe532ee4 LR: 00000001366cdbfc CTR: 0000000000000000&lt;BR /&gt;REGS: c00000000a957e80 TRAP: 0c00 Not tainted (5.15.71+g95448dd0dc9b)&lt;BR /&gt;MSR: 000000008002d002 &amp;lt;CE,EE,PR,ME&amp;gt; CR: 28002882 XER: 00000000&lt;BR /&gt;IRQMASK: 0&lt;BR /&gt;GPR00: 0000000000000161 00003fffd14f61a0 00003fffbe637200 0000000000000003&lt;BR /&gt;GPR04: 00000001366d9148 0000000000000000 0000000000000000 0000000000000000&lt;BR /&gt;GPR08: 0000000000000000 0000000000000000 0000000000000000 0000000000000000&lt;BR /&gt;GPR12: 0000000000000000 00003fffbe6cf810 000000010b5456f0 000000010b4fa188&lt;BR /&gt;GPR16: 0000000000000000 000000010b545810 000000010b5202b0 0000000000000000&lt;BR /&gt;GPR20: 0000000000000000 0000000000000000 0000000000000002 00003fffd14f6ee5&lt;BR /&gt;GPR24: 00003fffd14f6860 00000001366fd9e8 0000000000000000 00000001366fcbd0&lt;BR /&gt;GPR28: 00000001366d9148 0000000000000000 0000000000000000 0000000136701760&lt;BR /&gt;**bleep** [00003fffbe532ee4] 0x3fffbe532ee4&lt;BR /&gt;LR [00000001366cdbfc] 0x1366cdbfc&lt;BR /&gt;--- interrupt: c00&lt;BR /&gt;Instruction dump:&lt;BR /&gt;4e800020 28250003 40810068 3905fffc 7908f082 38c80001 70c90001 3943fffc&lt;BR /&gt;7c892378 40820070 78c8f842 7d0903a6 &amp;lt;80e90000&amp;gt; 390a0004 90ea0004 7c0006ac&lt;BR /&gt;---[ end trace e1f14bc598aaf8c6 ]---&lt;/P&gt;&lt;P&gt;Segmentation fault&lt;/P&gt;</description>
      <pubDate>Wed, 13 May 2026 15:03:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/failed-to-send-message-100-ret-is-0-while-loading-AMDGPU/m-p/2364970#M5406</guid>
      <dc:creator>Ganesh3955</dc:creator>
      <dc:date>2026-05-13T15:03:43Z</dc:date>
    </item>
    <item>
      <title>Re: failed to send message 100 ret is 0 while loading AMDGPU</title>
      <link>https://community.nxp.com/t5/T-Series/failed-to-send-message-100-ret-is-0-while-loading-AMDGPU/m-p/2365014#M5407</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Your log indicates AMDGPU fails during Polaris12 SMU firmware startup, while PCIe appears to enumerate correctly enough to reach late GPU init, so the issue is more likely driver/platform compatibility or probe-cleanup failure than basic T1040 PCIe link training.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 13 May 2026 16:31:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/failed-to-send-message-100-ret-is-0-while-loading-AMDGPU/m-p/2365014#M5407</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2026-05-13T16:31:11Z</dc:date>
    </item>
    <item>
      <title>Re: failed to send message 100 ret is 0 while loading AMDGPU</title>
      <link>https://community.nxp.com/t5/T-Series/failed-to-send-message-100-ret-is-0-while-loading-AMDGPU/m-p/2365223#M5408</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/34846"&gt;@Bio_TICFSL&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thank you for you reply,&lt;BR /&gt;&lt;BR /&gt;May i know whether the following platforms are compatible with each other:&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;- &amp;gt; NXP T1040 with AMD E9171 GPU&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;- &amp;gt;&amp;nbsp;NXP T2080 with AMD E9171 GPU&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;- &amp;gt; NXP T2080 with AMD E8860 GPU&lt;/P&gt;</description>
      <pubDate>Thu, 14 May 2026 04:51:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/failed-to-send-message-100-ret-is-0-while-loading-AMDGPU/m-p/2365223#M5408</guid>
      <dc:creator>Ganesh3955</dc:creator>
      <dc:date>2026-05-14T04:51:39Z</dc:date>
    </item>
    <item>
      <title>Re: failed to send message 100 ret is 0 while loading AMDGPU</title>
      <link>https://community.nxp.com/t5/T-Series/failed-to-send-message-100-ret-is-0-while-loading-AMDGPU/m-p/2365333#M5409</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/34846"&gt;@Bio_TICFSL&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I Bypassed SMU in AMDGPU driver , now i am facing below error(gfx ring test failure)&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;root@t1042d4rdb:~# insmod /amdgpu.ko&lt;BR /&gt;[drm] amdgpu kernel modesetting enabled.&lt;BR /&gt;[drm] initializing kernel modesetting (POLARIS12 0x1002:0x6987 0x1787:0x2389 0x80).&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: Trusted Memory Zone (TMZ) feature not supported&lt;BR /&gt;[drm] register mmio base: 0xA0000000&lt;BR /&gt;[drm] register mmio size: 262144&lt;BR /&gt;[drm] PCIE atomic ops is not supported&lt;BR /&gt;[drm] add ip block number 0 &amp;lt;vi_common&amp;gt;&lt;BR /&gt;[drm] add ip block number 1 &amp;lt;gmc_v8_0&amp;gt;&lt;BR /&gt;[drm] add ip block number 2 &amp;lt;tonga_ih&amp;gt;&lt;BR /&gt;[drm] add ip block number 3 &amp;lt;gfx_v8_0&amp;gt;&lt;BR /&gt;[drm] add ip block number 4 &amp;lt;sdma_v3_0&amp;gt;&lt;BR /&gt;[drm] add ip block number 5 &amp;lt;powerplay&amp;gt;&lt;BR /&gt;[drm] add ip block number 6 &amp;lt;dm&amp;gt;&lt;BR /&gt;[drm] add ip block number 7 &amp;lt;uvd_v6_0&amp;gt;&lt;BR /&gt;[drm] add ip block number 8 &amp;lt;vce_v3_0&amp;gt;&lt;BR /&gt;[drm:.check_atom_bios [amdgpu]] ATOMBIOS detected&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: Fetched VBIOS from ROM BAR&lt;BR /&gt;amdgpu: ATOM BIOS: 113-ER16BFE-001&lt;BR /&gt;[drm:.amdgpu_atombios_init [amdgpu]] atom firmware requested 00000000 0kb&lt;BR /&gt;[drm] UVD is enabled in VM mode&lt;BR /&gt;[drm] UVD ENC is enabled in VM mode&lt;BR /&gt;[drm] VCE enabled in VM mode&lt;BR /&gt;[drm] GPU posting now...&lt;BR /&gt;[drm] vm size is 64 GB, 2 levels, block size is 10-bit, fragment size is 9-bit&lt;BR /&gt;[drm:.gmc_v8_0_sw_init [amdgpu]]&lt;BR /&gt;amdgpu 0001:01:00.0: BAR 2: releasing [mem 0xd10000000-0xd101fffff 64bit pref]&lt;BR /&gt;amdgpu 0001:01:00.0: BAR 0: releasing [mem 0xd00000000-0xd0fffffff 64bit pref]&lt;BR /&gt;pcieport 0001:00:00.0: BAR 9: releasing [mem 0xd00000000-0xeffffffff 64bit pref]&lt;BR /&gt;pcieport 0001:00:00.0: BAR 9: assigned [mem 0xd00000000-0xe7fffffff 64bit pref]&lt;BR /&gt;amdgpu 0001:01:00.0: BAR 0: assigned [mem 0xd00000000-0xdffffffff 64bit pref]&lt;BR /&gt;amdgpu 0001:01:00.0: BAR 2: assigned [mem 0xe00000000-0xe001fffff 64bit pref]&lt;BR /&gt;pcieport 0001:00:00.0: PCI bridge to [bus 01]&lt;BR /&gt;pcieport 0001:00:00.0: bridge window [io 0x8000080000010000-0x800008000010ffff]&lt;BR /&gt;pcieport 0001:00:00.0: bridge window [mem 0xa0000000-0xafffffff]&lt;BR /&gt;pcieport 0001:00:00.0: bridge window [mem 0xd00000000-0xe7fffffff 64bit pref]&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: VRAM: 4096M 0x000000F400000000 - 0x000000F4FFFFFFFF (4096M used)&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: GART: 256M 0x000000FF00000000 - 0x000000FF0FFFFFFF&lt;BR /&gt;[drm] Detected VRAM RAM=4096M, BAR=4096M&lt;BR /&gt;[drm] RAM width 128bits GDDR5&lt;BR /&gt;[drm] amdgpu: 4096M of VRAM memory ready&lt;BR /&gt;[drm] amdgpu: 1457M of GTT memory ready.&lt;BR /&gt;[drm] GART: num cpu pages 65536, num gpu pages 65536&lt;BR /&gt;[drm:.amdgpu_ucode_print_mc_hdr [amdgpu]] MC&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] size_bytes: 32608&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] header_size_bytes: 40&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] header_version_major: 1&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] header_version_minor: 0&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ip_version_major: 8&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ip_version_minor: 1&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ucode_version: 0x00b4dc50&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ucode_size_bytes: 32160&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] ucode_array_offset_bytes: 448&lt;BR /&gt;[drm:.amdgpu_ucode_print_common_hdr [amdgpu]] crc32: 0x9b1e395c&lt;BR /&gt;[drm:.amdgpu_ucode_print_mc_hdr [amdgpu]] io_debug_size_bytes: 192&lt;BR /&gt;[drm:.amdgpu_ucode_print_mc_hdr [amdgpu]] io_debug_array_offset_bytes: 256&lt;BR /&gt;[drm] PCIE GART of 256M enabled (table at 0x000000F400000000).&lt;BR /&gt;[drm:.amdgpu_irq_init [amdgpu]] amdgpu: irq initialized.&lt;BR /&gt;[drm:.gfx_v8_0_sw_init [amdgpu]]&lt;BR /&gt;[drm] Chained IB support enabled!&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring gfx use gpu addr 0x000000ff00400040&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.0.0 use gpu addr 0x000000ff004000e0&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.1.0 use gpu addr 0x000000ff00400180&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.2.0 use gpu addr 0x000000ff00400220&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.3.0 use gpu addr 0x000000ff004002c0&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.0.1 use gpu addr 0x000000ff00400360&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.1.1 use gpu addr 0x000000ff00400400&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.2.1 use gpu addr 0x000000ff004004a0&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring comp_1.3.1 use gpu addr 0x000000ff00400540&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring kiq_2.1.0 use gpu addr 0x000000ff004005e0&lt;BR /&gt;[drm:.sdma_v3_0_sw_init [amdgpu]]&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring sdma0 use gpu addr 0x000000ff00400680&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring sdma1 use gpu addr 0x000000ff00400720&lt;BR /&gt;amdgpu: hwmgr_sw_init smu backed is polaris10_smu&lt;BR /&gt;[drm] Found UVD firmware Version: 1.130 Family ID: 16&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring uvd use gpu addr 0x000000f4001afa80&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring uvd_enc0 use gpu addr 0x000000ff00400860&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring uvd_enc1 use gpu addr 0x000000ff00400900&lt;BR /&gt;[drm] Found VCE firmware Version: 53.26 Binary ID: 3&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring vce0 use gpu addr 0x000000ff004009a0&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring vce1 use gpu addr 0x000000ff00400a40&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_fence_driver_start_ring [amdgpu]] fence driver on ring vce2 use gpu addr 0x000000ff00400ae0&lt;BR /&gt;[drm:.amdgpu_ih_process [amdgpu]] amdgpu_ih_process: rptr 0, wptr 16&lt;BR /&gt;[drm:.amdgpu_irq_dispatch [amdgpu]] Unhandled interrupt src_id: 141&lt;BR /&gt;amdgpu 0001:01:00.0: [drm:.amdgpu_ring_test_helper [amdgpu]] *ERROR* ring gfx test failed (-110)&lt;BR /&gt;[drm:.amdgpu_device_init [amdgpu]] *ERROR* hw_init of IP block &amp;lt;gfx_v8_0&amp;gt; failed -110&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: amdgpu_device_ip_init failed&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: Fatal error during GPU init&lt;BR /&gt;amdgpu 0001:01:00.0: amdgpu: amdgpu: finishing device.&lt;BR /&gt;[drm:.gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2&lt;BR /&gt;[drm:.gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2&lt;BR /&gt;[drm:.gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2&lt;BR /&gt;[drm:.gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2&lt;BR /&gt;amdgpu: probe of 0001:01:00.0 failed with error -110&lt;BR /&gt;BUG: Unable to handle kernel data access on read at 0x8000080080954000&lt;BR /&gt;Faulting instruction address: 0xc000000000011870&lt;BR /&gt;Oops: Kernel access of bad area, sig: 11 [#1]&lt;BR /&gt;BE PAGE_SIZE=4K SMP NR_CPUS=24 CoreNet Generic&lt;BR /&gt;Modules linked in: amdgpu(+) backlight drm_ttm_helper ttm gpu_sched ucc_uart fsl_jr_uio&lt;BR /&gt;CPU: 2 PID: 819 Comm: insmod Not tainted 5.15.71+g95448dd0dc9b #1&lt;BR /&gt;**bleep**: c000000000011870 LR: 8000000000e0efe0 CTR: 0000000000058400&lt;BR /&gt;REGS: c00000000a5aad80 TRAP: 0300 Not tainted (5.15.71+g95448dd0dc9b)&lt;BR /&gt;MSR: 0000000080029002 &amp;lt;CE,EE,ME&amp;gt; CR: 22002228 XER: 00000000&lt;BR /&gt;DEAR: 8000080080954000 ESR: 0000000000000000 IRQMASK: 0&lt;BR /&gt;GPR00: 8000000000e0efc0 c00000000a5ab020 c0000000013e8c00 c00000000c000000&lt;BR /&gt;GPR04: 8000080080954000 00000000002c2000 00000000000b0800 000000007ecd9000&lt;BR /&gt;GPR08: 0000000000058400 8000080080954000 c00000000bfffffc 80000000010b8988&lt;BR /&gt;GPR12: c0000000000117f4 c00000003ffff140 00000001050e5850 000000010509a188&lt;BR /&gt;GPR16: 0000000000000000 00000001050e5990 00000001050bfb80 0000000000000000&lt;BR /&gt;GPR20: 0000000000000000 0000000000000000 c00000000a916a48 8000080080954000&lt;BR /&gt;GPR24: 00000000002c2000 0000000000000000 c00000000a900010 0000000000000001&lt;BR /&gt;GPR28: c00000000a900000 c00000000a910000 0000000000000000 c00000000a910000&lt;BR /&gt;**bleep** [c000000000011870] ._memcpy_fromio+0x7c/0x100&lt;BR /&gt;LR [8000000000e0efe0] .amdgpu_uvd_suspend+0x1d4/0x268 [amdgpu]&lt;BR /&gt;Call Trace:&lt;BR /&gt;[c00000000a5ab020] [8000000000e0efc0] .amdgpu_uvd_suspend+0x1b4/0x268 [amdgpu] (unreliable)&lt;BR /&gt;[c00000000a5ab0f0] [8000000000e12fcc] .uvd_v6_0_sw_fini+0x1c/0xcc [amdgpu]&lt;BR /&gt;[c00000000a5ab180] [8000000000cf44b0] .amdgpu_device_fini_sw+0x124/0x378 [amdgpu]&lt;BR /&gt;[c00000000a5ab240] [8000000000cfbe0c] .amdgpu_driver_release_kms+0x1c/0x40 [amdgpu]&lt;BR /&gt;[c00000000a5ab2c0] [c0000000006fa1e4] .devm_drm_dev_init_release+0x78/0xcc&lt;BR /&gt;[c00000000a5ab340] [c00000000074b0ac] .devm_action_release+0x28/0x3c&lt;BR /&gt;[c00000000a5ab3b0] [c00000000074b5d0] .release_nodes+0x78/0x108&lt;BR /&gt;[c00000000a5ab450] [c00000000074cfd8] .devres_release_all+0xa8/0x11c&lt;BR /&gt;[c00000000a5ab510] [c0000000007455ec] .really_probe.part.0+0x1b8/0x440&lt;BR /&gt;[c00000000a5ab5b0] [c00000000074593c] .__driver_probe_device+0xc8/0x198&lt;BR /&gt;[c00000000a5ab640] [c000000000745a5c] .driver_probe_device+0x50/0x16c&lt;BR /&gt;[c00000000a5ab6e0] [c0000000007463c0] .__driver_attach+0xb4/0x200&lt;BR /&gt;[c00000000a5ab770] [c00000000074237c] .bus_for_each_dev+0x9c/0x110&lt;BR /&gt;[c00000000a5ab820] [c000000000744b08] .driver_attach+0x24/0x38&lt;BR /&gt;[c00000000a5ab890] [c000000000744350] .bus_add_driver+0x1d4/0x2a8&lt;BR /&gt;[c00000000a5ab940] [c000000000746ee0] .driver_register+0xa4/0x194&lt;BR /&gt;[c00000000a5ab9c0] [c0000000006211dc] .__pci_register_driver+0x58/0x6c&lt;BR /&gt;[c00000000a5aba30] [80000000010aa8e8] .amdgpu_init+0x74/0x94 [amdgpu]&lt;BR /&gt;[c00000000a5abab0] [c0000000000021cc] .do_one_initcall+0x6c/0x284&lt;BR /&gt;[c00000000a5abb90] [c000000000116ea0] .do_init_module+0x5c/0x2bc&lt;BR /&gt;[c00000000a5abc30] [c00000000011a37c] .__do_sys_finit_module+0xc4/0x10c&lt;BR /&gt;[c00000000a5abd60] [c000000000012454] .system_call_exception+0x11c/0x1c4&lt;BR /&gt;[c00000000a5abe10] [c0000000000001f8] system_call_common+0xf0/0x210&lt;BR /&gt;--- interrupt: c00 at 0x3fff82934ee4&lt;BR /&gt;**bleep**: 00003fff82934ee4 LR: 00000001194adbfc CTR: 0000000000000000&lt;BR /&gt;REGS: c00000000a5abe80 TRAP: 0c00 Not tainted (5.15.71+g95448dd0dc9b)&lt;BR /&gt;MSR: 000000008002d002 &amp;lt;CE,EE,PR,ME&amp;gt; CR: 28002882 XER: 00000000&lt;BR /&gt;IRQMASK: 0&lt;BR /&gt;GPR00: 0000000000000161 00003fffefee52c0 00003fff82a39200 0000000000000003&lt;BR /&gt;GPR04: 00000001194b9148 0000000000000000 0000000000000000 0000000000000000&lt;BR /&gt;GPR08: 0000000000000000 0000000000000000 0000000000000000 0000000000000000&lt;BR /&gt;GPR12: 0000000000000000 00003fff82ad1810 00000001050e5850 000000010509a188&lt;BR /&gt;GPR16: 0000000000000000 00000001050e5990 00000001050bfb80 0000000000000000&lt;BR /&gt;GPR20: 0000000000000000 0000000000000000 0000000000000002 00003fffefee5ee5&lt;BR /&gt;GPR24: 00003fffefee5980 00000001194dd9e8 0000000000000000 00000001194dcbd0&lt;BR /&gt;GPR28: 00000001194b9148 0000000000000000 0000000000000000 00000001194e1760&lt;BR /&gt;**bleep** [00003fff82934ee4] 0x3fff82934ee4&lt;BR /&gt;LR [00000001194adbfc] 0x1194adbfc&lt;BR /&gt;--- interrupt: c00&lt;BR /&gt;Instruction dump:&lt;BR /&gt;4e800020 28250003 40810068 3905fffc 7908f082 38c80001 70c90001 3943fffc&lt;BR /&gt;7c892378 40820070 78c8f842 7d0903a6 &amp;lt;80e90000&amp;gt; 390a0004 90ea0004 7c0006ac&lt;BR /&gt;---[ end trace fef1e0dc2e9ff52c ]---&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 May 2026 08:24:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/failed-to-send-message-100-ret-is-0-while-loading-AMDGPU/m-p/2365333#M5409</guid>
      <dc:creator>Ganesh3955</dc:creator>
      <dc:date>2026-05-14T08:24:49Z</dc:date>
    </item>
  </channel>
</rss>