<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Inquiry Regarding Boot Configuration in T1024 in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/Inquiry-Regarding-Boot-Configuration-in-T1024/m-p/2072213#M5183</link>
    <description>&lt;P&gt;Sorry, but 8-bit ECC is not supported for 512- and 2048-byte pages, please refer to chapter&amp;nbsp;23.5.6.2 BCH encoding of the RM.&lt;/P&gt;
&lt;P&gt;For 4-bit correction, 8 parity bytes, 8-bit correction 16 parity bytes, 24-bit correction 42&lt;BR /&gt;parity bytes, and 40-bit correction 70 parity bytes per sector are required. These parity&lt;BR /&gt;bytes are stored in the spare region of the page at offset 08h. For small pages, only 4-bit&lt;BR /&gt;mode is allowed. For a 2 KB page, four sectors of 512 bytes each can be present in the&lt;BR /&gt;main region; hence a total of 4x8= 32 parity bytes are store at offset 08h. For a 4 KB&lt;BR /&gt;page size, eight sectors of 512 bytes each can be present; hence 8x8 =64 parity bytes are&lt;BR /&gt;required for 4-bit mode and 128 bytes for 8-bit mode.&lt;/P&gt;</description>
    <pubDate>Tue, 01 Apr 2025 16:51:11 GMT</pubDate>
    <dc:creator>Oswalag</dc:creator>
    <dc:date>2025-04-01T16:51:11Z</dc:date>
    <item>
      <title>Inquiry Regarding Boot Configuration in T1024</title>
      <link>https://community.nxp.com/t5/T-Series/Inquiry-Regarding-Boot-Configuration-in-T1024/m-p/2070183#M5179</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I am currently designing a board to boot the T1024 from NAND flash, and the NAND I plan to use is equipped with 8-bit ECC.&lt;/P&gt;&lt;P&gt;In CodeWarrior Development Studio, when narrowing down the Boot Configuration options from the pull-down menu based on the specifications of the NAND (data width, page size, pages per block), only candidates with 4-bit ECC remain.&lt;/P&gt;&lt;P&gt;Does this imply that NAND with 8-bit ECC cannot be used, or does it indicate a potential risk of boot failure when using such NAND?&lt;/P&gt;&lt;P&gt;Thank you for your assistance.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;satoshi&lt;/P&gt;</description>
      <pubDate>Fri, 28 Mar 2025 08:54:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Inquiry-Regarding-Boot-Configuration-in-T1024/m-p/2070183#M5179</guid>
      <dc:creator>satoshi-123</dc:creator>
      <dc:date>2025-03-28T08:54:30Z</dc:date>
    </item>
    <item>
      <title>Re: Inquiry Regarding Boot Configuration in T1024</title>
      <link>https://community.nxp.com/t5/T-Series/Inquiry-Regarding-Boot-Configuration-in-T1024/m-p/2072213#M5183</link>
      <description>&lt;P&gt;Sorry, but 8-bit ECC is not supported for 512- and 2048-byte pages, please refer to chapter&amp;nbsp;23.5.6.2 BCH encoding of the RM.&lt;/P&gt;
&lt;P&gt;For 4-bit correction, 8 parity bytes, 8-bit correction 16 parity bytes, 24-bit correction 42&lt;BR /&gt;parity bytes, and 40-bit correction 70 parity bytes per sector are required. These parity&lt;BR /&gt;bytes are stored in the spare region of the page at offset 08h. For small pages, only 4-bit&lt;BR /&gt;mode is allowed. For a 2 KB page, four sectors of 512 bytes each can be present in the&lt;BR /&gt;main region; hence a total of 4x8= 32 parity bytes are store at offset 08h. For a 4 KB&lt;BR /&gt;page size, eight sectors of 512 bytes each can be present; hence 8x8 =64 parity bytes are&lt;BR /&gt;required for 4-bit mode and 128 bytes for 8-bit mode.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Apr 2025 16:51:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Inquiry-Regarding-Boot-Configuration-in-T1024/m-p/2072213#M5183</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2025-04-01T16:51:11Z</dc:date>
    </item>
  </channel>
</rss>