<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic T1040D4RDB Tx Buffer Not Ready in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T1040D4RDB-Tx-Buffer-Not-Ready/m-p/2066566#M5177</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I am using the T1040D4RDB with U-Boot and was trying to load a different Fman microcode into 0xEFF00000 and accidentally erased 0x20000 instead of 0x10000. This removed the QUICC engine microcode and now when I try to ping out of any port I get the following output:&lt;BR /&gt;Using FM1@DTSEC4&amp;nbsp;&amp;nbsp;device&lt;BR /&gt;FM1@DTSEC4: Tx error,&amp;nbsp;&amp;nbsp;txbd-&amp;gt;status = 0x8800&lt;BR /&gt;FM1@DTSEC4: Tx buffer not ready, txbd-&amp;gt;status = 0x8800&lt;BR /&gt;FM1@DTSEC4: Tx buffer not ready, txbd-&amp;gt;status = 0x8800&lt;BR /&gt;FM1@DTSEC4: Tx buffer not ready, txbd-&amp;gt;status = 0x8800&lt;BR /&gt;&lt;BR /&gt;I tried loading the iram_Type_A_T1040_r1.0.bin from &lt;A href="https://github.com/nxp-qoriq/qoriq-qe-ucode" target="_blank" rel="noopener noreferrer"&gt;https://github.com/nxp-qoriq/qoriq-qe-ucode&lt;/A&gt;&amp;nbsp;into&amp;nbsp;0xEFF10000 but I still get the same output. Is there a different file that I have to use specific to the D4RDB? Or is there a different issue entirely?&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Cole&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 21 Mar 2025 22:00:24 GMT</pubDate>
    <dc:creator>Cole_B</dc:creator>
    <dc:date>2025-03-21T22:00:24Z</dc:date>
    <item>
      <title>T1040D4RDB Tx Buffer Not Ready</title>
      <link>https://community.nxp.com/t5/T-Series/T1040D4RDB-Tx-Buffer-Not-Ready/m-p/2066566#M5177</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I am using the T1040D4RDB with U-Boot and was trying to load a different Fman microcode into 0xEFF00000 and accidentally erased 0x20000 instead of 0x10000. This removed the QUICC engine microcode and now when I try to ping out of any port I get the following output:&lt;BR /&gt;Using FM1@DTSEC4&amp;nbsp;&amp;nbsp;device&lt;BR /&gt;FM1@DTSEC4: Tx error,&amp;nbsp;&amp;nbsp;txbd-&amp;gt;status = 0x8800&lt;BR /&gt;FM1@DTSEC4: Tx buffer not ready, txbd-&amp;gt;status = 0x8800&lt;BR /&gt;FM1@DTSEC4: Tx buffer not ready, txbd-&amp;gt;status = 0x8800&lt;BR /&gt;FM1@DTSEC4: Tx buffer not ready, txbd-&amp;gt;status = 0x8800&lt;BR /&gt;&lt;BR /&gt;I tried loading the iram_Type_A_T1040_r1.0.bin from &lt;A href="https://github.com/nxp-qoriq/qoriq-qe-ucode" target="_blank" rel="noopener noreferrer"&gt;https://github.com/nxp-qoriq/qoriq-qe-ucode&lt;/A&gt;&amp;nbsp;into&amp;nbsp;0xEFF10000 but I still get the same output. Is there a different file that I have to use specific to the D4RDB? Or is there a different issue entirely?&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Cole&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Mar 2025 22:00:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1040D4RDB-Tx-Buffer-Not-Ready/m-p/2066566#M5177</guid>
      <dc:creator>Cole_B</dc:creator>
      <dc:date>2025-03-21T22:00:24Z</dc:date>
    </item>
    <item>
      <title>Re: T1040D4RDB Tx Buffer Not Ready</title>
      <link>https://community.nxp.com/t5/T-Series/T1040D4RDB-Tx-Buffer-Not-Ready/m-p/2073568#M5187</link>
      <description>&lt;P&gt;Probably fman ucode is broken, please deploy the attached fman ucode to your target board in u-boot with the following commands.&lt;/P&gt;
&lt;P&gt;=&amp;gt;tftp 0x1000000&amp;nbsp;fsl_fman_ucode_t1040_r1.1_106_4_18.bin&lt;/P&gt;
&lt;P&gt;=&amp;gt;erase&amp;nbsp;0xEFF00000 +$filesize&lt;/P&gt;
&lt;P&gt;=&amp;gt;cp.b&amp;nbsp;0x1000000&amp;nbsp;0xEFF00000&amp;nbsp;$filesize&lt;/P&gt;</description>
      <pubDate>Thu, 03 Apr 2025 09:17:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1040D4RDB-Tx-Buffer-Not-Ready/m-p/2073568#M5187</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2025-04-03T09:17:23Z</dc:date>
    </item>
  </channel>
</rss>