<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: T1042d4rdb-64b building process. in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T1042d4rdb-64b-building-process/m-p/2012594#M5098</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The link&amp;nbsp; you have provided contains the meta-qoriq repo. I am trying to build the fsl-toolchain or fsl/ls-image-main, on running bitbake-layers show-recipes, it shows that these(fsl-toolchain &amp;amp; fsl-image-main) reference meta-freescale.&lt;BR /&gt;I am not able to find this from the link you provided. But i have found &lt;A href="https://github.com/Freescale/meta-freescale" target="_self"&gt;https://github.com/Freescale/meta-freescale&lt;/A&gt; and this depends on openembeddedcore. I understand that i have to replace the url src of my project (meta-freescale) to the ones still being maintained above, but what branch do I have to use? I am not finding any list of supported devices which lists t1022 or t1042.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;/P&gt;</description>
    <pubDate>Thu, 12 Dec 2024 06:52:47 GMT</pubDate>
    <dc:creator>Mewan</dc:creator>
    <dc:date>2024-12-12T06:52:47Z</dc:date>
    <item>
      <title>T1042d4rdb-64b building process.</title>
      <link>https://community.nxp.com/t5/T-Series/T1042d4rdb-64b-building-process/m-p/2011032#M5095</link>
      <description>&lt;P&gt;I have downloaded the source and ppce5500 yocto cache from &lt;A href="https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&amp;amp;element=7726177," target="_blank"&gt;https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&amp;amp;element=7726177,&lt;/A&gt; I installed the source iso first and then the yocto cache, ran the host_prepare.sh, and sourced(fsl_env_setup) with machine t1042d4rdb-64b. I ran the command&lt;BR /&gt;$ bitbake fsl-toolchain&lt;BR /&gt;Got the error&lt;BR /&gt;"the '--set-upstream' option is no longer supported. Please use '--track' or '--set-upstream-to' instead." I update the source/poky/bitbake/lib/bb/fetch2/git.py file to use --set-upstream-to command and reran&lt;BR /&gt;$bitbake fsl-toolchain&lt;BR /&gt;And now i am getting the error below&lt;BR /&gt;"ERROR: Function failed: Fetcher failure: Fetch command failed with exit code 128, output:&lt;BR /&gt;fatal: branch 'origin/master' does not exist".&lt;BR /&gt;&lt;BR /&gt;Is there a way to resolve this? I checked the $$ git remote -v&lt;BR /&gt;fsl-public git://git.freescale.com/yocto/meta-freescale (fetch)&lt;BR /&gt;fsl-public git://git.freescale.com/yocto/meta-freescale (push)&lt;BR /&gt;and when i tried openning on chrome, it showed that the site does not exist.&lt;BR /&gt;&lt;BR /&gt;&lt;LI-PRODUCT title="T1042" id="T1042"&gt;&lt;/LI-PRODUCT&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Dec 2024 11:38:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1042d4rdb-64b-building-process/m-p/2011032#M5095</guid>
      <dc:creator>Mewan</dc:creator>
      <dc:date>2024-12-10T11:38:08Z</dc:date>
    </item>
    <item>
      <title>Re: T1042d4rdb-64b building process.</title>
      <link>https://community.nxp.com/t5/T-Series/T1042d4rdb-64b-building-process/m-p/2012408#M5097</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The git://git.freescale.com repository was replaced by&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://github.com/nxp-qoriq" target="_blank"&gt;https://github.com/nxp-qoriq&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Some recipes may still refer to the old repository so please replace them on the recipes where you are experiencing issues.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Thu, 12 Dec 2024 02:20:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1042d4rdb-64b-building-process/m-p/2012408#M5097</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2024-12-12T02:20:07Z</dc:date>
    </item>
    <item>
      <title>Re: T1042d4rdb-64b building process.</title>
      <link>https://community.nxp.com/t5/T-Series/T1042d4rdb-64b-building-process/m-p/2012594#M5098</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The link&amp;nbsp; you have provided contains the meta-qoriq repo. I am trying to build the fsl-toolchain or fsl/ls-image-main, on running bitbake-layers show-recipes, it shows that these(fsl-toolchain &amp;amp; fsl-image-main) reference meta-freescale.&lt;BR /&gt;I am not able to find this from the link you provided. But i have found &lt;A href="https://github.com/Freescale/meta-freescale" target="_self"&gt;https://github.com/Freescale/meta-freescale&lt;/A&gt; and this depends on openembeddedcore. I understand that i have to replace the url src of my project (meta-freescale) to the ones still being maintained above, but what branch do I have to use? I am not finding any list of supported devices which lists t1022 or t1042.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 12 Dec 2024 06:52:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1042d4rdb-64b-building-process/m-p/2012594#M5098</guid>
      <dc:creator>Mewan</dc:creator>
      <dc:date>2024-12-12T06:52:47Z</dc:date>
    </item>
    <item>
      <title>Re: T1042d4rdb-64b building process.</title>
      <link>https://community.nxp.com/t5/T-Series/T1042d4rdb-64b-building-process/m-p/2013142#M5099</link>
      <description>&lt;P&gt;You can review as an option dunfell branch, please take a look in the links below:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-qoriq/yocto-sdk/tree/dunfell" target="_blank"&gt;https://github.com/nxp-qoriq/yocto-sdk/tree/dunfell&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/Freescale/meta-freescale/tree/dunfell?tab=readme-ov-file" target="_blank"&gt;https://github.com/Freescale/meta-freescale/tree/dunfell?tab=readme-ov-file&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Dec 2024 21:59:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1042d4rdb-64b-building-process/m-p/2013142#M5099</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2024-12-12T21:59:26Z</dc:date>
    </item>
    <item>
      <title>Re: T1042d4rdb-64b building process.</title>
      <link>https://community.nxp.com/t5/T-Series/T1042d4rdb-64b-building-process/m-p/2014872#M5103</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I fetched the yocto sdk dunfell branch and updated the manifest file to use the freescale git source instead of the codeaurora source. Then I updated the src_url in the layers as well and removed nativesdk-cst and I finally had a successful build.&lt;BR /&gt;&lt;BR /&gt;Thanks for the assistance.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Dec 2024 03:46:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1042d4rdb-64b-building-process/m-p/2014872#M5103</guid>
      <dc:creator>Mewan</dc:creator>
      <dc:date>2024-12-17T03:46:12Z</dc:date>
    </item>
  </channel>
</rss>