<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックRe: t2081 pcie Issue</title>
    <link>https://community.nxp.com/t5/T-Series/t2081-pcie-Issue/m-p/2006669#M5093</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Here i attached the full log file&lt;/P&gt;</description>
    <pubDate>Wed, 04 Dec 2024 06:35:56 GMT</pubDate>
    <dc:creator>arumilli</dc:creator>
    <dc:date>2024-12-04T06:35:56Z</dc:date>
    <item>
      <title>t2081 pcie Issue</title>
      <link>https://community.nxp.com/t5/T-Series/t2081-pcie-Issue/m-p/2005064#M5088</link>
      <description>&lt;P&gt;I am working on T2081 custom board. After booting Linux and run the command&lt;STRONG&gt;dmesg | grep -i pci &lt;/STRONG&gt;i got some error&lt;STRONG&gt;.&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;How to resolve these issues.&lt;/P&gt;&lt;P&gt;I am using &lt;STRONG&gt;t2081 evk qds devicetree&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;root@t2081qds:/sys/bus/pci/devices# dmesg | grep -i pci&lt;BR /&gt;[ 0.318064] Found FSL PCI host bridge at 0x0000000ffe270000. Firmware bus number: 0-&amp;gt;0&lt;BR /&gt;[ 0.324595] PCI host bridge /pcie@ffe270000 ranges:&lt;BR /&gt;[ 0.342076] /pcie@ffe270000: PCICSRBAR @ 0xff000007&lt;BR /&gt;[ 0.345589] setup_pci_atmu: end of DRAM c0000000&lt;BR /&gt;[ 0.350059] /pcie@ffe270000: Setting PCI inbound window greater than memory size&lt;BR /&gt;[ 0.357009] EDAC PCI0: Giving out device to module MPC85xx_edac controller mpc85xx_pci_err : DEV ffe270000.pcie (INTERRUPT)&lt;BR /&gt;[ 0.366699] MPC85xx_edac acquired irq 23 for PCI Err&lt;BR /&gt;[ 0.370315] MPC85xx_edac PCI err registered&lt;BR /&gt;[ 0.373240] platform ffe270000.pcie:pcie@0: Invalid size 0xfffff9 for dma-range&lt;BR /&gt;[ 0.402817] PCI: Probing PCI hardware&lt;BR /&gt;[ 0.405168] fsl-pci ffe270000.pcie: PCI host bridge to bus 0000:00&lt;BR /&gt;[ 0.409963] pci_bus 0000:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x0000- 0xffff])&lt;BR /&gt;[ 0.417613] pci_bus 0000:00: root bus resource [mem 0xc40000000-0xc4fffffff] (bus address [0xe0000000-0xefffffff])&lt;BR /&gt;[ 0.426654] pci_bus 0000:00: root bus resource [bus 00]&lt;BR /&gt;[ 0.430563] pci_bus 0000:00: busn_res: [bus 00] end is updated to ff&lt;BR /&gt;[ 0.431298] pci 0000:00:00.0: [1957:0838] type 01 class 0x0b2000&lt;BR /&gt;[ 0.432030] pci 0000:00:00.0: [Firmware Bug]: reg 0x10: invalid BAR (can't size)&lt;BR /&gt;[ 0.439082] pci 0000:00:00.0: reg 0x38: [mem 0x00000000-0x00ffffff pref]&lt;BR /&gt;[ 0.442327] pci 0000:00:00.0: supports D1 D2&lt;BR /&gt;[ 0.442331] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot&lt;BR /&gt;[ 0.443943] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring&lt;BR /&gt;[ 0.451882] pci 0000:00:00.0: PCI bridge to [bus 01-ff]&lt;BR /&gt;[ 0.455836] pci 0000:00:00.0: bridge window [io 0x10000-0x10fff]&lt;BR /&gt;[ 0.455914] pci 0000:00:00.0: bridge window [mem 0x00000000-0x000fffff]&lt;BR /&gt;[ 0.456111] pci 0000:00:00.0: bridge window [mem 0x00000000-0x000fffff 64bit pref]&lt;BR /&gt;[ 0.456411] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01&lt;BR /&gt;[ 0.456417] pci_bus 0000:00: busn_res: [bus 00-ff] end is updated to 01&lt;BR /&gt;[ 0.456523] PCI 0000:00 Cannot reserve Legacy IO [io 0x10000-0x10fff]&lt;BR /&gt;[ 0.456595] pci 0000:00:00.0: BAR 6: no space for [mem size 0x01000000 pref]&lt;BR /&gt;[ 0.462256] pci 0000:00:00.0: BAR 6: failed to assign [mem size 0x01000000 pref]&lt;BR /&gt;[ 0.468342] pci 0000:00:00.0: PCI bridge to [bus 01]&lt;BR /&gt;[ 0.472026] pci 0000:00:00.0: bridge window [io 0x10000-0x1ffff]&lt;BR /&gt;[ 0.476950] pci 0000:00:00.0: bridge window [mem 0xc40000000-0xc4fffffff]&lt;BR /&gt;[ 0.482812] pci_bus 0000:00: resource 4 [io 0x10000-0x1ffff]&lt;BR /&gt;[ 0.482816] pci_bus 0000:00: resource 5 [mem 0xc40000000-0xc4fffffff]&lt;BR /&gt;[ 0.482819] pci_bus 0000:01: resource 0 [io 0x10000-0x1ffff]&lt;BR /&gt;[ 0.482823] pci_bus 0000:01: resource 1 [mem 0xc40000000-0xc4fffffff]&lt;BR /&gt;[ 0.482824] PCI: Probing PCI hardware done&lt;BR /&gt;[ 1.516030] PCI: CLS 0 bytes, default 64&lt;BR /&gt;[ 1.594297] aer 0000:00:00.0:pcie02: service driver aer loaded&lt;BR /&gt;[ 2.024312] ehci-pci: EHCI PCI platform driver&lt;BR /&gt;&lt;A href="mailto:root@t2081qds:/sys/bus/pci/devices" target="_blank"&gt;root@t2081qds:/sys/bus/pci/devices#&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Ravindra&lt;/P&gt;</description>
      <pubDate>Mon, 02 Dec 2024 10:10:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/t2081-pcie-Issue/m-p/2005064#M5088</guid>
      <dc:creator>arumilli</dc:creator>
      <dc:date>2024-12-02T10:10:00Z</dc:date>
    </item>
    <item>
      <title>Re: t2081 pcie Issue</title>
      <link>https://community.nxp.com/t5/T-Series/t2081-pcie-Issue/m-p/2005399#M5089</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Please validate your RCW configuration ( According to the SERDES configuration you selected), you can also try to test the pcie device under u-boot to se if the device is recognized with the pci commands.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Your Linux complains that it cannot assign the amount of memory the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;peripheral connected to the PCIe wants, please share complete log file in .txt format.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Dec 2024 19:49:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/t2081-pcie-Issue/m-p/2005399#M5089</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2024-12-02T19:49:36Z</dc:date>
    </item>
    <item>
      <title>Re: t2081 pcie Issue</title>
      <link>https://community.nxp.com/t5/T-Series/t2081-pcie-Issue/m-p/2006669#M5093</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Here i attached the full log file&lt;/P&gt;</description>
      <pubDate>Wed, 04 Dec 2024 06:35:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/t2081-pcie-Issue/m-p/2006669#M5093</guid>
      <dc:creator>arumilli</dc:creator>
      <dc:date>2024-12-04T06:35:56Z</dc:date>
    </item>
    <item>
      <title>Re: t2081 pcie Issue</title>
      <link>https://community.nxp.com/t5/T-Series/t2081-pcie-Issue/m-p/2059568#M5170</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Any Update on This regarding PCI issue in T2081 board&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ravindra.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Mar 2025 13:19:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/t2081-pcie-Issue/m-p/2059568#M5170</guid>
      <dc:creator>arumilli</dc:creator>
      <dc:date>2025-03-11T13:19:19Z</dc:date>
    </item>
    <item>
      <title>Re: t2081 pcie Issue</title>
      <link>https://community.nxp.com/t5/T-Series/t2081-pcie-Issue/m-p/2059574#M5171</link>
      <description>Hello,&lt;BR /&gt;Is there any update regarding the PCI issue?</description>
      <pubDate>Tue, 11 Mar 2025 13:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/t2081-pcie-Issue/m-p/2059574#M5171</guid>
      <dc:creator>arumilli</dc:creator>
      <dc:date>2025-03-11T13:27:33Z</dc:date>
    </item>
  </channel>
</rss>