<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 Re: Probability for CPU producing identical data in lockstep architecture?</title>
    <link>https://community.nxp.com/t5/T-Series/Probability-for-CPU-producing-identical-data-in-lockstep/m-p/2001845#M5085</link>
    <description>&lt;P&gt;There are no hardware provisions for that in any T-series or P-series processor and no recommendations for implementing it are available.&lt;/P&gt;</description>
    <pubDate>Tue, 26 Nov 2024 09:32:05 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2024-11-26T09:32:05Z</dc:date>
    <item>
      <title>Probability for CPU producing identical data in lockstep architecture?</title>
      <link>https://community.nxp.com/t5/T-Series/Probability-for-CPU-producing-identical-data-in-lockstep/m-p/2000837#M5084</link>
      <description>&lt;P&gt;If there is lockstep design to monitor the CPU T2081 output, what is the probability defeating the lockstep mechanism such as producing the identical erroneous data?&lt;/P&gt;&lt;P&gt;For example, if the data size of CPU output is 64 bits, could the probability of 2 CPUs producing the same erroneous data is 1/64*P(CPU0 Error)*P(CPU1 Error)?&lt;/P&gt;&lt;P&gt;The factor 1/data length could be used? Or what is the factor if not?&lt;/P&gt;</description>
      <pubDate>Mon, 25 Nov 2024 08:09:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Probability-for-CPU-producing-identical-data-in-lockstep/m-p/2000837#M5084</guid>
      <dc:creator>Xingzi</dc:creator>
      <dc:date>2024-11-25T08:09:26Z</dc:date>
    </item>
    <item>
      <title>Re: Probability for CPU producing identical data in lockstep architecture?</title>
      <link>https://community.nxp.com/t5/T-Series/Probability-for-CPU-producing-identical-data-in-lockstep/m-p/2001845#M5085</link>
      <description>&lt;P&gt;There are no hardware provisions for that in any T-series or P-series processor and no recommendations for implementing it are available.&lt;/P&gt;</description>
      <pubDate>Tue, 26 Nov 2024 09:32:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Probability-for-CPU-producing-identical-data-in-lockstep/m-p/2001845#M5085</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-11-26T09:32:05Z</dc:date>
    </item>
  </channel>
</rss>