<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 Re: Debugging u-boot from DDR  T2081 processor</title>
    <link>https://community.nxp.com/t5/T-Series/Debugging-u-boot-from-DDR-T2081-processor/m-p/1986291#M5076</link>
    <description>&lt;P&gt;We require this change because burning U-Boot into NOR via CodeWarrior is taking a significant amount of time. Loading U-Boot into DDR would provide us with a faster turnaround time for our development process.&lt;/P&gt;</description>
    <pubDate>Fri, 01 Nov 2024 13:30:16 GMT</pubDate>
    <dc:creator>Ashok0999</dc:creator>
    <dc:date>2024-11-01T13:30:16Z</dc:date>
    <item>
      <title>Debugging u-boot from DDR  T2081 processor</title>
      <link>https://community.nxp.com/t5/T-Series/Debugging-u-boot-from-DDR-T2081-processor/m-p/1986288#M5075</link>
      <description>&lt;P&gt;Hi Nxp Team,&lt;BR /&gt;&lt;BR /&gt;We have successfully built U-Boot for the NOR flash on the T2081 processor and have reached the U-Boot prompt. However, our Ethernet is currently not operational, making it challenging to perform further debugging.&lt;/P&gt;&lt;P&gt;To facilitate our debugging process, we would like to compile U-Boot to run from DDR, as we can load files into DDR via USB.&lt;/P&gt;&lt;P&gt;Could you please advise on the appropriate compilation options to enable this configuration?&lt;/P&gt;</description>
      <pubDate>Fri, 01 Nov 2024 13:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Debugging-u-boot-from-DDR-T2081-processor/m-p/1986288#M5075</guid>
      <dc:creator>Ashok0999</dc:creator>
      <dc:date>2024-11-01T13:26:40Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging u-boot from DDR  T2081 processor</title>
      <link>https://community.nxp.com/t5/T-Series/Debugging-u-boot-from-DDR-T2081-processor/m-p/1986291#M5076</link>
      <description>&lt;P&gt;We require this change because burning U-Boot into NOR via CodeWarrior is taking a significant amount of time. Loading U-Boot into DDR would provide us with a faster turnaround time for our development process.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Nov 2024 13:30:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Debugging-u-boot-from-DDR-T2081-processor/m-p/1986291#M5076</guid>
      <dc:creator>Ashok0999</dc:creator>
      <dc:date>2024-11-01T13:30:16Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging u-boot from DDR  T2081 processor</title>
      <link>https://community.nxp.com/t5/T-Series/Debugging-u-boot-from-DDR-T2081-processor/m-p/1989469#M5079</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The available procedure is&amp;nbsp; "RAMboot process using CodeWarrior"&lt;/P&gt;
&lt;P&gt;Please check chapter&amp;nbsp;6 U-Boot RAMboot in T1040D4RDB (It can also be used on boards that do not support SD/eMMC) in the attached guide.&lt;/P&gt;
&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 21:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Debugging-u-boot-from-DDR-T2081-processor/m-p/1989469#M5079</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2024-11-06T21:53:46Z</dc:date>
    </item>
  </channel>
</rss>