<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: e5500 timing when computing with subnormals (denorm) in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/e5500-timing-when-computing-with-subnormals-denorm/m-p/1916434#M4982</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;For FPU it says, Counts extra cycles delay due to denormalized inputs. If there is one, this is incremented 4 times, Two operands increments it 5 times. This shows the real penalty due to denorms, not just how often they occur.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 24 Jul 2024 18:31:03 GMT</pubDate>
    <dc:creator>Oswalag</dc:creator>
    <dc:date>2024-07-24T18:31:03Z</dc:date>
    <item>
      <title>e5500 timing when computing with subnormals (denorm)</title>
      <link>https://community.nxp.com/t5/T-Series/e5500-timing-when-computing-with-subnormals-denorm/m-p/1914192#M4981</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;While playing with single-precision floating-point arith in a T1040, it seemed to me that my algorithms were a little slower when subnormal values were involved. However, I could not find any specifics on subnormal instruction timing in the e5500 reference manual - is this information available anywhere else? Or timing is the same for normalized or subnormal numbers and there is a flaw in my experiment?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jul 2024 13:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/e5500-timing-when-computing-with-subnormals-denorm/m-p/1914192#M4981</guid>
      <dc:creator>ricardofranca</dc:creator>
      <dc:date>2024-07-22T13:33:05Z</dc:date>
    </item>
    <item>
      <title>Re: e5500 timing when computing with subnormals (denorm)</title>
      <link>https://community.nxp.com/t5/T-Series/e5500-timing-when-computing-with-subnormals-denorm/m-p/1916434#M4982</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;For FPU it says, Counts extra cycles delay due to denormalized inputs. If there is one, this is incremented 4 times, Two operands increments it 5 times. This shows the real penalty due to denorms, not just how often they occur.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jul 2024 18:31:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/e5500-timing-when-computing-with-subnormals-denorm/m-p/1916434#M4982</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2024-07-24T18:31:03Z</dc:date>
    </item>
  </channel>
</rss>