<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic T1024RDB ASLEEP Led is On Always in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T1024RDB-ASLEEP-Led-is-On-Always/m-p/1900186#M4956</link>
    <description>&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;İ have issue with t1024rdb board, when i powered up the board, ASLEEP led is always on and&amp;nbsp; no message in console. Then i tried to connect with peedi jtag adapter i failed with "BYPASS check failed" message as you can see. I checked dip switches but all of them is set default state. How can i detect the problem, do you have any clue ?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="peedi_t1024.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/287294iC12379AD14374EB3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="peedi_t1024.PNG" alt="peedi_t1024.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;peedi_t1024.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Fri, 05 Jul 2024 11:41:00 GMT</pubDate>
    <dc:creator>mehmet2793</dc:creator>
    <dc:date>2024-07-05T11:41:00Z</dc:date>
    <item>
      <title>T1024RDB ASLEEP Led is On Always</title>
      <link>https://community.nxp.com/t5/T-Series/T1024RDB-ASLEEP-Led-is-On-Always/m-p/1900186#M4956</link>
      <description>&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;İ have issue with t1024rdb board, when i powered up the board, ASLEEP led is always on and&amp;nbsp; no message in console. Then i tried to connect with peedi jtag adapter i failed with "BYPASS check failed" message as you can see. I checked dip switches but all of them is set default state. How can i detect the problem, do you have any clue ?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="peedi_t1024.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/287294iC12379AD14374EB3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="peedi_t1024.PNG" alt="peedi_t1024.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;peedi_t1024.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jul 2024 11:41:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1024RDB-ASLEEP-Led-is-On-Always/m-p/1900186#M4956</guid>
      <dc:creator>mehmet2793</dc:creator>
      <dc:date>2024-07-05T11:41:00Z</dc:date>
    </item>
    <item>
      <title>Re: T1024RDB ASLEEP Led is On Always</title>
      <link>https://community.nxp.com/t5/T-Series/T1024RDB-ASLEEP-Led-is-On-Always/m-p/1900544#M4958</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235981"&gt;@mehmet2793&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please inform us which SDK version are you using?&lt;/P&gt;
&lt;P&gt;We will be aware for your kind reply.&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Hector&lt;/P&gt;</description>
      <pubDate>Sat, 06 Jul 2024 00:51:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1024RDB-ASLEEP-Led-is-On-Always/m-p/1900544#M4958</guid>
      <dc:creator>Hector_Villarruel</dc:creator>
      <dc:date>2024-07-06T00:51:57Z</dc:date>
    </item>
  </channel>
</rss>