<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックRe: Communication with FPGA using T1013 IFC</title>
    <link>https://community.nxp.com/t5/T-Series/Communication-with-FPGA-using-T1013-IFC/m-p/1876156#M4895</link>
    <description>&lt;P&gt;&lt;SPAN&gt;The equivalent in the T1013 is IFC.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;"Low speed" in this context means something similar to the 66MHz of a MPC5777C EBI.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 28 May 2024 08:52:37 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2024-05-28T08:52:37Z</dc:date>
    <item>
      <title>Communication with FPGA using T1013 IFC</title>
      <link>https://community.nxp.com/t5/T-Series/Communication-with-FPGA-using-T1013-IFC/m-p/1872022#M4889</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am assessing a possible use of the T1013 in an application that performs access to an FPGA. My hardware/firmware friends use the EBI in 5xxx devices and the eLBC in the P1013; I would like to know if the equivalent in the T1013 would be the IFC.&lt;/P&gt;&lt;P&gt;As the T1023/24/13/14 states "The IFC supports both NAND and NOR flash, as well as a&lt;BR /&gt;general purpose memory-mapped interface for connecting low speed ASICs and FPGAs", I was wondering if "low speed" in this context means something similar to the 66MHz of a MPC5777C EBI or something much slower.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Thu, 23 May 2024 13:09:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Communication-with-FPGA-using-T1013-IFC/m-p/1872022#M4889</guid>
      <dc:creator>ricardofranca</dc:creator>
      <dc:date>2024-05-23T13:09:19Z</dc:date>
    </item>
    <item>
      <title>Re: Communication with FPGA using T1013 IFC</title>
      <link>https://community.nxp.com/t5/T-Series/Communication-with-FPGA-using-T1013-IFC/m-p/1876156#M4895</link>
      <description>&lt;P&gt;&lt;SPAN&gt;The equivalent in the T1013 is IFC.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;"Low speed" in this context means something similar to the 66MHz of a MPC5777C EBI.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 28 May 2024 08:52:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Communication-with-FPGA-using-T1013-IFC/m-p/1876156#M4895</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-05-28T08:52:37Z</dc:date>
    </item>
  </channel>
</rss>