<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: T1024 IFC do not work in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T1024-IFC-do-not-work/m-p/1702697#M4706</link>
    <description>&lt;P&gt;I am sorry for the late reply.&lt;/P&gt;&lt;P&gt;My problem was with the pull-down resistor on pin D8.(IFC_A20)&lt;/P&gt;&lt;P&gt;After removing it, my borad worked well.&lt;/P&gt;&lt;P&gt;I designed a board by referring to the T1024RDB schematic.&lt;/P&gt;&lt;P&gt;The resistor is R13 on sheet 4.&lt;/P&gt;</description>
    <pubDate>Thu, 10 Aug 2023 06:57:51 GMT</pubDate>
    <dc:creator>hankjeon</dc:creator>
    <dc:date>2023-08-10T06:57:51Z</dc:date>
    <item>
      <title>T1024 IFC do not work</title>
      <link>https://community.nxp.com/t5/T-Series/T1024-IFC-do-not-work/m-p/1513732#M4514</link>
      <description>&lt;P&gt;I made a custom board using T1024, and set RCW source for 16-bit NOR Flash.&lt;/P&gt;&lt;P&gt;However, CS0# signal keeps HIGH during POR sequence.&lt;/P&gt;&lt;P&gt;From Trace32 I confirmed RCW source is set correctly.&lt;/P&gt;&lt;P&gt;Using Trace32, CPU registers and DDR can be accessed.&lt;/P&gt;&lt;P&gt;What am I missed? What do I check first ?&lt;/P&gt;</description>
      <pubDate>Thu, 01 Sep 2022 06:04:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1024-IFC-do-not-work/m-p/1513732#M4514</guid>
      <dc:creator>hankjeon</dc:creator>
      <dc:date>2022-09-01T06:04:32Z</dc:date>
    </item>
    <item>
      <title>Re: T1024 IFC do not work</title>
      <link>https://community.nxp.com/t5/T-Series/T1024-IFC-do-not-work/m-p/1523743#M4529</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205692"&gt;@hankjeon&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I highly recommend you to check the RCW file, could you share with me your RCW file?&lt;BR /&gt;I think the problem is in the RCW, I believe that the NOR flash is not configured correctly on the RCW,&lt;BR /&gt;On the RCW source section in Code Warrior, you have to select "Serial NOR", then click on the check box and then and check for errors.&lt;/P&gt;
&lt;P&gt;Please refer to the attached image for reference.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Hector Villarruel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Sep 2022 18:10:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1024-IFC-do-not-work/m-p/1523743#M4529</guid>
      <dc:creator>Hector_Villarruel</dc:creator>
      <dc:date>2022-09-16T18:10:41Z</dc:date>
    </item>
    <item>
      <title>Re: T1024 IFC do not work</title>
      <link>https://community.nxp.com/t5/T-Series/T1024-IFC-do-not-work/m-p/1699738#M4704</link>
      <description>&lt;P&gt;I also meet this problem,how do you resolve this problem&lt;/P&gt;</description>
      <pubDate>Sun, 06 Aug 2023 22:24:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1024-IFC-do-not-work/m-p/1699738#M4704</guid>
      <dc:creator>Jaygao</dc:creator>
      <dc:date>2023-08-06T22:24:04Z</dc:date>
    </item>
    <item>
      <title>Re: T1024 IFC do not work</title>
      <link>https://community.nxp.com/t5/T-Series/T1024-IFC-do-not-work/m-p/1699739#M4705</link>
      <description>is it relative to the rcw flie?the cs0 should keep low when the power on if set as the rcw source as 16bit nor flash</description>
      <pubDate>Sun, 06 Aug 2023 22:28:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1024-IFC-do-not-work/m-p/1699739#M4705</guid>
      <dc:creator>Jaygao</dc:creator>
      <dc:date>2023-08-06T22:28:48Z</dc:date>
    </item>
    <item>
      <title>Re: T1024 IFC do not work</title>
      <link>https://community.nxp.com/t5/T-Series/T1024-IFC-do-not-work/m-p/1702697#M4706</link>
      <description>&lt;P&gt;I am sorry for the late reply.&lt;/P&gt;&lt;P&gt;My problem was with the pull-down resistor on pin D8.(IFC_A20)&lt;/P&gt;&lt;P&gt;After removing it, my borad worked well.&lt;/P&gt;&lt;P&gt;I designed a board by referring to the T1024RDB schematic.&lt;/P&gt;&lt;P&gt;The resistor is R13 on sheet 4.&lt;/P&gt;</description>
      <pubDate>Thu, 10 Aug 2023 06:57:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1024-IFC-do-not-work/m-p/1702697#M4706</guid>
      <dc:creator>hankjeon</dc:creator>
      <dc:date>2023-08-10T06:57:51Z</dc:date>
    </item>
  </channel>
</rss>