<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: T2080 Core power supply in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T2080-Core-power-supply/m-p/1652031#M4640</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213571"&gt;@Har_ika30&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;You can select regulator based on your current requirement. Based on your requirement which 20A if you are selecting 30A then its fine. &lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mrudang&lt;/P&gt;</description>
    <pubDate>Wed, 17 May 2023 11:21:55 GMT</pubDate>
    <dc:creator>mrudangshelat-13</dc:creator>
    <dc:date>2023-05-17T11:21:55Z</dc:date>
    <item>
      <title>T2080 Core power supply</title>
      <link>https://community.nxp.com/t5/T-Series/T2080-Core-power-supply/m-p/1651116#M4639</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Iam using T2080 processor in my design, the core supply is taking around 20A of current.&lt;/P&gt;&lt;P&gt;I have selected a part with 60A part with dual outputs (each output support 30A). One output of the regulator will be using for T2080 Core supply and other output to other source.&lt;/P&gt;&lt;P&gt;Can i do it in that way? or Complete 60A regulator is required for T2080.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And in T2080 evaluation board, T2080 needs max 25A for the core but still kept 60A regulator.&lt;/P&gt;&lt;P&gt;Can anyone tell me why 60A regulator has been kept in the evaluation board?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;Harika B N V L&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 May 2023 11:19:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080-Core-power-supply/m-p/1651116#M4639</guid>
      <dc:creator>Har_ika30</dc:creator>
      <dc:date>2023-05-16T11:19:17Z</dc:date>
    </item>
    <item>
      <title>Re: T2080 Core power supply</title>
      <link>https://community.nxp.com/t5/T-Series/T2080-Core-power-supply/m-p/1652031#M4640</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213571"&gt;@Har_ika30&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;You can select regulator based on your current requirement. Based on your requirement which 20A if you are selecting 30A then its fine. &lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mrudang&lt;/P&gt;</description>
      <pubDate>Wed, 17 May 2023 11:21:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080-Core-power-supply/m-p/1652031#M4640</guid>
      <dc:creator>mrudangshelat-13</dc:creator>
      <dc:date>2023-05-17T11:21:55Z</dc:date>
    </item>
  </channel>
</rss>