<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックT1042RDB bring-up error (error writing memory [CCS last error: Scan timeout])</title>
    <link>https://community.nxp.com/t5/T-Series/T1042RDB-bring-up-error-error-writing-memory-CCS-last-error-Scan/m-p/1607964#M4583</link>
    <description>&lt;P&gt;Please refer to the diagnostic information as attached. Any advice? Thanks.&lt;/P&gt;</description>
    <pubDate>Wed, 01 Mar 2023 23:13:44 GMT</pubDate>
    <dc:creator>Ray_33</dc:creator>
    <dc:date>2023-03-01T23:13:44Z</dc:date>
    <item>
      <title>T1042RDB bring-up error (error writing memory [CCS last error: Scan timeout])</title>
      <link>https://community.nxp.com/t5/T-Series/T1042RDB-bring-up-error-error-writing-memory-CCS-last-error-Scan/m-p/1607964#M4583</link>
      <description>&lt;P&gt;Please refer to the diagnostic information as attached. Any advice? Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 01 Mar 2023 23:13:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1042RDB-bring-up-error-error-writing-memory-CCS-last-error-Scan/m-p/1607964#M4583</guid>
      <dc:creator>Ray_33</dc:creator>
      <dc:date>2023-03-01T23:13:44Z</dc:date>
    </item>
    <item>
      <title>Re: T1042RDB bring-up error (error writing memory [CCS last error: Scan timeout])</title>
      <link>https://community.nxp.com/t5/T-Series/T1042RDB-bring-up-error-error-writing-memory-CCS-last-error-Scan/m-p/1610341#M4585</link>
      <description>&lt;P&gt;Hello Ray_33&lt;/P&gt;
&lt;P&gt;Hope this post finds you well,&lt;/P&gt;
&lt;P&gt;Could you please be so kind to answer the following questions?&lt;/P&gt;
&lt;P&gt;Could you please provide more details about your connection?&lt;/P&gt;
&lt;P&gt;Are connecting the CodeWarrior Tap over USB or Ethernet?&lt;/P&gt;
&lt;P&gt;Are you using Windows or linux ?&lt;/P&gt;
&lt;P&gt;Which version of linux or Windows are you currently using to perform the test?&lt;/P&gt;
&lt;P&gt;I will be waiting for your kind update,&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Hector Villarruel&lt;/P&gt;</description>
      <pubDate>Tue, 07 Mar 2023 00:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1042RDB-bring-up-error-error-writing-memory-CCS-last-error-Scan/m-p/1610341#M4585</guid>
      <dc:creator>Hector_Villarruel</dc:creator>
      <dc:date>2023-03-07T00:00:58Z</dc:date>
    </item>
    <item>
      <title>Re: T1042RDB bring-up error (error writing memory [CCS last error: Scan timeout])</title>
      <link>https://community.nxp.com/t5/T-Series/T1042RDB-bring-up-error-error-writing-memory-CCS-last-error-Scan/m-p/1611188#M4586</link>
      <description>&lt;P&gt;CodeWarrior Tap is connected over USB as indicated by the starting guide.&lt;/P&gt;&lt;P&gt;I'm using Windows 10, 64 bit OS.&lt;/P&gt;&lt;P&gt;Please feel free to let me know if you need more information.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Mar 2023 22:48:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1042RDB-bring-up-error-error-writing-memory-CCS-last-error-Scan/m-p/1611188#M4586</guid>
      <dc:creator>Ray_33</dc:creator>
      <dc:date>2023-03-07T22:48:44Z</dc:date>
    </item>
    <item>
      <title>Re: T1042RDB bring-up error (error writing memory [CCS last error: Scan timeout])</title>
      <link>https://community.nxp.com/t5/T-Series/T1042RDB-bring-up-error-error-writing-memory-CCS-last-error-Scan/m-p/1613243#M4593</link>
      <description>&lt;P&gt;Hello Ray_33&lt;/P&gt;
&lt;P&gt;Unfortunately, the only connection available is via ethernet for Windows 10, 64 bit OS.&lt;/P&gt;
&lt;P&gt;Have a wonderful day,&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Hector Villarruel&lt;/P&gt;</description>
      <pubDate>Fri, 10 Mar 2023 16:13:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1042RDB-bring-up-error-error-writing-memory-CCS-last-error-Scan/m-p/1613243#M4593</guid>
      <dc:creator>Hector_Villarruel</dc:creator>
      <dc:date>2023-03-10T16:13:02Z</dc:date>
    </item>
    <item>
      <title>Re: T1042RDB bring-up error (error writing memory [CCS last error: Scan timeout])</title>
      <link>https://community.nxp.com/t5/T-Series/T1042RDB-bring-up-error-error-writing-memory-CCS-last-error-Scan/m-p/1615243#M4594</link>
      <description>&lt;P&gt;Hi Hector,&lt;/P&gt;&lt;P&gt;Thanks for the reply. I did try to configure TAP as ethernet access, but it seems I still got same issue. The connecting status shows good, but once it passed to T1042RDB_init_core.tcl, the debug process will halt with below information: "No source available for "0x00000000FFFFFFFC (0x00000000FFFFFFFC)()". Please see below screenshot.&lt;/P&gt;&lt;P&gt;Any further suggestion?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Ray_33_0-1678831701757.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/214581iDF52D8A40011E1AB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Ray_33_0-1678831701757.png" alt="Ray_33_0-1678831701757.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Ray_33_0-1678831701757.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Mar 2023 22:09:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1042RDB-bring-up-error-error-writing-memory-CCS-last-error-Scan/m-p/1615243#M4594</guid>
      <dc:creator>Ray_33</dc:creator>
      <dc:date>2023-03-14T22:09:07Z</dc:date>
    </item>
    <item>
      <title>Re: T1042RDB bring-up error (error writing memory [CCS last error: Scan timeout])</title>
      <link>https://community.nxp.com/t5/T-Series/T1042RDB-bring-up-error-error-writing-memory-CCS-last-error-Scan/m-p/1617836#M4601</link>
      <description>&lt;P&gt;Hello Ray_33&lt;BR /&gt;Hope this post finds you well,&lt;/P&gt;
&lt;P&gt;Please close CW and delete .metadata folder from your workspace. Then create a new bareboard project using the new project wizard and select T1042. Then download the default application in your board.&lt;/P&gt;
&lt;P&gt;What could be the cause of this problem ?&lt;BR /&gt;- software installed,&lt;BR /&gt;- project,&lt;BR /&gt;- interface,&lt;BR /&gt;- board.&lt;/P&gt;
&lt;P&gt;To check the different point I recommend to use a sample project.&lt;BR /&gt;You can create a sample with the project Wizard &lt;BR /&gt;File + New + CodeWarrior Bareboard Project Wizard&lt;BR /&gt;Here you can create an example with all your hardware configuration: interface + board.&lt;BR /&gt;For this test I recommend to use an eval board.&lt;BR /&gt;This will valid the Tool installation and Interface.&lt;BR /&gt;If this project example is running the problem could be on the project or your own board.&lt;/P&gt;
&lt;P&gt;Now you can replace the eval board with your board.&lt;BR /&gt;If this example project is running on your board, the problem is linked to your project.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Hector Villarruel&lt;/P&gt;</description>
      <pubDate>Fri, 17 Mar 2023 18:15:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1042RDB-bring-up-error-error-writing-memory-CCS-last-error-Scan/m-p/1617836#M4601</guid>
      <dc:creator>Hector_Villarruel</dc:creator>
      <dc:date>2023-03-17T18:15:43Z</dc:date>
    </item>
  </channel>
</rss>