<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックT1023WLAN Core not responding error</title>
    <link>https://community.nxp.com/t5/T-Series/T1023WLAN-Core-not-responding-error/m-p/1546510#M4533</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I corrupted the u-boot flash on the t1023wlan board and am trying to re-flash the board using the jtag connector and codewarrior TAP. However, when I try to do so, I repeatedly get&amp;nbsp;"error: T1020: Core not responding". I have tried the default jtag chains as well as a custom chain based on the rcw I recovered from the board when it was working but none of these worked.&lt;/P&gt;</description>
    <pubDate>Mon, 31 Oct 2022 23:09:20 GMT</pubDate>
    <dc:creator>WesleyVong</dc:creator>
    <dc:date>2022-10-31T23:09:20Z</dc:date>
    <item>
      <title>T1023WLAN Core not responding error</title>
      <link>https://community.nxp.com/t5/T-Series/T1023WLAN-Core-not-responding-error/m-p/1546510#M4533</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I corrupted the u-boot flash on the t1023wlan board and am trying to re-flash the board using the jtag connector and codewarrior TAP. However, when I try to do so, I repeatedly get&amp;nbsp;"error: T1020: Core not responding". I have tried the default jtag chains as well as a custom chain based on the rcw I recovered from the board when it was working but none of these worked.&lt;/P&gt;</description>
      <pubDate>Mon, 31 Oct 2022 23:09:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1023WLAN-Core-not-responding-error/m-p/1546510#M4533</guid>
      <dc:creator>WesleyVong</dc:creator>
      <dc:date>2022-10-31T23:09:20Z</dc:date>
    </item>
    <item>
      <title>Re: T1023WLAN Core not responding error</title>
      <link>https://community.nxp.com/t5/T-Series/T1023WLAN-Core-not-responding-error/m-p/1547407#M4534</link>
      <description>&lt;P&gt;&lt;SPAN&gt;In your CCS log, there is error at JTAG diagnostics,&amp;nbsp;Error measuring IR length.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If the test fails to measure the length of the instruction register, then an error, Error measuring IR length, is thrown.&lt;BR /&gt;The error might be due to one or more of the following reasons:&lt;BR /&gt;• TRST stuck low: This may hold the target JTAG logic in reset, preventing any shifts to occur.&lt;BR /&gt;• TMS disconnected or stuck: This may prevent the target from making any JTAG state changes.&lt;BR /&gt;• TCK disconnected or stuck: This may prevent any state changes or clocking of data.&lt;BR /&gt;• TDI disconnected or stuck: This may prevent the test pattern data from getting into the target.&lt;BR /&gt;• TDO disconnected or stuck: This may prevent the test pattern data from getting out of the target.&lt;BR /&gt;If the test fails, then it is possible that there is a physical connection problem with the JTAG pins, or the JTAG frequency is too high.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please try whether it is helpful to configure "JTAG clock speed" lower from Run-&amp;gt;Debug Configurations-&amp;gt;&amp;lt;project&amp;gt;-core00_RAM_T1023_Download-&amp;gt;Edit-&amp;gt;Connection-&amp;gt;JTAG settings.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Nov 2022 05:13:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1023WLAN-Core-not-responding-error/m-p/1547407#M4534</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-11-02T05:13:06Z</dc:date>
    </item>
    <item>
      <title>Re: T1023WLAN Core not responding error</title>
      <link>https://community.nxp.com/t5/T-Series/T1023WLAN-Core-not-responding-error/m-p/1547883#M4535</link>
      <description>&lt;P&gt;Thanks, it turns out the board I was using was broken. I switched it out and it works now!&lt;/P&gt;</description>
      <pubDate>Wed, 02 Nov 2022 18:08:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1023WLAN-Core-not-responding-error/m-p/1547883#M4535</guid>
      <dc:creator>WesleyVong</dc:creator>
      <dc:date>2022-11-02T18:08:24Z</dc:date>
    </item>
  </channel>
</rss>