<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Cann't boot T2080QDS-PA board,Uboot show &amp;quot;Waiting for D_INIT timeout. Memory may not work.&amp;amp; in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/Cann-t-boot-T2080QDS-PA-board-Uboot-show-quot-Waiting-for-D-INIT/m-p/1522081#M4524</link>
    <description>&lt;P&gt;The Ram timings are off. I have the same issue with T2080-QDS 1U board. Doing a reset seems to get you past the issue but it is not a good solution. check your ram timings..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 14 Sep 2022 16:01:17 GMT</pubDate>
    <dc:creator>Dsiebert</dc:creator>
    <dc:date>2022-09-14T16:01:17Z</dc:date>
    <item>
      <title>Cann't boot T2080QDS-PA board,Uboot show "Waiting for D_INIT timeout. Memory may not work."</title>
      <link>https://community.nxp.com/t5/T-Series/Cann-t-boot-T2080QDS-PA-board-Uboot-show-quot-Waiting-for-D-INIT/m-p/1519624#M4520</link>
      <description>&lt;P&gt;Dear，&lt;/P&gt;&lt;P&gt;I have just started working on a T2080QDS-PA board. the board failing in the U-boot sequence immediately after detecting the DDR3 ram ("Waiting for D_INIT timeout. Memory may not work."). and all configuration switches and&amp;nbsp;jump as default reference&amp;nbsp;QorIQ T2080 Development SystemQuick Start Guide,I replaced the new T2080 CPU and DDR Moduler,but the issue same before,and used the Flash Programmer(Superpro6100) to program the orignal image (from QorIQ SDK2.0/SDK1.9/SDK1.8/SDK1.7) to NorFlash,but can't close the issue,Would you give me some suggestions?thanks!&lt;/P&gt;&lt;P&gt;lzh&lt;/P&gt;&lt;P&gt;======================================================&lt;/P&gt;&lt;P&gt;U-Boot 2016.012.0+ga9b437f (May 15 2016 - 18:12:07 +0800)&lt;/P&gt;&lt;P&gt;CPU0: T2080, Version: 1.1, (0x85300011)&lt;BR /&gt;Core: e6500, Version: 2.0, (0x80400120)&lt;BR /&gt;Clock Configuration:&lt;BR /&gt;CPU0:1800 MHz, CPU1:1800 MHz, CPU2:1800 MHz, CPU3:1800 MHz,&lt;BR /&gt;CCB:600 MHz,&lt;BR /&gt;DDR:933.333 MHz (1866.667 MT/s data rate) (Asynchronous), IFC:150 MHz&lt;BR /&gt;FMAN1: 700 MHz&lt;BR /&gt;QMAN: 300 MHz&lt;BR /&gt;PME: 600 MHz&lt;BR /&gt;L1: D-cache 32 KiB enabled&lt;BR /&gt;I-cache 32 KiB enabled&lt;BR /&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 0c070012 0e000000 00000000 00000000&lt;BR /&gt;00000010: 66150002 00000000 ec027000 c1000000&lt;BR /&gt;00000020: 00000000 00000000 00000000 000307fc&lt;BR /&gt;00000030: 00000000 00000000 00000000 00000004&lt;BR /&gt;I2C: ready&lt;BR /&gt;Board: T2080QDS, Sys ID: 0x28, Board Arch: V1, Board Version: A, boot from vBank0&lt;BR /&gt;FPGA: v7 (T1040QDS_2013_1120_1155), build 243 on Wed Nov 20 17:55:56 2013&lt;BR /&gt;SERDES Reference Clocks:&lt;BR /&gt;SD1_CLK1=156.25MHZ, SD1_CLK2=100.00MHz&lt;BR /&gt;SD2_CLK1=100.00MHz, SD2_CLK2=100.00MHz&lt;BR /&gt;SPI: ready&lt;BR /&gt;DRAM: Initializing....using SPD&lt;BR /&gt;Detected UDIMM 9JSF25672AZ-2G1K1&lt;BR /&gt;Waiting for D_INIT timeout. Memory may not work.&lt;/P&gt;&lt;P&gt;===================================================================&lt;/P&gt;</description>
      <pubDate>Thu, 08 Sep 2022 23:59:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Cann-t-boot-T2080QDS-PA-board-Uboot-show-quot-Waiting-for-D-INIT/m-p/1519624#M4520</guid>
      <dc:creator>leizhihualqytvw</dc:creator>
      <dc:date>2022-09-08T23:59:14Z</dc:date>
    </item>
    <item>
      <title>Re: Cann't boot T2080QDS-PA board,Uboot show "Waiting for D_INIT timeout. Memory may not work.&amp;</title>
      <link>https://community.nxp.com/t5/T-Series/Cann-t-boot-T2080QDS-PA-board-Uboot-show-quot-Waiting-for-D-INIT/m-p/1522081#M4524</link>
      <description>&lt;P&gt;The Ram timings are off. I have the same issue with T2080-QDS 1U board. Doing a reset seems to get you past the issue but it is not a good solution. check your ram timings..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Sep 2022 16:01:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Cann-t-boot-T2080QDS-PA-board-Uboot-show-quot-Waiting-for-D-INIT/m-p/1522081#M4524</guid>
      <dc:creator>Dsiebert</dc:creator>
      <dc:date>2022-09-14T16:01:17Z</dc:date>
    </item>
    <item>
      <title>Re: Cann't boot T2080QDS-PA board,Uboot show "Waiting for D_INIT timeout. Memory may not work.&amp;</title>
      <link>https://community.nxp.com/t5/T-Series/Cann-t-boot-T2080QDS-PA-board-Uboot-show-quot-Waiting-for-D-INIT/m-p/1535772#M4530</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;leizhihualqytvw!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You have to set the Linux SDK step by step.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;For your board you can see the steps following the link.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://docs.nxp.com/bundle/GUID-39A0A446-70E5-4ED7-A580-E7508B61A5F1/page/GUID-30F66DE6-BAD0-4ED6-A122-FF58A9EB3ABD.html" target="_blank"&gt;Welcome to the Linux SDK for QorIQ Processors Knowledge Center | QorIQ SDK v2.0-1703 Documentation | NXP Semiconductors&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Oct 2022 16:23:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Cann-t-boot-T2080QDS-PA-board-Uboot-show-quot-Waiting-for-D-INIT/m-p/1535772#M4530</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2022-10-11T16:23:26Z</dc:date>
    </item>
    <item>
      <title>Re: Cann't boot T2080QDS-PA board,Uboot show "Waiting for D_INIT timeout. Memory may not work.&amp;</title>
      <link>https://community.nxp.com/t5/T-Series/Cann-t-boot-T2080QDS-PA-board-Uboot-show-quot-Waiting-for-D-INIT/m-p/1593816#M4575</link>
      <description>&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;Have you been resolve this problem. I had the trouble the same as you with custom board use b4860&lt;/P&gt;&lt;P&gt;Thanks and brgs&lt;/P&gt;</description>
      <pubDate>Mon, 06 Feb 2023 08:56:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Cann-t-boot-T2080QDS-PA-board-Uboot-show-quot-Waiting-for-D-INIT/m-p/1593816#M4575</guid>
      <dc:creator>sonminh</dc:creator>
      <dc:date>2023-02-06T08:56:05Z</dc:date>
    </item>
  </channel>
</rss>