<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックT2080RDB - CodeWarrior for PowerPC - how to create RCW?</title>
    <link>https://community.nxp.com/t5/T-Series/T2080RDB-CodeWarrior-for-PowerPC-how-to-create-RCW/m-p/1488859#M4486</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;What I really need to do is modify my existing RCW. I could do it in Notepad++ with the HexEditor plugin and manually calculate the checksum but I don't really understand what is before and after the RCW registers. What I mean is, at the start of RCW I see:&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;aa 55 aa 55 01 0e 01 00&lt;/P&gt;&lt;P&gt;Then there are all the RCW register bits.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Followed by 7 bytes of some data - what is it? Size?&lt;/P&gt;&lt;P&gt;And at the end there's one byte of checksum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;First of all, I managed to find&amp;nbsp;QCVS PBL for ARM arch but I don't seem to be able to find QCVS for PowerPC.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to create a new RCW. What is the algorithm to create it or where is the QCVS and CodeWarrior I could use to create it automatically, please?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 13 Jul 2022 15:05:53 GMT</pubDate>
    <dc:creator>MJ_STAR</dc:creator>
    <dc:date>2022-07-13T15:05:53Z</dc:date>
    <item>
      <title>T2080RDB - CodeWarrior for PowerPC - how to create RCW?</title>
      <link>https://community.nxp.com/t5/T-Series/T2080RDB-CodeWarrior-for-PowerPC-how-to-create-RCW/m-p/1488859#M4486</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;What I really need to do is modify my existing RCW. I could do it in Notepad++ with the HexEditor plugin and manually calculate the checksum but I don't really understand what is before and after the RCW registers. What I mean is, at the start of RCW I see:&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;aa 55 aa 55 01 0e 01 00&lt;/P&gt;&lt;P&gt;Then there are all the RCW register bits.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Followed by 7 bytes of some data - what is it? Size?&lt;/P&gt;&lt;P&gt;And at the end there's one byte of checksum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;First of all, I managed to find&amp;nbsp;QCVS PBL for ARM arch but I don't seem to be able to find QCVS for PowerPC.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to create a new RCW. What is the algorithm to create it or where is the QCVS and CodeWarrior I could use to create it automatically, please?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jul 2022 15:05:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080RDB-CodeWarrior-for-PowerPC-how-to-create-RCW/m-p/1488859#M4486</guid>
      <dc:creator>MJ_STAR</dc:creator>
      <dc:date>2022-07-13T15:05:53Z</dc:date>
    </item>
    <item>
      <title>Re: T2080RDB - CodeWarrior for PowerPC - how to create RCW?</title>
      <link>https://community.nxp.com/t5/T-Series/T2080RDB-CodeWarrior-for-PowerPC-how-to-create-RCW/m-p/1490982#M4489</link>
      <description>&lt;P&gt;Please download CodeWarrior for PA 10.5.1 from the following link and install it.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://drive.google.com/file/d/18YIFeSnzZlcE1ZgSNUlTYM955gh9_B56/view?usp=sharing" target="_blank"&gt;https://drive.google.com/file/d/18YIFeSnzZlcE1ZgSNUlTYM955gh9_B56/view?usp=sharing&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Then download QCVS for PA 4.5 from the following link&lt;/P&gt;
&lt;P&gt;&lt;A href="https://drive.google.com/file/d/1f0DqcGRtVlMarYG3J1HcREcZ3PaH_xgr/view?usp=sharing" target="_blank"&gt;https://drive.google.com/file/d/1f0DqcGRtVlMarYG3J1HcREcZ3PaH_xgr/view?usp=sharing&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Please open CodeWarrior IDE and install QCVS from Help-&amp;gt;Install New Software-&amp;gt;Add-&amp;gt;Archive.&lt;/P&gt;
&lt;P&gt;Please create QCVS project from File-&amp;gt;New-&amp;gt;QorIQ Configuration Project.&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jul 2022 10:03:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080RDB-CodeWarrior-for-PowerPC-how-to-create-RCW/m-p/1490982#M4489</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-07-18T10:03:09Z</dc:date>
    </item>
  </channel>
</rss>