<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic T1024 : BOOT fail in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T1024-BOOT-fail/m-p/1485797#M4482</link>
    <description>&lt;P&gt;「4.7.1 Power-On Reset Sequence」excerpt　&lt;/P&gt;&lt;P&gt;9. If the IFC's NAND Flash interface is configured as the RCW source, the reset block&lt;BR /&gt;instructs the IFC to load a boot block from Flash into the internal buffer RAM of the&lt;BR /&gt;IFC. Once complete, the reset block proceeds to instruct the Pre-Boot Loader to&lt;BR /&gt;begin reading in RCW data. Note that if the IFC NAND Flash interface reports an&lt;BR /&gt;ECC error, the device reset sequence is halted indefinitely, waiting for another&lt;BR /&gt;PORESET_B or hard reset.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is this correct in the interpretation that the CPU stops reading the SPI if there is an error in the RCW (SPI read) data?&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 07 Jul 2022 01:49:54 GMT</pubDate>
    <dc:creator>kojimiura</dc:creator>
    <dc:date>2022-07-07T01:49:54Z</dc:date>
    <item>
      <title>T1024 : BOOT fail</title>
      <link>https://community.nxp.com/t5/T-Series/T1024-BOOT-fail/m-p/1485797#M4482</link>
      <description>&lt;P&gt;「4.7.1 Power-On Reset Sequence」excerpt　&lt;/P&gt;&lt;P&gt;9. If the IFC's NAND Flash interface is configured as the RCW source, the reset block&lt;BR /&gt;instructs the IFC to load a boot block from Flash into the internal buffer RAM of the&lt;BR /&gt;IFC. Once complete, the reset block proceeds to instruct the Pre-Boot Loader to&lt;BR /&gt;begin reading in RCW data. Note that if the IFC NAND Flash interface reports an&lt;BR /&gt;ECC error, the device reset sequence is halted indefinitely, waiting for another&lt;BR /&gt;PORESET_B or hard reset.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is this correct in the interpretation that the CPU stops reading the SPI if there is an error in the RCW (SPI read) data?&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jul 2022 01:49:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1024-BOOT-fail/m-p/1485797#M4482</guid>
      <dc:creator>kojimiura</dc:creator>
      <dc:date>2022-07-07T01:49:54Z</dc:date>
    </item>
    <item>
      <title>Re: T1024 : BOOT fail</title>
      <link>https://community.nxp.com/t5/T-Series/T1024-BOOT-fail/m-p/1487964#M4483</link>
      <description>&lt;P&gt;Yes, correct.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jul 2022 08:25:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1024-BOOT-fail/m-p/1487964#M4483</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-07-12T08:25:49Z</dc:date>
    </item>
    <item>
      <title>Re: T1024 : BOOT fail</title>
      <link>https://community.nxp.com/t5/T-Series/T1024-BOOT-fail/m-p/1487968#M4484</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Thank you for answering.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jul 2022 08:30:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1024-BOOT-fail/m-p/1487968#M4484</guid>
      <dc:creator>kojimiura</dc:creator>
      <dc:date>2022-07-12T08:30:11Z</dc:date>
    </item>
  </channel>
</rss>