<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Question about T1042 board in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/Question-about-T1042-board/m-p/1481529#M4468</link>
    <description>&lt;P&gt;Hi. I'm looking for T1042D4RDB-PA Board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I heard that for code uploading and debugging I need CodeWarrior license which is IDE for T1042 board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, I found that there is CodeWarrior Tap which is Hardware.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Quesetion is for code uploading and debugging, do I need both of them (CW, CW Tap)??&lt;/P&gt;&lt;P&gt;Or do I only need CW for Code Uploading and Debugging?&lt;/P&gt;</description>
    <pubDate>Wed, 29 Jun 2022 04:44:15 GMT</pubDate>
    <dc:creator>Junho</dc:creator>
    <dc:date>2022-06-29T04:44:15Z</dc:date>
    <item>
      <title>Question about T1042 board</title>
      <link>https://community.nxp.com/t5/T-Series/Question-about-T1042-board/m-p/1481529#M4468</link>
      <description>&lt;P&gt;Hi. I'm looking for T1042D4RDB-PA Board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I heard that for code uploading and debugging I need CodeWarrior license which is IDE for T1042 board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, I found that there is CodeWarrior Tap which is Hardware.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Quesetion is for code uploading and debugging, do I need both of them (CW, CW Tap)??&lt;/P&gt;&lt;P&gt;Or do I only need CW for Code Uploading and Debugging?&lt;/P&gt;</description>
      <pubDate>Wed, 29 Jun 2022 04:44:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Question-about-T1042-board/m-p/1481529#M4468</guid>
      <dc:creator>Junho</dc:creator>
      <dc:date>2022-06-29T04:44:15Z</dc:date>
    </item>
  </channel>
</rss>