<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 Git folder for t2080rdb</title>
    <link>https://community.nxp.com/t5/T-Series/Git-folder-for-t2080rdb/m-p/1434903#M4414</link>
    <description>&lt;P&gt;Can any one send me git folder for t2080rdb? With the yocto sdk code for t2080rdb, my built code does not detect c29- EP present on the t2080rdb board . Thanks in advance&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 28 Mar 2022 15:22:53 GMT</pubDate>
    <dc:creator>monalihaware</dc:creator>
    <dc:date>2022-03-28T15:22:53Z</dc:date>
    <item>
      <title>Git folder for t2080rdb</title>
      <link>https://community.nxp.com/t5/T-Series/Git-folder-for-t2080rdb/m-p/1434903#M4414</link>
      <description>&lt;P&gt;Can any one send me git folder for t2080rdb? With the yocto sdk code for t2080rdb, my built code does not detect c29- EP present on the t2080rdb board . Thanks in advance&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Mar 2022 15:22:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Git-folder-for-t2080rdb/m-p/1434903#M4414</guid>
      <dc:creator>monalihaware</dc:creator>
      <dc:date>2022-03-28T15:22:53Z</dc:date>
    </item>
    <item>
      <title>Re: Git folder for t2080rdb</title>
      <link>https://community.nxp.com/t5/T-Series/Git-folder-for-t2080rdb/m-p/1435464#M4415</link>
      <description>&lt;P&gt;Please download and install QorIQ Linux 2.0 ISO from&amp;nbsp;&lt;A href="https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/linux-sdk-for-qoriq-processors:SDKLINUX?tab=Design_Tools_Tab#nogo" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/linux-sdk-for-qoriq-processors:SDKLINUX?tab=Design_Tools_Tab#nogo&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Please download and install&amp;nbsp;&lt;A class="download-link" href="https://freescaleesd.flexnetoperations.com/337170/637/10322637/QorIQ%20Linux%20SDK%20v2.0%20SOURCE.iso?ftpRequestID=9371755337&amp;amp;server=freescaleesd.flexnetoperations.com&amp;amp;dtm=DTM20220329105301NDQ3NzQ2OTIw&amp;amp;authparam=1648576381_2bc17e3d410a4ef4b57b504dfc1c41d9&amp;amp;ext=.iso" target="_blank"&gt;QorIQ Linux SDK v2.0 SOURCE.iso&lt;/A&gt;&amp;nbsp;and&amp;nbsp;&lt;A class="download-link" href="https://freescaleesd.flexnetoperations.com/337170/307/10295307/QorIQ%20Linux%20SDK%20v2.0%20PPCE6500%20Yocto%20Cache.iso?ftpRequestID=9371755247&amp;amp;server=freescaleesd.flexnetoperations.com&amp;amp;dtm=DTM20220329105300ODEyNzMyOTc0&amp;amp;authparam=1648576380_c08f9e20a3f2e9e58dc28202a111e081&amp;amp;ext=.iso" target="_blank"&gt;QorIQ Linux SDK v2.0 PPCE6500 Yocto Cache.iso,&amp;nbsp;&lt;/A&gt;then build your image.&lt;/P&gt;
&lt;P&gt;You could download the image ISO&amp;nbsp;&lt;A class="download-link" href="https://freescaleesd.flexnetoperations.com/337170/487/10318487/QorIQ%20Linux%20SDK%20v2.0%20PPCE6500%20IMAGE.iso?ftpRequestID=9371755327&amp;amp;server=freescaleesd.flexnetoperations.com&amp;amp;dtm=DTM20220329105301MTk0MDA1NTQy&amp;amp;authparam=1648576381_edc9b0ebe741ca1e6f928a62af317a08&amp;amp;ext=.iso" target="_blank"&gt;QorIQ Linux SDK v2.0 PPCE6500 IMAGE.iso&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;and use the images inside to do verification.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Mar 2022 09:57:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Git-folder-for-t2080rdb/m-p/1435464#M4415</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-03-29T09:57:56Z</dc:date>
    </item>
    <item>
      <title>Re: Git folder for t2080rdb</title>
      <link>https://community.nxp.com/t5/T-Series/Git-folder-for-t2080rdb/m-p/1435499#M4416</link>
      <description>&lt;P&gt;I have used the same ISOs and SDK and generated uboot.bin file for t2080rdb. The file it generates is used to be dumped into alternate&lt;BR /&gt;uboot area of NOR flash. And when i boot t2080rdb from alternate area of the NOR flash, it does not detect the c29 co-processor present on the rdb board.&lt;BR /&gt;So what is the difference between the BIN&lt;BR /&gt;generated using this SDK and the "u-boot-nor-2016.01+fslgit-r0.bin" -predefined image for t2080rdb (which detects the c29 co-processor)?&lt;/P&gt;</description>
      <pubDate>Tue, 29 Mar 2022 11:08:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Git-folder-for-t2080rdb/m-p/1435499#M4416</guid>
      <dc:creator>monalihaware</dc:creator>
      <dc:date>2022-03-29T11:08:29Z</dc:date>
    </item>
    <item>
      <title>Re: Git folder for t2080rdb</title>
      <link>https://community.nxp.com/t5/T-Series/Git-folder-for-t2080rdb/m-p/1445002#M4427</link>
      <description>&lt;P&gt;Please rebuild u-boot with the following command.&lt;/P&gt;
&lt;P&gt;$ bitbake u-boot -c cleansstate&lt;/P&gt;
&lt;P&gt;$ bitbake u-boot&lt;/P&gt;</description>
      <pubDate>Mon, 18 Apr 2022 07:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Git-folder-for-t2080rdb/m-p/1445002#M4427</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-04-18T07:53:46Z</dc:date>
    </item>
  </channel>
</rss>