<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to use T1024RDB on multiple devices on same network in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/How-to-use-T1024RDB-on-multiple-devices-on-same-network/m-p/1403633#M4363</link>
    <description>&lt;P&gt;You could use ssh to access T1024RDB on&amp;nbsp;&lt;SPAN&gt;Computer B.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;$ ssh -l root &amp;lt;ip_address&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 24 Jan 2022 02:58:47 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-01-24T02:58:47Z</dc:date>
    <item>
      <title>How to use T1024RDB on multiple devices on same network</title>
      <link>https://community.nxp.com/t5/T-Series/How-to-use-T1024RDB-on-multiple-devices-on-same-network/m-p/1401388#M4362</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I have two PCs on the same network. For example Computer A and Computer B. They are both connected to network with Ethernet cable.&lt;/P&gt;&lt;P&gt;I also have, one T1024RDB. I usually use with both of the PCs. But I really tired of unplug and plug all setup so I want to use T1024RDB on a software like Tera Term or an equivalent software.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The setup on my mind is like the following,&lt;/P&gt;&lt;P&gt;2 Ethernet cables coming through network and connected to T1024RDB,&lt;/P&gt;&lt;P&gt;A static IP is given to T1024RDB,&lt;/P&gt;&lt;P&gt;UART connected to Computer A.&lt;/P&gt;&lt;P&gt;And I want to connect from Computer B to T1024RDB on Tera Term.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My questions are,&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is this setup technically possible?&lt;UL&gt;&lt;LI&gt;If it's possible, should I use a software on Computer B like virtual serial port or Wireless RS232 module.&lt;/LI&gt;&lt;LI&gt;What is the best solution in this case?&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;Is there any example or tutorial to follow?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR /&gt;I am kind of newbie for all of these stuff so any information that you will give precious for me.&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jan 2022 09:38:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/How-to-use-T1024RDB-on-multiple-devices-on-same-network/m-p/1401388#M4362</guid>
      <dc:creator>alhnkyhn</dc:creator>
      <dc:date>2022-01-19T09:38:58Z</dc:date>
    </item>
    <item>
      <title>Re: How to use T1024RDB on multiple devices on same network</title>
      <link>https://community.nxp.com/t5/T-Series/How-to-use-T1024RDB-on-multiple-devices-on-same-network/m-p/1403633#M4363</link>
      <description>&lt;P&gt;You could use ssh to access T1024RDB on&amp;nbsp;&lt;SPAN&gt;Computer B.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;$ ssh -l root &amp;lt;ip_address&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Jan 2022 02:58:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/How-to-use-T1024RDB-on-multiple-devices-on-same-network/m-p/1403633#M4363</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-01-24T02:58:47Z</dc:date>
    </item>
  </channel>
</rss>