<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: T4241, PCIe enumeration issue in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T4241-PCIe-enumeration-issue/m-p/1395033#M4334</link>
    <description>&lt;P&gt;Please provide the processor connection schematics as searchable PDF.&lt;/P&gt;</description>
    <pubDate>Wed, 05 Jan 2022 18:44:40 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2022-01-05T18:44:40Z</dc:date>
    <item>
      <title>T4241, PCIe enumeration issue</title>
      <link>https://community.nxp.com/t5/T-Series/T4241-PCIe-enumeration-issue/m-p/1394916#M4333</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are using T4241, with the following RCW configurations, also added uboot prints and lspci utility prints.&amp;nbsp; In RCW PCIe1 is selected to be 5GT/s with 8 lane. But link width is downgrading to x1 lane.&lt;/P&gt;&lt;P&gt;Thanks for any information!&lt;/P&gt;&lt;P&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 0c080012 0e12120e 00000000 08000000&lt;BR /&gt;00000010: 04360848 30547a00 ec03f000 f9000000&lt;BR /&gt;00000020: 00080000 00000000 00000000 0003e000&lt;BR /&gt;00000030: 00000000 50000000 00000000 00000038&lt;/P&gt;&lt;P&gt;Here are the uboot prints:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;U-Boot 2016.012.0+ga9b437f (Mar 28 2019 - 16:23:11 +0530)

CPU0: T4241, Version: 2.0, (0x82400020)
Core: e6500, Version: 2.0, (0x80400120)
Clock Configuration:
CPU0:1800 MHz, CPU1:1800 MHz, CPU2:1800 MHz, CPU3:1800 MHz,
CPU4:1800 MHz, CPU5:1800 MHz, CPU6:1800 MHz, CPU7:1800 MHz,
CPU8:1800 MHz, CPU9:1800 MHz, CPU10:1800 MHz, CPU11:1800 MHz,
CCB:600 MHz,
DDR:800 MHz (1600 MT/s data rate) (Asynchronous), IFC:150 MHz
FMAN1: 700 MHz
FMAN2: 600 MHz
QMAN: 300 MHz
PME: 466.667 MHz
L1: D-cache 32 KiB enabled
I-cache 32 KiB enabled
Reset Configuration Word (RCW):
00000000: 0c080012 0e12120e 00000000 08000000
00000010: 04360848 30547a00 ec03f000 f9000000
00000020: 00080000 00000000 00000000 0003e000
00000030: 00000000 50000000 00000000 00000038
I2C: ready
Board: T4241, SERDES Reference Clocks:
SERDES1=125MHz SERDES2=125MHz
SERDES3=100MHz SERDES4=100MHz
SPI: ready
DRAM: Initializing DDR
10 GiB left unmapped
12 GiB (DDR3, 64-bit, CL=11, ECC on)

Value From Fuse Register = 10250

Corresponding value to be Written = 42

VID Write Successfull
Flash: 256 MiB
L2: 2 MiB enabled
enable l2 for cluster 1 fec60000
enable l2 for cluster 2 feca0000
Corenet Platform Cache: 1.5 MiB enabled
A007186 Serdes PLL locked
A007186 Serdes PLL locked
NAND: 0 MiB
MMC: FSL_SDHC: 0
PCIe1: Root Complex, x1 gen2, regs @ 0xfe240000
01:00.0 - 10ee:7028 - Memory controller
PCIe1: Bus 00 - 01
PCIe3: Root Complex, no link, regs @ 0xfe260000
PCIe3: Bus 02 - 02
PCIe4: Root Complex, no link, regs @ 0xfe270000
PCIe4: Bus 03 - 03
In: serial
Out: serial
Err: serial
Net:
Fman1: Uploading microcode version 108.4.5
Could not get PHY for FM_TGEC_MDIO: addr 16
Failed to connect

Fman2: Uploading microcode version 108.4.5
Could not get PHY for FSL_MDIO0: addr 1
Failed to connect
Could not get PHY for FSL_MDIO0: addr 2
Failed to connect
PHY reset timed out
FM1@TGEC1, FM2@DTSEC1, FM2@DTSEC2, FM2@DTSEC5 [PRIME], FM2@DTSEC6, FM2@DTSEC9, FM2@DTSEC10

POST Start:

POST Complete

U-boot Software Version : 1.0

tap env addr 0
Updating Boot Status Successful
Hit any key to stop autoboot: 0
Q4241_uboot&amp;gt;
&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;lspci output prints&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@t4240rdb:~# ./lspci -vvv -d 10ee:7028
0000:01:00.0 Class 0580: Device 10ee:7028
        Subsystem: Device 10ee:0007
        Control: I/O- Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr- Stepping- SERR- FastB2B- DisINTx-
        Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast &amp;gt;TAbort- &amp;lt;TAbort- &amp;lt;MAbort- &amp;gt;SERR- &amp;lt;PERR- INTx-
        Latency: 0, Cache Line Size: 32 bytes
        Interrupt: pin A routed to IRQ 40
        IOMMU group: 60
        Region 0: Memory at c00000000 (32-bit, non-prefetchable) [size=2K]
        Capabilities: [40] Power Management version 3
                Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0+,D1+,D2+,D3hot+,D3cold-)
                Status: D0 NoSoftRst+ PME-Enable- DSel=0 DScale=0 PME-
        Capabilities: [48] MSI: Enable- Count=1/1 Maskable- 64bit+
                Address: 0000000000000000  Data: 0000
        Capabilities: [60] Express (v2) Endpoint, MSI 00
                DevCap: MaxPayload 256 bytes, PhantFunc 0, Latency L0s &amp;lt;64ns, L1 unlimited
                        ExtTag- AttnBtn- AttnInd- PwrInd- RBE+ FLReset- SlotPowerLimit 0.000W
                DevCtl: CorrErr- NonFatalErr- FatalErr- UnsupReq-
                        RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
                        MaxPayload 128 bytes, MaxReadReq 512 bytes
                DevSta: CorrErr- NonFatalErr- FatalErr- UnsupReq- AuxPwr- TransPend-
                LnkCap: Port #0, Speed 5GT/s, Width x8, ASPM L0s, Exit Latency L0s unlimited
                        ClockPM- Surprise- LLActRep- BwNot- ASPMOptComp-
                LnkCtl: ASPM Disabled; RCB 64 bytes, Disabled- CommClk-
                        ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
                LnkSta: Speed 5GT/s (ok), Width x1 (downgraded)
                        TrErr- Train- SlotClk- DLActive- BWMgmt- ABWMgmt-
                DevCap2: Completion Timeout: Range B, TimeoutDis- NROPrPrP- LTR-
                         10BitTagComp- 10BitTagReq- OBFF Not Supported, ExtFmt- EETLPPrefix-
                         EmergencyPowerReduction Not Supported, EmergencyPowerReductionInit-
                         FRS- TPHComp- ExtTPHComp-
                         AtomicOpsCap: 32bit- 64bit- 128bitCAS-
                DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis- LTR- OBFF Disabled,
                         AtomicOpsCtl: ReqEn-
                LnkCtl2: Target Link Speed: 5GT/s, EnterCompliance- SpeedDis-
                         Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
                         Compliance De-emphasis: -6dB
                LnkSta2: Current De-emphasis Level: -6dB, EqualizationComplete- EqualizationPhase1-
                         EqualizationPhase2- EqualizationPhase3- LinkEqualizationRequest-
                         Retimer- 2Retimers- CrosslinkRes: unsupported
        Capabilities: [9c] MSI-X: Enable- Count=1 Masked-
                Vector table: BAR=0 offset=00000000
                PBA: BAR=0 offset=00000000
        Capabilities: [100 v1] Device Serial Number 00-00-00-01-01-00-0a-35&lt;/LI-CODE&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Balaji.G&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jan 2022 15:52:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4241-PCIe-enumeration-issue/m-p/1394916#M4333</guid>
      <dc:creator>immbalu</dc:creator>
      <dc:date>2022-01-05T15:52:12Z</dc:date>
    </item>
    <item>
      <title>Re: T4241, PCIe enumeration issue</title>
      <link>https://community.nxp.com/t5/T-Series/T4241-PCIe-enumeration-issue/m-p/1395033#M4334</link>
      <description>&lt;P&gt;Please provide the processor connection schematics as searchable PDF.&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jan 2022 18:44:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4241-PCIe-enumeration-issue/m-p/1395033#M4334</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-05T18:44:40Z</dc:date>
    </item>
    <item>
      <title>Re: T4241, PCIe enumeration issue</title>
      <link>https://community.nxp.com/t5/T-Series/T4241-PCIe-enumeration-issue/m-p/1395612#M4336</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/56916"&gt;@ufedor&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for the reply.,&lt;/P&gt;&lt;P&gt;i'm sharing the&amp;nbsp;&lt;SPAN&gt;schematic&amp;nbsp;&lt;/SPAN&gt;connections between processor and fpga. please find the attached pdf.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Balaji.G&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jan 2022 12:35:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4241-PCIe-enumeration-issue/m-p/1395612#M4336</guid>
      <dc:creator>immbalu</dc:creator>
      <dc:date>2022-01-06T12:35:07Z</dc:date>
    </item>
    <item>
      <title>Re: T4241, PCIe enumeration issue</title>
      <link>https://community.nxp.com/t5/T-Series/T4241-PCIe-enumeration-issue/m-p/1396107#M4338</link>
      <description>&lt;P&gt;In the provided schematics T4241 PCIe lanes are connected to the FPGA in arbitrary order.&lt;/P&gt;
&lt;P&gt;Please consider that order of lanes is very important.&lt;/P&gt;
&lt;P&gt;For the x8 configuration it could be either (T4241 &amp;lt;-&amp;gt; FPGA):&lt;/P&gt;
&lt;P&gt;0 &amp;lt;-&amp;gt; 0&lt;/P&gt;
&lt;P&gt;1 &amp;lt;-&amp;gt; 1&lt;/P&gt;
&lt;P&gt;..&lt;/P&gt;
&lt;P&gt;6 &amp;lt;-&amp;gt; 6&lt;/P&gt;
&lt;P&gt;7 &amp;lt;-&amp;gt; 7&lt;/P&gt;
&lt;P&gt;or&lt;/P&gt;
&lt;P&gt;0 &amp;lt;-&amp;gt; 7&lt;/P&gt;
&lt;P&gt;1 &amp;lt;-&amp;gt; 6&lt;/P&gt;
&lt;P&gt;...&lt;/P&gt;
&lt;P&gt;6 &amp;lt;-&amp;gt; 1&lt;/P&gt;
&lt;P&gt;7 &amp;lt;-&amp;gt; 0&lt;/P&gt;
&lt;P&gt;As result only T4241 lane 7 connected to the FPGA lane 0 works. &lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jan 2022 10:24:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4241-PCIe-enumeration-issue/m-p/1396107#M4338</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-07T10:24:36Z</dc:date>
    </item>
    <item>
      <title>Re: T4241, PCIe enumeration issue</title>
      <link>https://community.nxp.com/t5/T-Series/T4241-PCIe-enumeration-issue/m-p/1396586#M4339</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/56916"&gt;@ufedor&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;In the schismatics,&lt;/P&gt;&lt;P&gt;lane 0 is connected as,&lt;/P&gt;&lt;P&gt;SD3_TX0 is connected to&amp;nbsp;MGTXRXP3_116 and&amp;nbsp;SD3_TX0_B is connected to&amp;nbsp;MGTXRXN3_116,&lt;/P&gt;&lt;P&gt;MGTXTXN3_116 is connected to&amp;nbsp;SD3_RX0_B and MGTXTXP3_116 is connected to&amp;nbsp;SD3_RX0&amp;nbsp;&lt;/P&gt;&lt;P&gt;lane 1 is connected as,&lt;/P&gt;&lt;P&gt;SD3_TX1 is connected to&amp;nbsp;MGTXRXP2_116 and&amp;nbsp;SD3_TX1_B is connected to&amp;nbsp;MGTXRXN2_116,&lt;/P&gt;&lt;P&gt;MGTXTXN2_116 is connected to&amp;nbsp;SD3_RX1_B and MGTXTXP2_116 is connected to&amp;nbsp;SD3_RX1&amp;nbsp;&lt;/P&gt;&lt;P&gt;and same as other lanes which is in lane reversal order. This can be confirmed by referring to&amp;nbsp;&lt;A href="https://www.xilinx.com/support/documentation/boards_and_kits/kc705_Schematic_xtp132_rev1_1.pdf" target="_blank"&gt;https://www.xilinx.com/support/documentation/boards_and_kits/kc705_Schematic_xtp132_rev1_1.pdf&lt;/A&gt;&amp;nbsp;schismatics page no 9.&lt;/P&gt;&lt;P&gt;Also, some times pcie is detecting as x2 gen 1 and sometimes its detecting as x1 gen 2.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Balaji.G.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jan 2022 07:00:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4241-PCIe-enumeration-issue/m-p/1396586#M4339</guid>
      <dc:creator>immbalu</dc:creator>
      <dc:date>2022-01-10T07:00:33Z</dc:date>
    </item>
    <item>
      <title>Re: T4241, PCIe enumeration issue</title>
      <link>https://community.nxp.com/t5/T-Series/T4241-PCIe-enumeration-issue/m-p/1396653#M4340</link>
      <description>&lt;P&gt;How the PCIe lanes are implemented and what are the lanes lengths?&lt;/P&gt;
&lt;P&gt;Did you simulate the PCIe lanes in HyperLynx?&lt;/P&gt;
&lt;P&gt;Have you reported the issue to Xilinx and what is their response?&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jan 2022 08:52:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4241-PCIe-enumeration-issue/m-p/1396653#M4340</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-10T08:52:05Z</dc:date>
    </item>
    <item>
      <title>Re: T4241, PCIe enumeration issue</title>
      <link>https://community.nxp.com/t5/T-Series/T4241-PCIe-enumeration-issue/m-p/1416426#M4385</link>
      <description>&lt;P&gt;Found the issue with SI analysis&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Balaji.G&lt;/P&gt;</description>
      <pubDate>Mon, 21 Feb 2022 04:49:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4241-PCIe-enumeration-issue/m-p/1416426#M4385</guid>
      <dc:creator>immbalu</dc:creator>
      <dc:date>2022-02-21T04:49:13Z</dc:date>
    </item>
  </channel>
</rss>