<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックRe: T4240RDB</title>
    <link>https://community.nxp.com/t5/T-Series/T4240RDB/m-p/460063#M425</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Socket for the SATA Data Cable is present on-board.&lt;/P&gt;&lt;P&gt;SATA Power cable is provided by the RDB's PSU.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Mar 2016 16:22:47 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2016-03-08T16:22:47Z</dc:date>
    <item>
      <title>T4240RDB</title>
      <link>https://community.nxp.com/t5/T-Series/T4240RDB/m-p/460062#M424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to connect a SATA hard disk to the T4240RDB board? What kind of cabling is needed?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 13:40:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240RDB/m-p/460062#M424</guid>
      <dc:creator>bogdantanasa</dc:creator>
      <dc:date>2016-03-08T13:40:22Z</dc:date>
    </item>
    <item>
      <title>Re: T4240RDB</title>
      <link>https://community.nxp.com/t5/T-Series/T4240RDB/m-p/460063#M425</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Socket for the SATA Data Cable is present on-board.&lt;/P&gt;&lt;P&gt;SATA Power cable is provided by the RDB's PSU.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 16:22:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240RDB/m-p/460063#M425</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-03-08T16:22:47Z</dc:date>
    </item>
    <item>
      <title>Re: T4240RDB</title>
      <link>https://community.nxp.com/t5/T-Series/T4240RDB/m-p/460064#M426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;Can you also tell me if the board is delivered with DDR3 memory or one has to buy it separately? If yes, which kind of memory is delivered?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 16:37:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240RDB/m-p/460064#M426</guid>
      <dc:creator>bogdantanasa</dc:creator>
      <dc:date>2016-03-08T16:37:30Z</dc:date>
    </item>
    <item>
      <title>Re: T4240RDB</title>
      <link>https://community.nxp.com/t5/T-Series/T4240RDB/m-p/460065#M427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The RDB is equipped with 3 x 4GB UDIMMs.&lt;/P&gt;&lt;P&gt;The RDB documentation is available at:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-power-architecture-processors/qoriq-t4240-reference-design-board:T4240RDB?fpsp=1&amp;amp;tab=Documentation_Tab" title="http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-power-architecture-processors/qoriq-t4240-reference-design-board:T4240RDB?fpsp=1&amp;amp;tab=Documentation_Tab"&gt;QorIQ T4240 Reference Design Board|NXP&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 17:33:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240RDB/m-p/460065#M427</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-03-08T17:33:51Z</dc:date>
    </item>
    <item>
      <title>Re: T4240RDB</title>
      <link>https://community.nxp.com/t5/T-Series/T4240RDB/m-p/460066#M428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am wondering if this is really true (i.e. 12GB of memory).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the T4240RDBQS.pdf it says that 3 DIMMS slots are supported (2 GB per DIMM) while in T4240RDBFS.pdf it says:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt; "Three unbuffered DDR3 240-pin uDIMM modules with ECC (72-bit bus), 6 GB memory, 1866 MT/s data rate"&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;which would suggest that the memory is pre-installed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The confusing arises from the fact that T4240RDBQS.pdf does not give the impression that the memory is pre-installed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 14:13:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240RDB/m-p/460066#M428</guid>
      <dc:creator>bogdantanasa</dc:creator>
      <dc:date>2016-03-09T14:13:19Z</dc:date>
    </item>
    <item>
      <title>Re: T4240RDB</title>
      <link>https://community.nxp.com/t5/T-Series/T4240RDB/m-p/460067#M429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are right.&lt;/P&gt;&lt;P&gt;I'm sorry for the issue with the memory size.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the real board booting log shows:&lt;/P&gt;&lt;P&gt;DRAM:&amp;nbsp; Initializing....using SPD&lt;/P&gt;&lt;P&gt;Detected UDIMM 9JSF25672AZ-2G1K1&lt;/P&gt;&lt;P&gt;Detected UDIMM 9JSF25672AZ-2G1K1&lt;/P&gt;&lt;P&gt;Detected UDIMM 9JSF25672AZ-2G1K1&lt;/P&gt;&lt;P&gt;4 GiB left unmapped&lt;/P&gt;&lt;P&gt;6 GiB (DDR3, 64-bit, CL=13, ECC on)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DDR Controller Interleaving Mode: 3-way 4KB&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The memory surely is pre-installed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issue was caused by the RDB board documentation issue (QorIQ T4240 Reference Design Board Quick Start, Rev. 2) where the log is:&lt;/P&gt;&lt;P&gt;DRAM: Initializing....using SPD&lt;/P&gt;&lt;P&gt;Detected UDIMM 18JSF51272AZ-1G9K1&lt;/P&gt;&lt;P&gt;Detected UDIMM 18JSF51272AZ-1G9K1&lt;/P&gt;&lt;P&gt;Detected UDIMM 18JSF51272AZ-1G9K1&lt;/P&gt;&lt;P&gt;10 GiB left unmapped&lt;/P&gt;&lt;P&gt;12 GiB (DDR3, 64-bit, CL=13, ECC on)&lt;/P&gt;&lt;P&gt;DDR Controller Interleaving Mode: 3-way 4KB&lt;/P&gt;&lt;P&gt;DDR Chip-Select Interleaving Mode: CS0+CS1&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 14:20:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T4240RDB/m-p/460067#M429</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-03-09T14:20:42Z</dc:date>
    </item>
  </channel>
</rss>