<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: flash error on T1042 based customized board using code warrior tap in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/flash-error-on-T1042-based-customized-board-using-code-warrior/m-p/1345965#M4227</link>
    <description>&lt;P&gt;The problem is solved by forced RCW mode in code warrior using the customized RCW file in the target option.&lt;/P&gt;</description>
    <pubDate>Fri, 24 Sep 2021 16:03:46 GMT</pubDate>
    <dc:creator>Abubakar</dc:creator>
    <dc:date>2021-09-24T16:03:46Z</dc:date>
    <item>
      <title>flash error on T1042 based customized board using code warrior tap</title>
      <link>https://community.nxp.com/t5/T-Series/flash-error-on-T1042-based-customized-board-using-code-warrior/m-p/1340572#M4197</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to bring up T1042 based customized board with nothing flashed on the nor flash. As a first step, I am flashing RCW on it using code warrior tap by following way:&lt;/P&gt;&lt;P&gt;I am running the board on the hardcoded RCW setting using dip switches and flashing the customized RCW using code warrior bare board project but it fails to initialize the target with following error on console:&lt;/P&gt;&lt;P&gt;fl::target -lc "flashing_kit-core00_RAM_T1042_Download"&lt;BR /&gt;fl::target -b 0x0 0x5130&lt;BR /&gt;fl::target -v off -l off&lt;BR /&gt;cmdwin::fl::device -d "JS28F00AM29EWL" -o "64Mx16x1" -a 0xe8000000 0xefffffff&lt;BR /&gt;cmdwin::fl::image -f "C:\\Users\\CW\\Desktop\\code warrior projects\\flashing kit\\rcw.bin" -t "Auto Detect" -re on -r 0xe8000000 0xefffffff -oe on -o 0xeff40000&lt;BR /&gt;cmdwin::fl::erase image&lt;BR /&gt;Beginning Operation ...&lt;BR /&gt;-------------------------&lt;BR /&gt;Auto-detection is successful.&lt;BR /&gt;File is of type Binary/Raw Format.&lt;BR /&gt;&lt;BR /&gt;Performing target initialization ...&lt;BR /&gt;failed on register write: L2MMU_CAM1&lt;BR /&gt;failed on register write: L2MMU_CAM2&lt;BR /&gt;failed on register write: L2MMU_CAM3&lt;BR /&gt;failed on register write: L2MMU_CAM4&lt;BR /&gt;failed on register write: L2MMU_CAM5&lt;BR /&gt;Error writing memory&lt;BR /&gt;[CCS last error: Scan timeout ](CCSProtocolPlugin)&lt;BR /&gt;Error: invalid input value&lt;BR /&gt;Error: Couldn't stop the target. Can't stop the target.&lt;BR /&gt;Error: Couldn't stop the target.Can't stop the target.&lt;/P&gt;&lt;P&gt;The related error images are attached&amp;nbsp; as well.&lt;/P&gt;&lt;P&gt;In this case, no rcw is present on board as i am bringing up a new board. Can you please tell me why am I getting these errors?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 11:51:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/flash-error-on-T1042-based-customized-board-using-code-warrior/m-p/1340572#M4197</guid>
      <dc:creator>Abubakar</dc:creator>
      <dc:date>2021-09-15T11:51:44Z</dc:date>
    </item>
    <item>
      <title>Re: flash error on T1042 based customized board using code warrior tap</title>
      <link>https://community.nxp.com/t5/T-Series/flash-error-on-T1042-based-customized-board-using-code-warrior/m-p/1340651#M4198</link>
      <description>&lt;P&gt;Please provide additional information:&lt;/P&gt;
&lt;P&gt;1) Confirm that TRST_B is pulsed low (asserted) during power-on reset sequence;&lt;/P&gt;
&lt;P&gt;2) A digital scope trace(s) showing behavior of all reset signals when hard-coded RCW option is selected;&lt;/P&gt;
&lt;P&gt;3) The processor connection schematics as searchable PDF.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 13:34:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/flash-error-on-T1042-based-customized-board-using-code-warrior/m-p/1340651#M4198</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-09-15T13:34:25Z</dc:date>
    </item>
    <item>
      <title>Re: flash error on T1042 based customized board using code warrior tap</title>
      <link>https://community.nxp.com/t5/T-Series/flash-error-on-T1042-based-customized-board-using-code-warrior/m-p/1341132#M4200</link>
      <description>&lt;P&gt;1) Yes, TRST_B is managed and asserted on power on reset sequence.&lt;/P&gt;&lt;P&gt;2) I had verified some of the signals but am not sure which particular reset signals you are talking about. Can you elaborate?&lt;/P&gt;&lt;P&gt;3) Sorry I cannot share them due to company policy but they are the same as in the t1042d4rdb reference kit.&lt;/P&gt;&lt;P&gt;Recently, I encountered another error while flashing in which the erase command was succeeded but error occurred on flashing. The console output is below:&lt;/P&gt;&lt;P&gt;fl::target -lc "jtag_flash-core00_RAM_T1042_Download"&lt;BR /&gt;fl::target -b 0x0 0x5130&lt;BR /&gt;fl::target -v off -l off&lt;BR /&gt;cmdwin::fl::device -d "JS28F00AM29EWL" -o "128Mx8x1" -a 0xe8000000 0xefffffff&lt;BR /&gt;cmdwin::fl::image -f "C:\\Users\\CW\\Desktop\\mydtb_spi_disable.dtb" -t "Auto Detect" -re on -r 0xe8000000 0xefffffff -oe on -o 0xe8000000&lt;BR /&gt;cmdwin::fl::erase image&lt;BR /&gt;Beginning Operation ...&lt;BR /&gt;-------------------------&lt;BR /&gt;Auto-detection is successful.&lt;BR /&gt;File is of type Binary/Raw Format.&lt;BR /&gt;&lt;BR /&gt;Performing target initialization ...&lt;BR /&gt;Downloading Flash Device Driver ...&lt;BR /&gt;Reading flash ID ...&lt;BR /&gt;Erasing Sector 0xE8000000 to 0xE801FFFF&lt;BR /&gt;Erasing ...&lt;BR /&gt;Erase Command Succeeded&lt;BR /&gt;cmdwin::fl::write verify&lt;BR /&gt;-------------------------&lt;BR /&gt;Using restricted address range 0xE8000000 to 0xEFFFFFFF&lt;BR /&gt;Programming file C:\Users\CW\Desktop\mydtb_spi_disable.dtb&lt;BR /&gt;Auto-detection is successful.&lt;BR /&gt;File is of type Binary/Raw Format.&lt;BR /&gt;&lt;BR /&gt;Downloading Flash Device Driver ...&lt;BR /&gt;Reading flash ID ...&lt;BR /&gt;Auto-detection is successful.&lt;BR /&gt;File is of type Binary/Raw Format.&lt;BR /&gt;&lt;BR /&gt;Downloading 0x00001BA0 bytes to be programmed at 0xE8000000&lt;BR /&gt;Executing program with verify ....&lt;BR /&gt;Error: Program with Verify failed. Flash driver reports the following error(s): Chip reported error during program. Pleasecheck that the sector you are programming is erased.&lt;/P&gt;&lt;P&gt;Error: Program with Verify failed. Flash driver reports the following error(s): Chip reported error during program. Please check&lt;BR /&gt;that the sector you are programming is erased.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Sep 2021 04:40:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/flash-error-on-T1042-based-customized-board-using-code-warrior/m-p/1341132#M4200</guid>
      <dc:creator>Abubakar</dc:creator>
      <dc:date>2021-09-16T04:40:27Z</dc:date>
    </item>
    <item>
      <title>Re: flash error on T1042 based customized board using code warrior tap</title>
      <link>https://community.nxp.com/t5/T-Series/flash-error-on-T1042-based-customized-board-using-code-warrior/m-p/1342506#M4204</link>
      <description>&lt;P&gt;2) Please refer to the QorIQ T1040 Reference Manual, Figure 4-1. Power-on reset sequence.&lt;/P&gt;</description>
      <pubDate>Sat, 18 Sep 2021 11:17:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/flash-error-on-T1042-based-customized-board-using-code-warrior/m-p/1342506#M4204</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-09-18T11:17:38Z</dc:date>
    </item>
    <item>
      <title>Re: flash error on T1042 based customized board using code warrior tap</title>
      <link>https://community.nxp.com/t5/T-Series/flash-error-on-T1042-based-customized-board-using-code-warrior/m-p/1345965#M4227</link>
      <description>&lt;P&gt;The problem is solved by forced RCW mode in code warrior using the customized RCW file in the target option.&lt;/P&gt;</description>
      <pubDate>Fri, 24 Sep 2021 16:03:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/flash-error-on-T1042-based-customized-board-using-code-warrior/m-p/1345965#M4227</guid>
      <dc:creator>Abubakar</dc:creator>
      <dc:date>2021-09-24T16:03:46Z</dc:date>
    </item>
  </channel>
</rss>