<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックRe: Instruction Address Translation for T2080</title>
    <link>https://community.nxp.com/t5/T-Series/Instruction-Address-Translation-for-T2080/m-p/458963#M421</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have the same problem. Is it a CodeWarrior problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Aug 2019 10:34:48 GMT</pubDate>
    <dc:creator>manoloruiz</dc:creator>
    <dc:date>2019-08-14T10:34:48Z</dc:date>
    <item>
      <title>Instruction Address Translation for T2080</title>
      <link>https://community.nxp.com/t5/T-Series/Instruction-Address-Translation-for-T2080/m-p/458961#M419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I am trying to make Windriver Vxworks 5.5.2 running on Core#3 of T2080 Soc (AMP mode). My platform is T2080RDB board from FreeScale.&lt;/P&gt;&lt;P&gt;Now I can boot the vxworks 5.5.2 on core#3 from U-boot with this command:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# tftpboot 0x20100000 vxWorks.bin &amp;amp;&amp;amp; cpu 3 release 0x201002e8 6 1 1&lt;/P&gt;&lt;P&gt;I reserve the RAM from 0x20000000 - 0x3FFFFFFF (512MB) for Vxworks running on Core#3, so I setup one TLB1 entry 1 to map 0x0 -&amp;gt; 0x20000000, 512MB.&lt;/P&gt;&lt;P&gt;The Vxworks 5.5.2 is built with Text segment is set to 0x100000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issue is that the Instruction Address Translation for T2080 does not work but the Data Address Translation for T2080 works. &lt;/P&gt;&lt;P&gt;When execute code from any address in 0x1xxxxx (For example: TLB mis handler ... ), the Core#3 always get 0xDEADBEEF (The reset value of RAM) for instruction.&lt;/P&gt;&lt;P&gt;I use Codewarrior to debug the system and I found that the Data Address Translation works, I can read the value at that memory correctly (not 0xDEADBEEF).&lt;/P&gt;&lt;P&gt;It seems that E6500 Core#3 does not care about TLB when making Instruction Address Translation. &lt;/P&gt;&lt;P&gt;Is this an errata of Chip ? How could I overcome this ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,Quan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2015 08:58:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Instruction-Address-Translation-for-T2080/m-p/458961#M419</guid>
      <dc:creator>quancao</dc:creator>
      <dc:date>2015-08-24T08:58:02Z</dc:date>
    </item>
    <item>
      <title>Re: Instruction Address Translation for T2080</title>
      <link>https://community.nxp.com/t5/T-Series/Instruction-Address-Translation-for-T2080/m-p/458962#M420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ah, I found out that issue is from CodeWarrior, not T2080 core. I can run vxworks 5.5.2 on core#3 to application code. That is the issue of CodeWarrior which it could not read the instruction correctly. It seems that is the issue of caching in CodeWarrior.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2015 10:42:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Instruction-Address-Translation-for-T2080/m-p/458962#M420</guid>
      <dc:creator>quancao</dc:creator>
      <dc:date>2015-08-24T10:42:05Z</dc:date>
    </item>
    <item>
      <title>Re: Instruction Address Translation for T2080</title>
      <link>https://community.nxp.com/t5/T-Series/Instruction-Address-Translation-for-T2080/m-p/458963#M421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have the same problem. Is it a CodeWarrior problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Aug 2019 10:34:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Instruction-Address-Translation-for-T2080/m-p/458963#M421</guid>
      <dc:creator>manoloruiz</dc:creator>
      <dc:date>2019-08-14T10:34:48Z</dc:date>
    </item>
  </channel>
</rss>