<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 Re: how to integrate python modules in RFS file for python 2.7.18</title>
    <link>https://community.nxp.com/t5/T-Series/how-to-integrate-python-modules-in-RFS-file-for-python-2-7-18/m-p/1331441#M4181</link>
    <description>&lt;P&gt;Find the following in the Section 3.3.13 in SDK 2.0-1703 documrntation:&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Q: &lt;/STRONG&gt;How do I add a pre-built binary into the rootfs?&lt;/P&gt;</description>
    <pubDate>Mon, 30 Aug 2021 04:55:14 GMT</pubDate>
    <dc:creator>Pavel</dc:creator>
    <dc:date>2021-08-30T04:55:14Z</dc:date>
    <item>
      <title>how to integrate python modules in RFS file for python 2.7.18</title>
      <link>https://community.nxp.com/t5/T-Series/how-to-integrate-python-modules-in-RFS-file-for-python-2-7-18/m-p/1327382#M4175</link>
      <description>&lt;P&gt;I have added python package 2.7.18 by earlier solution provided by you. pyhton2.7.18 does get intergated in file system. But I find no default python mdoules in /usr/lib64/python2.7 directory. Earlier for python 2.7.9, we got these modules automatically.&amp;nbsp;&amp;nbsp; For python2.7.18, i need to move all such modules and files from yocto SDK to corresponding directory in card linux (every time i fuse new RFS to card)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To make such modules part of rfs by default,&amp;nbsp; i tried to copy all such modules and files in merge folder and then run fsl-image-core. But i am getting this error.&amp;nbsp; (i have already added 'python' in IMAGE_INSTALL_append f&lt;FONT face="Arial, Helvetica"&gt;sl-image-core.bb&lt;/FONT&gt; )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Arial, Helvetica"&gt;&lt;FONT size="2"&gt;ERROR: Unable to install packages. Command '/home/ngntemp/brtr/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/sysroots/i686-linux/usr/bin/smart --log-level=warning --data-dir=/home/ngntemp/brtr/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/t1040d4rdb_64b-fsl-linux/fsl-image-core/1.0-r0/rootfs/var/lib/smart install -y quagga@ppc64e5500 lsb@ppc64e5500 net-snmp@ppc64e5500 packagegroup-fsl-mfgtools@all python-core-2.7.18-r1@ppc64e5500 openssh@ppc64e5500 packagegroup-core-ssh-openssh@all packagegroup-core-boot@t1040d4rdb_64b monit@ppc64e5500 tcl@ppc64e5500 udev-extraconf@ppc64e5500 merge-files@all packagegroup-fsl-benchmark-core@all sqlite3@ppc64e5500 run-postinsts@all udev-rules-qoriq@ppc64e5500 packagegroup-fsl-networking-core@all packagegroup-fsl-tools-core@all libpam@ppc64e5500' returned 1:&lt;BR /&gt;Loading cache...&lt;BR /&gt;Updating cache...&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ######################################## [100%]&lt;BR /&gt;&lt;BR /&gt;Computing transaction...error: Can't install merge-files-1.0-r0@all: no package provides libpython2.7.so.1.0&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;ERROR: Function failed: do_rootfs&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/ngntemp/brtr/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/t1040d4rdb_64b-fsl-linux/fsl-image-core/1.0-r0/temp/log.do_rootfs.18342&lt;BR /&gt;ERROR: Task 7 (/home/ngntemp/brtr/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-fsl/images/fsl-image-core.bb, do_rootfs) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 3361 tasks of which 3348 didn't need to be rerun and 1 failed.&lt;BR /&gt;No currently running tasks (3361 of 3362)&lt;BR /&gt;&lt;BR /&gt;Summary: 1 task failed:&lt;BR /&gt;&amp;nbsp; /home/ngntemp/brtr/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-fsl/images/fsl-image-core.bb, do_rootfs&lt;BR /&gt;Summary: There was 1 WARNING message shown.&lt;BR /&gt;Summary: There were 2 ERROR messages shown, returning a non-zero exit code.&lt;BR /&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please suggest a way to integrate pyhton modules by default&amp;nbsp; into rfs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Aug 2021 05:15:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/how-to-integrate-python-modules-in-RFS-file-for-python-2-7-18/m-p/1327382#M4175</guid>
      <dc:creator>sandeepk1980</dc:creator>
      <dc:date>2021-08-23T05:15:12Z</dc:date>
    </item>
    <item>
      <title>Re: how to integrate python modules in RFS file for python 2.7.18</title>
      <link>https://community.nxp.com/t5/T-Series/how-to-integrate-python-modules-in-RFS-file-for-python-2-7-18/m-p/1331441#M4181</link>
      <description>&lt;P&gt;Find the following in the Section 3.3.13 in SDK 2.0-1703 documrntation:&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Q: &lt;/STRONG&gt;How do I add a pre-built binary into the rootfs?&lt;/P&gt;</description>
      <pubDate>Mon, 30 Aug 2021 04:55:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/how-to-integrate-python-modules-in-RFS-file-for-python-2-7-18/m-p/1331441#M4181</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2021-08-30T04:55:14Z</dc:date>
    </item>
  </channel>
</rss>