<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic T2080 Descriptor command format fields in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T2080-Descriptor-command-format-fields/m-p/1314498#M4150</link>
    <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;I am trying to develop Crypto driver for T2080. I have a doubt related to the descriptor command fields .&lt;/P&gt;&lt;P&gt;The macros available in desc.h file of SDK seems to set Command bits following bit positions 31,30,29,28.....2,1,0(MSB-LSB) but for example FIFO LOAD Command Format in the T2080 SEC Reference Manual has the bit positions as 0,1,2.........28,29,30,31(LSB-MSB).&lt;/P&gt;&lt;P&gt;So do we need to use the macros availabe in desc.h as is or do we need to change the macros setting as per T2080SECRM bit ordering?&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Faizanbaig Inamdar&lt;/P&gt;</description>
    <pubDate>Wed, 28 Jul 2021 11:05:01 GMT</pubDate>
    <dc:creator>Faizanbaig</dc:creator>
    <dc:date>2021-07-28T11:05:01Z</dc:date>
    <item>
      <title>T2080 Descriptor command format fields</title>
      <link>https://community.nxp.com/t5/T-Series/T2080-Descriptor-command-format-fields/m-p/1314498#M4150</link>
      <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;I am trying to develop Crypto driver for T2080. I have a doubt related to the descriptor command fields .&lt;/P&gt;&lt;P&gt;The macros available in desc.h file of SDK seems to set Command bits following bit positions 31,30,29,28.....2,1,0(MSB-LSB) but for example FIFO LOAD Command Format in the T2080 SEC Reference Manual has the bit positions as 0,1,2.........28,29,30,31(LSB-MSB).&lt;/P&gt;&lt;P&gt;So do we need to use the macros availabe in desc.h as is or do we need to change the macros setting as per T2080SECRM bit ordering?&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Faizanbaig Inamdar&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jul 2021 11:05:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080-Descriptor-command-format-fields/m-p/1314498#M4150</guid>
      <dc:creator>Faizanbaig</dc:creator>
      <dc:date>2021-07-28T11:05:01Z</dc:date>
    </item>
  </channel>
</rss>