<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-SeriesのトピックRe: Uboot code for t2081</title>
    <link>https://community.nxp.com/t5/T-Series/Uboot-code-for-t2081/m-p/1291123#M4076</link>
    <description>&lt;P&gt;Please refer to the following definition in&amp;nbsp;configs/T2081QDS_defconfig&lt;/P&gt;
&lt;P&gt;CONFIG_SYS_EXTRA_OPTIONS="PPC_T2081"&lt;/P&gt;</description>
    <pubDate>Fri, 11 Jun 2021 06:31:39 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2021-06-11T06:31:39Z</dc:date>
    <item>
      <title>Uboot code for t2081</title>
      <link>https://community.nxp.com/t5/T-Series/Uboot-code-for-t2081/m-p/1290801#M4075</link>
      <description>&lt;P&gt;I have a custom board with t2081 processor . So for uboot code, i used t208xqds machine. I generated the code for t208xqds machine in ubuntu 14.04.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Now, i have edited the T208XQDS.H file with-&lt;BR /&gt;"CONFIG_PPC_T2081 " as i intend to define t2081 processor and not t2080. And i did not define any where-&lt;BR /&gt;CONFIG_PPC_T2080&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Then why in the u-boot.cfg and generated config.h file, i see-&lt;/P&gt;&lt;P&gt;CONFIG_PPC_T2080 1&lt;/P&gt;&lt;P&gt;Actually i am generating bin file for the nor flash. Where the&lt;BR /&gt;"CONFIG_PPC_T2080 1" is defined, i m not able to find where it is defined. Which else file i need to change?&lt;/P&gt;&lt;P&gt;Actually&amp;nbsp; beacuse of&amp;nbsp; this scenario i am getting&amp;nbsp; serdes1 and serdes2,&amp;nbsp; wheras t2081 doesn't&amp;nbsp; have serdes2. Can any 1 help in this?&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jun 2021 14:38:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Uboot-code-for-t2081/m-p/1290801#M4075</guid>
      <dc:creator>monalihaware</dc:creator>
      <dc:date>2021-06-10T14:38:26Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot code for t2081</title>
      <link>https://community.nxp.com/t5/T-Series/Uboot-code-for-t2081/m-p/1291123#M4076</link>
      <description>&lt;P&gt;Please refer to the following definition in&amp;nbsp;configs/T2081QDS_defconfig&lt;/P&gt;
&lt;P&gt;CONFIG_SYS_EXTRA_OPTIONS="PPC_T2081"&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jun 2021 06:31:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Uboot-code-for-t2081/m-p/1291123#M4076</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-06-11T06:31:39Z</dc:date>
    </item>
  </channel>
</rss>