<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic T1040 VLAN issue in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T1040-VLAN-issue/m-p/454489#M405</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using the vconfig&amp;nbsp; command we set up vlan inet interface atT1040 board. The following commands were used:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ifconfig fm1-gb4 0.0.0.0 up&lt;/P&gt;&lt;P&gt;vconfig add fm1-gb4 4080&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #Creates fm1-gb4.4080, which is a vlan device with tpid=0x8100&lt;/P&gt;&lt;P&gt;ifconfig fm1-gb4.4080 1.0.0.1 up&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If we ping from a PC connected to T1040 fm1-gb4 LAN port the tcpdump shows that VLAN tagged packets are received, see:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@t1040rdb:/flashfs/Peter# tcpdump -s0 -XX -i fm1-gb4&lt;/P&gt;&lt;P&gt;tcpdump: WARNING: fm1-gb4: no IPv4 address assigned&lt;/P&gt;&lt;P&gt;tcpdump: verbose output suppressed, use -v or -vv for full protocol decode&lt;/P&gt;&lt;P&gt;listening on fm1-gb4, link-type EN10MB (Ethernet), capture size 65535 bytes&lt;/P&gt;&lt;P&gt;10:26:46.154909 ARP, Request who-has 1.0.0.1 tell 1.0.0.2, length 46&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0000:&amp;nbsp; ffff ffff ffff 001b 2181 0ad3 8100 0ff0&amp;nbsp; ........!.......&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0010:&amp;nbsp; 0806 0001 0800 0604 0001 001b 2181 0ad3&amp;nbsp; ............!...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0020:&amp;nbsp; 0100 0002 0000 0000 0000 0100 0001 0000&amp;nbsp; ................&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0030:&amp;nbsp; 0000 0000 0000 0000 0000 0000 0000 0000&amp;nbsp; ................&lt;/P&gt;&lt;P&gt;10:26:47.156905 ARP, Request who-has 1.0.0.1 tell 1.0.0.2, length 46&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0000:&amp;nbsp; ffff ffff ffff 001b 2181 0ad3 8100 0ff0&amp;nbsp; ........!.......&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0010:&amp;nbsp; 0806 0001 0800 0604 0001 001b 2181 0ad3&amp;nbsp; ............!...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0020:&amp;nbsp; 0100 0002 0000 0000 0000 0100 0001 0000&amp;nbsp; ................&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0030:&amp;nbsp; 0000 0000 0000 0000 0000 0000 0000 0000&amp;nbsp; ................&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RX packet counter of of fm1-gb4 increase but the RX packet counter of fm1-gb4.4080 does not increase.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can cause this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Oct 2015 16:21:22 GMT</pubDate>
    <dc:creator>keestrommel</dc:creator>
    <dc:date>2015-10-12T16:21:22Z</dc:date>
    <item>
      <title>T1040 VLAN issue</title>
      <link>https://community.nxp.com/t5/T-Series/T1040-VLAN-issue/m-p/454489#M405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using the vconfig&amp;nbsp; command we set up vlan inet interface atT1040 board. The following commands were used:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ifconfig fm1-gb4 0.0.0.0 up&lt;/P&gt;&lt;P&gt;vconfig add fm1-gb4 4080&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #Creates fm1-gb4.4080, which is a vlan device with tpid=0x8100&lt;/P&gt;&lt;P&gt;ifconfig fm1-gb4.4080 1.0.0.1 up&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If we ping from a PC connected to T1040 fm1-gb4 LAN port the tcpdump shows that VLAN tagged packets are received, see:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@t1040rdb:/flashfs/Peter# tcpdump -s0 -XX -i fm1-gb4&lt;/P&gt;&lt;P&gt;tcpdump: WARNING: fm1-gb4: no IPv4 address assigned&lt;/P&gt;&lt;P&gt;tcpdump: verbose output suppressed, use -v or -vv for full protocol decode&lt;/P&gt;&lt;P&gt;listening on fm1-gb4, link-type EN10MB (Ethernet), capture size 65535 bytes&lt;/P&gt;&lt;P&gt;10:26:46.154909 ARP, Request who-has 1.0.0.1 tell 1.0.0.2, length 46&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0000:&amp;nbsp; ffff ffff ffff 001b 2181 0ad3 8100 0ff0&amp;nbsp; ........!.......&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0010:&amp;nbsp; 0806 0001 0800 0604 0001 001b 2181 0ad3&amp;nbsp; ............!...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0020:&amp;nbsp; 0100 0002 0000 0000 0000 0100 0001 0000&amp;nbsp; ................&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0030:&amp;nbsp; 0000 0000 0000 0000 0000 0000 0000 0000&amp;nbsp; ................&lt;/P&gt;&lt;P&gt;10:26:47.156905 ARP, Request who-has 1.0.0.1 tell 1.0.0.2, length 46&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0000:&amp;nbsp; ffff ffff ffff 001b 2181 0ad3 8100 0ff0&amp;nbsp; ........!.......&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0010:&amp;nbsp; 0806 0001 0800 0604 0001 001b 2181 0ad3&amp;nbsp; ............!...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0020:&amp;nbsp; 0100 0002 0000 0000 0000 0100 0001 0000&amp;nbsp; ................&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0030:&amp;nbsp; 0000 0000 0000 0000 0000 0000 0000 0000&amp;nbsp; ................&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RX packet counter of of fm1-gb4 increase but the RX packet counter of fm1-gb4.4080 does not increase.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can cause this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Oct 2015 16:21:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1040-VLAN-issue/m-p/454489#M405</guid>
      <dc:creator>keestrommel</dc:creator>
      <dc:date>2015-10-12T16:21:22Z</dc:date>
    </item>
  </channel>
</rss>