<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic T2080 MPIC Global Timer not multicasting in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T2080-MPIC-Global-Timer-not-multicasting/m-p/1262348#M4040</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have been implementing a time triggered routine on the T2080RDB PCA platform. I use the global timer A group, more precisely the timer 0.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I set the GTVPRA0 accordingly, the destination register to multicast on all cores. The CTPR is also correctly set for all cores (masks interrupts 0 to 14, my&amp;nbsp;GTVPRA0 is set to have a priority of 15).&lt;BR /&gt;&lt;BR /&gt;However, the interrupt is only triggered on the CPU 0 (I don't use SMT so only one thread is enabled).&lt;/P&gt;&lt;P&gt;I can't find where my mistake is. I am pretty sure I forgot to set a register somewhere, but the fact that the CPU 0 receives the interrupts bugs me. Also, this implementation was first done on the P2020 target (that uses a PIC, not an MPIC) and it worked like a charm.&lt;/P&gt;&lt;P&gt;I was wondering if anyone had an idea about what to check to fix this issue.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Alexy&lt;/P&gt;</description>
    <pubDate>Thu, 15 Apr 2021 00:32:08 GMT</pubDate>
    <dc:creator>OXmose</dc:creator>
    <dc:date>2021-04-15T00:32:08Z</dc:date>
    <item>
      <title>T2080 MPIC Global Timer not multicasting</title>
      <link>https://community.nxp.com/t5/T-Series/T2080-MPIC-Global-Timer-not-multicasting/m-p/1262348#M4040</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have been implementing a time triggered routine on the T2080RDB PCA platform. I use the global timer A group, more precisely the timer 0.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I set the GTVPRA0 accordingly, the destination register to multicast on all cores. The CTPR is also correctly set for all cores (masks interrupts 0 to 14, my&amp;nbsp;GTVPRA0 is set to have a priority of 15).&lt;BR /&gt;&lt;BR /&gt;However, the interrupt is only triggered on the CPU 0 (I don't use SMT so only one thread is enabled).&lt;/P&gt;&lt;P&gt;I can't find where my mistake is. I am pretty sure I forgot to set a register somewhere, but the fact that the CPU 0 receives the interrupts bugs me. Also, this implementation was first done on the P2020 target (that uses a PIC, not an MPIC) and it worked like a charm.&lt;/P&gt;&lt;P&gt;I was wondering if anyone had an idea about what to check to fix this issue.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Alexy&lt;/P&gt;</description>
      <pubDate>Thu, 15 Apr 2021 00:32:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080-MPIC-Global-Timer-not-multicasting/m-p/1262348#M4040</guid>
      <dc:creator>OXmose</dc:creator>
      <dc:date>2021-04-15T00:32:08Z</dc:date>
    </item>
    <item>
      <title>Re: T2080 MPIC Global Timer not multicasting</title>
      <link>https://community.nxp.com/t5/T-Series/T2080-MPIC-Global-Timer-not-multicasting/m-p/1262471#M4041</link>
      <description>&lt;P&gt;What is the MPIC_GTDRA0 value?&lt;/P&gt;</description>
      <pubDate>Thu, 15 Apr 2021 04:33:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080-MPIC-Global-Timer-not-multicasting/m-p/1262471#M4041</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-04-15T04:33:37Z</dc:date>
    </item>
    <item>
      <title>Re: T2080 MPIC Global Timer not multicasting</title>
      <link>https://community.nxp.com/t5/T-Series/T2080-MPIC-Global-Timer-not-multicasting/m-p/1267297#M4047</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry for the late reply, I was not able to connect for the past week.&lt;BR /&gt;The value of&amp;nbsp;&lt;SPAN&gt;MPIC_GTDRA0 is 0x000000FF.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;We are investigating a synchronization issue at the moment, maybe the issue comes from here.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Alexy&lt;/P&gt;</description>
      <pubDate>Fri, 23 Apr 2021 13:39:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T2080-MPIC-Global-Timer-not-multicasting/m-p/1267297#M4047</guid>
      <dc:creator>OXmose</dc:creator>
      <dc:date>2021-04-23T13:39:44Z</dc:date>
    </item>
  </channel>
</rss>