<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 T1040d4 custom board without CPLD, JTAG programming issue</title>
    <link>https://community.nxp.com/t5/T-Series/T1040d4-custom-board-without-CPLD-JTAG-programming-issue/m-p/1252318#M4020</link>
    <description>Hi I have custom board designed using T1040d4 qoriq powerpc. My bareboard powerpc is currently power on using onboard power sequencing without using any CPLD. Right now i have no serial interface to monitor and debug it as both T1040 UART interfaced are attached with some other hardware over custom board. #Issue# when attached via CW usb tap its Jtag unable to program and flash bootloader via code warrior it shows " IR scan measure error" also "core not responding " in jtag log console.</description>
    <pubDate>Thu, 25 Mar 2021 17:03:07 GMT</pubDate>
    <dc:creator>Wj_khi</dc:creator>
    <dc:date>2021-03-25T17:03:07Z</dc:date>
    <item>
      <title>T1040d4 custom board without CPLD, JTAG programming issue</title>
      <link>https://community.nxp.com/t5/T-Series/T1040d4-custom-board-without-CPLD-JTAG-programming-issue/m-p/1252318#M4020</link>
      <description>Hi I have custom board designed using T1040d4 qoriq powerpc. My bareboard powerpc is currently power on using onboard power sequencing without using any CPLD. Right now i have no serial interface to monitor and debug it as both T1040 UART interfaced are attached with some other hardware over custom board. #Issue# when attached via CW usb tap its Jtag unable to program and flash bootloader via code warrior it shows " IR scan measure error" also "core not responding " in jtag log console.</description>
      <pubDate>Thu, 25 Mar 2021 17:03:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1040d4-custom-board-without-CPLD-JTAG-programming-issue/m-p/1252318#M4020</guid>
      <dc:creator>Wj_khi</dc:creator>
      <dc:date>2021-03-25T17:03:07Z</dc:date>
    </item>
    <item>
      <title>Re: T1040d4 custom board without CPLD, JTAG programming issue</title>
      <link>https://community.nxp.com/t5/T-Series/T1040d4-custom-board-without-CPLD-JTAG-programming-issue/m-p/1252743#M4021</link>
      <description>&lt;P&gt;Please refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/CodeWarrior-Development-Tools/T1040d4-custom-board-without-CPLD-JTAG-programming-issue/td-p/1252322" target="_blank"&gt;https://community.nxp.com/t5/CodeWarrior-Development-Tools/T1040d4-custom-board-without-CPLD-JTAG-programming-issue/td-p/1252322&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Mar 2021 09:13:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1040d4-custom-board-without-CPLD-JTAG-programming-issue/m-p/1252743#M4021</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-03-26T09:13:10Z</dc:date>
    </item>
  </channel>
</rss>