<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 Re: t1024 flash deployment</title>
    <link>https://community.nxp.com/t5/T-Series/t1024-flash-deployment/m-p/1234366#M3984</link>
    <description>&lt;P&gt;when I checked mtdparts I obtained the following result,&lt;/P&gt;&lt;P&gt;=&amp;gt; mtdparts&lt;BR /&gt;incorrect device type in spi0=spife110000.1&lt;/P&gt;&lt;P&gt;Also, in uboot there is not any command about nor , I mean there are for nand like below commands but nothing for nor flash, I want to use nor flash because nor is 128MB, nand is 64KB. Or could you guide me about how can I do?&lt;/P&gt;&lt;P&gt;Thank you for your consideration.&lt;/P&gt;&lt;P&gt;=&amp;gt; nand help&lt;BR /&gt;nand - NAND sub-system&lt;/P&gt;&lt;P&gt;Usage:&lt;BR /&gt;nand info - show available NAND devices&lt;BR /&gt;nand device [dev] - show or set current device&lt;BR /&gt;nand read - addr off|partition size&lt;BR /&gt;nand write - addr off|partition size&lt;BR /&gt;read/write 'size' bytes starting at offset 'off'&lt;BR /&gt;to/from memory address 'addr', skipping bad blocks.&lt;BR /&gt;nand read.raw - addr off|partition [count]&lt;BR /&gt;nand write.raw[.noverify] - addr off|partition [count]&lt;BR /&gt;Use read.raw/write.raw to avoid ECC and access the flash as-is.&lt;BR /&gt;nand erase[.spread] [clean] off size - erase 'size' bytes from offset 'off'&lt;BR /&gt;With '.spread', erase enough for given file size, otherwise,&lt;BR /&gt;'size' includes skipped bad blocks.&lt;BR /&gt;nand erase.part [clean] partition - erase entire mtd partition'&lt;BR /&gt;nand erase.chip [clean] - erase entire chip'&lt;BR /&gt;nand bad - show bad blocks&lt;BR /&gt;nand dump[.oob] off - dump page&lt;BR /&gt;nand scrub [-y] off size | scrub.part partition | scrub.chip&lt;BR /&gt;really clean NAND erasing bad blocks (UNSAFE)&lt;BR /&gt;nand markbad off [...] - mark bad block(s) at offset (UNSAFE)&lt;BR /&gt;nand biterr off - make a bit error at offset (UNSAFE)&lt;BR /&gt;=&amp;gt;&lt;/P&gt;</description>
    <pubDate>Mon, 22 Feb 2021 12:46:51 GMT</pubDate>
    <dc:creator>emras</dc:creator>
    <dc:date>2021-02-22T12:46:51Z</dc:date>
    <item>
      <title>t1024 flash deployment</title>
      <link>https://community.nxp.com/t5/T-Series/t1024-flash-deployment/m-p/1232848#M3979</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I have used as usual&amp;nbsp; NFS Deployment for development environment. Also I have tested SD Deployment.&lt;/P&gt;&lt;P&gt;I wonder about flash deployment. I have seen Ramdisk Deployment from Flash section in sdk documentation but it uses /dev/ram and the changes are disappear after reboot the system. I dont want this situation. How can I implement flash boot with nor or nand flashes with permanent changes. I work with T1024 yocto project and used those images, fsl-image-mfgtool-t1024rdb-64b.rootfs.tar.gz...&lt;/P&gt;&lt;P&gt;When I did quick search, I saw "ubifs". I need to implement ubifs for flash deployment ? is it necessary ?&lt;/P&gt;&lt;P&gt;Could you guide me for permanent flash boot with file system, kernel, device tree?&lt;/P&gt;&lt;P&gt;Thank you for your time and consideration.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Feb 2021 12:55:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/t1024-flash-deployment/m-p/1232848#M3979</guid>
      <dc:creator>emras</dc:creator>
      <dc:date>2021-02-18T12:55:51Z</dc:date>
    </item>
    <item>
      <title>Re: t1024 flash deployment</title>
      <link>https://community.nxp.com/t5/T-Series/t1024-flash-deployment/m-p/1233317#M3981</link>
      <description>&lt;P&gt;Please refer to the SDK documentation describing the NOR Flash memory map:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://docs.nxp.com/bundle/GUID-39A0A446-70E5-4ED7-A580-E7508B61A5F1/page/GUID-9D0808B4-40A3-48AD-9B08-AFE14FD4A2C9.html" target="_blank"&gt;https://docs.nxp.com/bundle/GUID-39A0A446-70E5-4ED7-A580-E7508B61A5F1/page/GUID-9D0808B4-40A3-48AD-9B08-AFE14FD4A2C9.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also you can refer or use "as is" complete 128 MB NOR Flash binary image provided in the "QorIQ Linux SDK v2.0 PPC64E5500 IMAGE.iso" available for free download from:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/linux-sdk-for-qoriq-processors:SDKLINUX?code=SDKLINUX&amp;amp;nodeId=0152109D3F8624&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#nogo" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/linux-sdk-for-qoriq-processors:SDKLINUX?code=SDKLINUX&amp;amp;nodeId=0152109D3F8624&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#nogo&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Feb 2021 05:01:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/t1024-flash-deployment/m-p/1233317#M3981</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-02-19T05:01:33Z</dc:date>
    </item>
    <item>
      <title>Re: t1024 flash deployment</title>
      <link>https://community.nxp.com/t5/T-Series/t1024-flash-deployment/m-p/1233335#M3982</link>
      <description>&lt;P&gt;Thanks ufedor,&lt;/P&gt;&lt;P&gt;I have checked again and again I have not seen 128 MB any file, when I checked system memory map just IFC-NOR Flash is 128 MB but it is a definition not an image. Also what image did you mean? uboot image or kernel image or file system.. the first link refers to flash memory usage not a how to work with flash with permanent file system. Also I think I need to do something in uboot like /dev/ram (but it is temporary). Could you guide me much more?&lt;/P&gt;&lt;P&gt;Thank you for your time and consideration.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Feb 2021 05:55:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/t1024-flash-deployment/m-p/1233335#M3982</guid>
      <dc:creator>emras</dc:creator>
      <dc:date>2021-02-19T05:55:05Z</dc:date>
    </item>
    <item>
      <title>Re: t1024 flash deployment</title>
      <link>https://community.nxp.com/t5/T-Series/t1024-flash-deployment/m-p/1233340#M3983</link>
      <description>&lt;P&gt;Thanks ufedor,&lt;/P&gt;&lt;P&gt;I have checked again and again I have not seen 128 MB any file, when I checked system memory map just IFC-NOR Flash is 128 MB but it is a definition not an image. Also what image did you mean? uboot image or kernel image or file system.. the first link refers to flash memory usage not a how to work with flash with permanent file system. Also I think I need to do something in uboot like /dev/ram (but it is temporary). Could you guide me much more?&lt;/P&gt;&lt;P&gt;Thank you for your time and consideration.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Feb 2021 05:58:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/t1024-flash-deployment/m-p/1233340#M3983</guid>
      <dc:creator>emras</dc:creator>
      <dc:date>2021-02-19T05:58:31Z</dc:date>
    </item>
    <item>
      <title>Re: t1024 flash deployment</title>
      <link>https://community.nxp.com/t5/T-Series/t1024-flash-deployment/m-p/1234366#M3984</link>
      <description>&lt;P&gt;when I checked mtdparts I obtained the following result,&lt;/P&gt;&lt;P&gt;=&amp;gt; mtdparts&lt;BR /&gt;incorrect device type in spi0=spife110000.1&lt;/P&gt;&lt;P&gt;Also, in uboot there is not any command about nor , I mean there are for nand like below commands but nothing for nor flash, I want to use nor flash because nor is 128MB, nand is 64KB. Or could you guide me about how can I do?&lt;/P&gt;&lt;P&gt;Thank you for your consideration.&lt;/P&gt;&lt;P&gt;=&amp;gt; nand help&lt;BR /&gt;nand - NAND sub-system&lt;/P&gt;&lt;P&gt;Usage:&lt;BR /&gt;nand info - show available NAND devices&lt;BR /&gt;nand device [dev] - show or set current device&lt;BR /&gt;nand read - addr off|partition size&lt;BR /&gt;nand write - addr off|partition size&lt;BR /&gt;read/write 'size' bytes starting at offset 'off'&lt;BR /&gt;to/from memory address 'addr', skipping bad blocks.&lt;BR /&gt;nand read.raw - addr off|partition [count]&lt;BR /&gt;nand write.raw[.noverify] - addr off|partition [count]&lt;BR /&gt;Use read.raw/write.raw to avoid ECC and access the flash as-is.&lt;BR /&gt;nand erase[.spread] [clean] off size - erase 'size' bytes from offset 'off'&lt;BR /&gt;With '.spread', erase enough for given file size, otherwise,&lt;BR /&gt;'size' includes skipped bad blocks.&lt;BR /&gt;nand erase.part [clean] partition - erase entire mtd partition'&lt;BR /&gt;nand erase.chip [clean] - erase entire chip'&lt;BR /&gt;nand bad - show bad blocks&lt;BR /&gt;nand dump[.oob] off - dump page&lt;BR /&gt;nand scrub [-y] off size | scrub.part partition | scrub.chip&lt;BR /&gt;really clean NAND erasing bad blocks (UNSAFE)&lt;BR /&gt;nand markbad off [...] - mark bad block(s) at offset (UNSAFE)&lt;BR /&gt;nand biterr off - make a bit error at offset (UNSAFE)&lt;BR /&gt;=&amp;gt;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Feb 2021 12:46:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/t1024-flash-deployment/m-p/1234366#M3984</guid>
      <dc:creator>emras</dc:creator>
      <dc:date>2021-02-22T12:46:51Z</dc:date>
    </item>
  </channel>
</rss>