<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Seriesのトピックbitbake -c compile -f virtual/kernel</title>
    <link>https://community.nxp.com/t5/T-Series/bitbake-c-compile-f-virtual-kernel/m-p/1212095#M3953</link>
    <description>&lt;P&gt;I&lt;/P&gt;&lt;P&gt;I modify the kernel code and recompile&lt;/P&gt;&lt;P&gt;Use the following command：&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;$ bitbake -c menuconfig virtual/kernel&lt;/P&gt;&lt;P&gt;$ bitbake -c compile -f virtual/kernel&lt;/P&gt;&lt;P&gt;When I execute the command $ bitbake -c menuconfig virtual/kernel.It has the same error as below, I found a solution in the community and executed this command successfully。&lt;/P&gt;&lt;P&gt;But&amp;nbsp;When I execute the command $bitbake -c compile -f virtual/kernel .&lt;SPAN&gt;This error came out again.&lt;/SPAN&gt;&lt;SPAN&gt;The last command menuconfig did not reproduce this error.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Does anyone have a similar problem? help me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NOTE: Preparing RunQueue&lt;BR /&gt;NOTE: Tainting hash to force rebuild of task /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb, do_compile&lt;BR /&gt;WARNING: /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb.do_compile is tainted from a forced run&lt;BR /&gt;NOTE: Executing SetScene Tasks&lt;BR /&gt;NOTE: Executing RunQueue Tasks&lt;BR /&gt;ERROR: oe_runmake failed&lt;BR /&gt;ERROR: Function failed: do_compile (log file is located at /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work/t2080rdb_64b-fsl-linux/linux-qoriq/4.1-r0/temp/log.do_compile.123112)&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work/t2080rdb_64b-fsl-linux/linux-qoriq/4.1-r0/temp/log.do_compile.123112&lt;BR /&gt;Log data follows:&lt;BR /&gt;| DEBUG: Executing shell function do_compile&lt;BR /&gt;| NOTE: make -j 4 uImage CC=powerpc64-fsl-linux-gcc -fuse-ld=bfd --sysroot=/home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/sysroots/t2080rdb-64b LD=powerpc64-fsl-linux-ld.bfd --sysroot=/home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/sysroots/t2080rdb-64b LOADADDR=0x80008000&lt;BR /&gt;| CHK include/config/kernel.release&lt;BR /&gt;| GEN ./Makefile&lt;BR /&gt;| CHK include/generated/uapi/linux/version.h&lt;BR /&gt;| CHK include/generated/utsrelease.h&lt;BR /&gt;| Using /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work-shared/t2080rdb-64b/kernel-source as source for kernel&lt;BR /&gt;| CHK include/generated/bounds.h&lt;BR /&gt;| CHK include/generated/asm-offsets.h&lt;BR /&gt;| CALL /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work-shared/t2080rdb-64b/kernel-source/scripts/checksyscalls.sh&lt;BR /&gt;| CHK include/generated/compile.h&lt;BR /&gt;| CALL /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work-shared/t2080rdb-64b/kernel-source/arch/powerpc/kernel/systbl_chk.sh&lt;BR /&gt;| CHK kernel/config_data.h&lt;BR /&gt;| make[4]: *** No rule to make target `drivers/net/virt_nic.o', needed by `drivers/net/built-in.o'. Stop.&lt;BR /&gt;| make[4]: *** Waiting for unfinished jobs....&lt;BR /&gt;| LD drivers/video/backlight/built-in.o&lt;BR /&gt;| CC drivers/video/console/dummycon.o&lt;BR /&gt;| CC drivers/virt/fsl_hypervisor.o&lt;BR /&gt;| make[3]: *** [drivers/net] Error 2&lt;BR /&gt;| make[3]: *** Waiting for unfinished jobs....&lt;BR /&gt;| CC drivers/video/fbdev/core/fb_notify.o&lt;BR /&gt;| CC drivers/video/console/vgacon.o&lt;BR /&gt;| LD drivers/video/fbdev/omap2/displays-new/built-in.o&lt;BR /&gt;| LD drivers/video/fbdev/omap2/dss/built-in.o&lt;BR /&gt;| LD drivers/video/fbdev/omap2/built-in.o&lt;BR /&gt;| LD drivers/video/fbdev/core/built-in.o&lt;BR /&gt;| LD drivers/video/fbdev/built-in.o&lt;BR /&gt;| LD drivers/virt/built-in.o&lt;BR /&gt;| LD drivers/video/console/built-in.o&lt;BR /&gt;| LD drivers/video/built-in.o&lt;BR /&gt;| make[2]: *** [drivers] Error 2&lt;BR /&gt;| make[1]: *** [sub-make] Error 2&lt;BR /&gt;| make: *** [__sub-make] Error 2&lt;BR /&gt;| WARNING: /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work/t2080rdb_64b-fsl-linux/linux-qoriq/4.1-r0/temp/run.do_compile.123112:1 exit 1 from&lt;BR /&gt;| exit 1&lt;BR /&gt;| ERROR: oe_runmake failed&lt;BR /&gt;| ERROR: Function failed: do_compile (log file is located at /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work/t2080rdb_64b-fsl-linux/linux-qoriq/4.1-r0/temp/log.do_compile.123112)&lt;BR /&gt;ERROR: Task 5 (/home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb, do_compile) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 286 tasks of which 285 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;BR /&gt;/home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb, do_compile&lt;BR /&gt;Summary: There was 1 WARNING message shown.&lt;BR /&gt;Summary: There were 2 ERROR messages shown, returning a non-zero exit code.&lt;/P&gt;</description>
    <pubDate>Fri, 15 Jan 2021 03:29:41 GMT</pubDate>
    <dc:creator>zmq001</dc:creator>
    <dc:date>2021-01-15T03:29:41Z</dc:date>
    <item>
      <title>bitbake -c compile -f virtual/kernel</title>
      <link>https://community.nxp.com/t5/T-Series/bitbake-c-compile-f-virtual-kernel/m-p/1212095#M3953</link>
      <description>&lt;P&gt;I&lt;/P&gt;&lt;P&gt;I modify the kernel code and recompile&lt;/P&gt;&lt;P&gt;Use the following command：&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;$ bitbake -c menuconfig virtual/kernel&lt;/P&gt;&lt;P&gt;$ bitbake -c compile -f virtual/kernel&lt;/P&gt;&lt;P&gt;When I execute the command $ bitbake -c menuconfig virtual/kernel.It has the same error as below, I found a solution in the community and executed this command successfully。&lt;/P&gt;&lt;P&gt;But&amp;nbsp;When I execute the command $bitbake -c compile -f virtual/kernel .&lt;SPAN&gt;This error came out again.&lt;/SPAN&gt;&lt;SPAN&gt;The last command menuconfig did not reproduce this error.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Does anyone have a similar problem? help me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NOTE: Preparing RunQueue&lt;BR /&gt;NOTE: Tainting hash to force rebuild of task /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb, do_compile&lt;BR /&gt;WARNING: /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb.do_compile is tainted from a forced run&lt;BR /&gt;NOTE: Executing SetScene Tasks&lt;BR /&gt;NOTE: Executing RunQueue Tasks&lt;BR /&gt;ERROR: oe_runmake failed&lt;BR /&gt;ERROR: Function failed: do_compile (log file is located at /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work/t2080rdb_64b-fsl-linux/linux-qoriq/4.1-r0/temp/log.do_compile.123112)&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work/t2080rdb_64b-fsl-linux/linux-qoriq/4.1-r0/temp/log.do_compile.123112&lt;BR /&gt;Log data follows:&lt;BR /&gt;| DEBUG: Executing shell function do_compile&lt;BR /&gt;| NOTE: make -j 4 uImage CC=powerpc64-fsl-linux-gcc -fuse-ld=bfd --sysroot=/home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/sysroots/t2080rdb-64b LD=powerpc64-fsl-linux-ld.bfd --sysroot=/home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/sysroots/t2080rdb-64b LOADADDR=0x80008000&lt;BR /&gt;| CHK include/config/kernel.release&lt;BR /&gt;| GEN ./Makefile&lt;BR /&gt;| CHK include/generated/uapi/linux/version.h&lt;BR /&gt;| CHK include/generated/utsrelease.h&lt;BR /&gt;| Using /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work-shared/t2080rdb-64b/kernel-source as source for kernel&lt;BR /&gt;| CHK include/generated/bounds.h&lt;BR /&gt;| CHK include/generated/asm-offsets.h&lt;BR /&gt;| CALL /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work-shared/t2080rdb-64b/kernel-source/scripts/checksyscalls.sh&lt;BR /&gt;| CHK include/generated/compile.h&lt;BR /&gt;| CALL /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work-shared/t2080rdb-64b/kernel-source/arch/powerpc/kernel/systbl_chk.sh&lt;BR /&gt;| CHK kernel/config_data.h&lt;BR /&gt;| make[4]: *** No rule to make target `drivers/net/virt_nic.o', needed by `drivers/net/built-in.o'. Stop.&lt;BR /&gt;| make[4]: *** Waiting for unfinished jobs....&lt;BR /&gt;| LD drivers/video/backlight/built-in.o&lt;BR /&gt;| CC drivers/video/console/dummycon.o&lt;BR /&gt;| CC drivers/virt/fsl_hypervisor.o&lt;BR /&gt;| make[3]: *** [drivers/net] Error 2&lt;BR /&gt;| make[3]: *** Waiting for unfinished jobs....&lt;BR /&gt;| CC drivers/video/fbdev/core/fb_notify.o&lt;BR /&gt;| CC drivers/video/console/vgacon.o&lt;BR /&gt;| LD drivers/video/fbdev/omap2/displays-new/built-in.o&lt;BR /&gt;| LD drivers/video/fbdev/omap2/dss/built-in.o&lt;BR /&gt;| LD drivers/video/fbdev/omap2/built-in.o&lt;BR /&gt;| LD drivers/video/fbdev/core/built-in.o&lt;BR /&gt;| LD drivers/video/fbdev/built-in.o&lt;BR /&gt;| LD drivers/virt/built-in.o&lt;BR /&gt;| LD drivers/video/console/built-in.o&lt;BR /&gt;| LD drivers/video/built-in.o&lt;BR /&gt;| make[2]: *** [drivers] Error 2&lt;BR /&gt;| make[1]: *** [sub-make] Error 2&lt;BR /&gt;| make: *** [__sub-make] Error 2&lt;BR /&gt;| WARNING: /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work/t2080rdb_64b-fsl-linux/linux-qoriq/4.1-r0/temp/run.do_compile.123112:1 exit 1 from&lt;BR /&gt;| exit 1&lt;BR /&gt;| ERROR: oe_runmake failed&lt;BR /&gt;| ERROR: Function failed: do_compile (log file is located at /home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b/tmp/work/t2080rdb_64b-fsl-linux/linux-qoriq/4.1-r0/temp/log.do_compile.123112)&lt;BR /&gt;ERROR: Task 5 (/home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb, do_compile) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 286 tasks of which 285 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;BR /&gt;/home/can/t2080/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb, do_compile&lt;BR /&gt;Summary: There was 1 WARNING message shown.&lt;BR /&gt;Summary: There were 2 ERROR messages shown, returning a non-zero exit code.&lt;/P&gt;</description>
      <pubDate>Fri, 15 Jan 2021 03:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/bitbake-c-compile-f-virtual-kernel/m-p/1212095#M3953</guid>
      <dc:creator>zmq001</dc:creator>
      <dc:date>2021-01-15T03:29:41Z</dc:date>
    </item>
    <item>
      <title>Re: bitbake -c compile -f virtual/kernel</title>
      <link>https://community.nxp.com/t5/T-Series/bitbake-c-compile-f-virtual-kernel/m-p/1221733#M3957</link>
      <description>&lt;P&gt;It seems that there is problem with Linux Kernel configuration file.&lt;/P&gt;
&lt;P&gt;Would you please send Linux Kernel configuration file(.config) in&amp;nbsp;build_t2080rdb-64b/tmp/work/t2080rdb_64b-fsl-linux/linux-qoriq/4.1-r0/build/.config to me to do more investigation?&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jan 2021 07:15:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/bitbake-c-compile-f-virtual-kernel/m-p/1221733#M3957</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-01-27T07:15:09Z</dc:date>
    </item>
  </channel>
</rss>