<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 Re: T1022 Processor configuration</title>
    <link>https://community.nxp.com/t5/T-Series/T1022-Processor-configuration/m-p/1198525#M3921</link>
    <description>&lt;P&gt;It is a valid configuration.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 14 Dec 2020 04:36:10 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2020-12-14T04:36:10Z</dc:date>
    <item>
      <title>T1022 Processor configuration</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Processor-configuration/m-p/1197849#M3912</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello All,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am using T1022 processor i&lt;/SPAN&gt;&lt;SPAN&gt;n one of the designs. In the design, I do not want to use the RGMII/MII on EC1 or EC2 interface, but want to use only MDIO at 2.5V. I understand that for this use case:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt; power L1VDD and LVDD will have to be kept at 2.5V&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt; EC1 and EC2 will be configured as GPIOs and&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt; there will be no requirement for oscillator on EC*_GTX_CLK125.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can someone confirm whether it is a valid configuration or not?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 05:31:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Processor-configuration/m-p/1197849#M3912</guid>
      <dc:creator>swatig</dc:creator>
      <dc:date>2020-12-11T05:31:24Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 Processor configuration</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-Processor-configuration/m-p/1198525#M3921</link>
      <description>&lt;P&gt;It is a valid configuration.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Dec 2020 04:36:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-Processor-configuration/m-p/1198525#M3921</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2020-12-14T04:36:10Z</dc:date>
    </item>
  </channel>
</rss>