<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: T1022 IFC LSB in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/T1022-IFC-LSB/m-p/1156692#M3843</link>
    <description>&lt;P&gt;Connect 8-bit port&amp;nbsp; to&amp;nbsp;&lt;SPAN class="fontstyle0"&gt;AD[0:7], AD0 is the most significant bit.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 22 Sep 2020 05:52:56 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2020-09-22T05:52:56Z</dc:date>
    <item>
      <title>T1022 IFC LSB</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-IFC-LSB/m-p/1155348#M3836</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We would like to connect a TL16C752D Dual UART to the IFC bus on the T1022. We are assuming the GPCM mode is the most suitable for this application?&lt;/P&gt;&lt;P&gt;We are also unsure what LSB of address and data bus should be?&lt;/P&gt;&lt;P&gt;Should the address start at IFC_A31?&lt;/P&gt;&lt;P&gt;Is the Data bus LSB IFC_AD7 and MSB IFC_AD0?&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2020 07:32:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-IFC-LSB/m-p/1155348#M3836</guid>
      <dc:creator>jack_mcculloch</dc:creator>
      <dc:date>2020-09-18T07:32:35Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 IFC LSB</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-IFC-LSB/m-p/1155944#M3838</link>
      <description>&lt;P&gt;In the normal GPCM mode of operation ADDR bus carries the least significant bits. ADDR[31] will carry the lsb of the system address.&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2020 03:26:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-IFC-LSB/m-p/1155944#M3838</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2020-09-21T03:26:50Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 IFC LSB</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-IFC-LSB/m-p/1156083#M3840</link>
      <description>&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;And how do we align the data bus if we are using 8 bits?&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2020 07:49:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-IFC-LSB/m-p/1156083#M3840</guid>
      <dc:creator>jack_mcculloch</dc:creator>
      <dc:date>2020-09-21T07:49:22Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 IFC LSB</title>
      <link>https://community.nxp.com/t5/T-Series/T1022-IFC-LSB/m-p/1156692#M3843</link>
      <description>&lt;P&gt;Connect 8-bit port&amp;nbsp; to&amp;nbsp;&lt;SPAN class="fontstyle0"&gt;AD[0:7], AD0 is the most significant bit.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Sep 2020 05:52:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/T1022-IFC-LSB/m-p/1156692#M3843</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2020-09-22T05:52:56Z</dc:date>
    </item>
  </channel>
</rss>