<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Does T4240QDS development/test board support Display? in T-Series</title>
    <link>https://community.nxp.com/t5/T-Series/Does-T4240QDS-development-test-board-support-Display/m-p/1152090#M3827</link>
    <description>&lt;P&gt;T4240QDS does not possess a display port.&lt;/P&gt;
&lt;P&gt;UART COM port is used for communication with a host PC.&lt;/P&gt;
&lt;P&gt;Technically, a PCIe graphics card can be inserted into an on-board PCIe slot, but there is no such reference solution from NXP.&lt;/P&gt;</description>
    <pubDate>Fri, 11 Sep 2020 10:10:41 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2020-09-11T10:10:41Z</dc:date>
    <item>
      <title>Does T4240QDS development/test board support Display?</title>
      <link>https://community.nxp.com/t5/T-Series/Does-T4240QDS-development-test-board-support-Display/m-p/1151938#M3825</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm going through schematic and Layout of&amp;nbsp;&lt;SPAN class="fontstyle0"&gt;T4240QDS development/test board&lt;/SPAN&gt;&amp;nbsp;and I can't find any display support on&amp;nbsp; &lt;SPAN class="fontstyle0"&gt;T4240QDS development/test board. I want to connect display with this board to use it as normal PC. Can anyone tell me how can I connect display with this board and through which port or component I can do that?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Also I noticed that there is no GPU support available on board. Do I have to connect some GPU for display as well with that board?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Sep 2020 05:17:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Does-T4240QDS-development-test-board-support-Display/m-p/1151938#M3825</guid>
      <dc:creator>A-R</dc:creator>
      <dc:date>2020-09-11T05:17:53Z</dc:date>
    </item>
    <item>
      <title>Re: Does T4240QDS development/test board support Display?</title>
      <link>https://community.nxp.com/t5/T-Series/Does-T4240QDS-development-test-board-support-Display/m-p/1152090#M3827</link>
      <description>&lt;P&gt;T4240QDS does not possess a display port.&lt;/P&gt;
&lt;P&gt;UART COM port is used for communication with a host PC.&lt;/P&gt;
&lt;P&gt;Technically, a PCIe graphics card can be inserted into an on-board PCIe slot, but there is no such reference solution from NXP.&lt;/P&gt;</description>
      <pubDate>Fri, 11 Sep 2020 10:10:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Does-T4240QDS-development-test-board-support-Display/m-p/1152090#M3827</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-09-11T10:10:41Z</dc:date>
    </item>
    <item>
      <title>Re: Does T4240QDS development/test board support Display?</title>
      <link>https://community.nxp.com/t5/T-Series/Does-T4240QDS-development-test-board-support-Display/m-p/1152123#M3828</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/56916"&gt;@ufedor&lt;/a&gt;&amp;nbsp;Thanks for your reply. I want to ask some more questions as well.&lt;BR /&gt;&lt;BR /&gt;I went through T1040 which have DIU. Now can I use that processor for GUI based Linux? And also is there any reference design available of that processor with Display/VGA/HDMI?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I'm looking for any NXP processor on which I can do some processing using GUI based Linux. Can you recommend any processor with it's reference design? It will be very helpful for me.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Sep 2020 11:55:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/Does-T4240QDS-development-test-board-support-Display/m-p/1152123#M3828</guid>
      <dc:creator>A-R</dc:creator>
      <dc:date>2020-09-11T11:55:44Z</dc:date>
    </item>
  </channel>
</rss>