<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>T-Series中的主题 Re: DDR3 Address Command Routing</title>
    <link>https://community.nxp.com/t5/T-Series/DDR3-Address-Command-Routing/m-p/1083974#M3727</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your prompt reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Jun 2020 06:11:52 GMT</pubDate>
    <dc:creator>athershehzad</dc:creator>
    <dc:date>2020-06-11T06:11:52Z</dc:date>
    <item>
      <title>DDR3 Address Command Routing</title>
      <link>https://community.nxp.com/t5/T-Series/DDR3-Address-Command-Routing/m-p/1083972#M3725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sir I am designing a custom board using T1042 and I am using on board DDR3 SDRAMs. While routing DDR3 signals, I am following this document "AN3940-Hardware and Layout Consideration For DDR3".. I am a little bit confused in point 31 in this document i.e.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE height="468" width="854"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD style="width: 846px;"&gt;&lt;SPAN class=""&gt;Ensure fly-by topology is used for address/command/control and clock groups. The routing in fly-by topology&lt;BR /&gt;should go from chip 0 to chip &lt;/SPAN&gt;&lt;SPAN class=""&gt;n &lt;/SPAN&gt;&lt;SPAN class=""&gt;and can be in the order that is most convenient for the board design. The&lt;BR /&gt;fly-by topology routing of address/command/ control and clock groups must end at the termination resistors&lt;BR /&gt;that are after chip &lt;/SPAN&gt;&lt;SPAN class=""&gt;n.&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;Choose one of the following options to select the impedances and spacings for the DDR3&lt;BR /&gt;address/command/control group.&lt;BR /&gt;Option #1 (wider traces—lower trace impedance)&lt;BR /&gt;• Single-ended impedance = 40 &lt;/SPAN&gt;&lt;SPAN class=""&gt;Ω&lt;/SPAN&gt;&lt;SPAN class=""&gt;. The lower impedance allows traces to be slightly closer with less&lt;BR /&gt;cross-talk.&lt;BR /&gt;• Utilize wider traces if stackup allows (7–8 mils)&lt;BR /&gt;• Spacing to other like signals = 1.5x to 2.0x&lt;BR /&gt;• Spacing to all other non-DDR signals = 3–4x&lt;BR /&gt;Option #2 (smaller traces—higher trace impedance)&lt;BR /&gt;• Single-ended impedance = 50 &lt;/SPAN&gt;&lt;SPAN class=""&gt;Ω&lt;/SPAN&gt;&lt;SPAN class=""&gt;.&lt;BR /&gt;• Smaller trace widths (5–6 mils) can be used.&lt;BR /&gt;• Spacing between like signals should increase to 3x (for 5 mils) or 2.5x (for 6 mils) respectively&lt;BR /&gt;• Spacing to all other non-DDR signals = 3–4x with regards to tuning&lt;BR /&gt;• Tune signals to +/-10 mils of the clock at each device&lt;/SPAN&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;In the second option it states that tune signals to +-10 mils of the clock at each device however in the first option it did not say it.&lt;/P&gt;&lt;P&gt;My question is why is it necessary for the signals routed at 50 ohm impedance to length matched and this is not a requirement for 40 ohm impedance signals ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2020 04:44:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/DDR3-Address-Command-Routing/m-p/1083972#M3725</guid>
      <dc:creator>athershehzad</dc:creator>
      <dc:date>2020-06-11T04:44:29Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Address Command Routing</title>
      <link>https://community.nxp.com/t5/T-Series/DDR3-Address-Command-Routing/m-p/1083973#M3726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"&lt;SPAN class=""&gt;Tune signals to +/-10 mils of the clock at each device&lt;/SPAN&gt;" applies to both options.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2020 05:54:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/DDR3-Address-Command-Routing/m-p/1083973#M3726</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-06-11T05:54:56Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Address Command Routing</title>
      <link>https://community.nxp.com/t5/T-Series/DDR3-Address-Command-Routing/m-p/1083974#M3727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your prompt reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2020 06:11:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/DDR3-Address-Command-Routing/m-p/1083974#M3727</guid>
      <dc:creator>athershehzad</dc:creator>
      <dc:date>2020-06-11T06:11:52Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Address Command Routing</title>
      <link>https://community.nxp.com/t5/T-Series/DDR3-Address-Command-Routing/m-p/1083975#M3728</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sir as you had confirmed that i must follow this rule so I have to add lengths to my address command signals to tune them. I am using discrete RAMs in my design and after adding lengths to the signals, they will become greater than 7 inch in length that will violate rule # 23 that states :&lt;/P&gt;&lt;TABLE height="46" width="780"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD style="width: 772px;"&gt;&lt;SPAN class=""&gt;Ensure the max lead-in trace length for data/address/command signals are no longer than 7 inches&lt;/SPAN&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;Can you tell what rule should be given priority ?&lt;/P&gt;&lt;P&gt;Can you explain the term lead-in trace length ?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ather&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jun 2020 08:43:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/T-Series/DDR3-Address-Command-Routing/m-p/1083975#M3728</guid>
      <dc:creator>athershehzad</dc:creator>
      <dc:date>2020-06-15T08:43:18Z</dc:date>
    </item>
  </channel>
</rss>